This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

还是来问问专家:看门狗到底功耗多大?

msp430G2系列,指导手册中有这样一段:

The MSP430 devices have several low-power modes. Different clock signals are available in different
low-power modes. The requirements of the user’s application and the type of clocking used determine
how the WDT+ should be configured. For example, the WDT+ should not be configured in watchdog mode
with SMCLK as its clock source if the user wants to use low-power mode 3 because the WDT+ will keep
SMCLK enabled for its clock source, increasing the current consumption of LPM3. When the watchdog
timer+ is not required, the WDTHOLD bit can be used to hold the WDTCNT, reducing power consumption.

但是在哪里查到底多少功耗呀?