msp430g2332用内部时钟时,批量生产时每个板上的频率都不同,与设定的频点会差几十赫兹,怎么办?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
msp430g2332用内部时钟时,批量生产时每个板上的频率都不同,与设定的频点会差几十赫兹,怎么办?
大部分msp430内部都存储有ti出厂时校准dco的参数,msp430g2332也有。
在初始化的时候添加上相关代码就能校准dco,代码见如下例程
******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP430G2xx2 Demo - Basic Clock, Output Buffered clocks with preloaded DCO // calibration constants for BCSCTL1 and DCOCTL. // // Description: Buffer ACLK on P1.0, default SMCLK(DCO) on P1.4 and MCLK/10 on // P1.1. DCO is software selectable to 1, 8, 12, or 16Mhz using calibration // contstants in INFOA. // // ACLK = LFXT1 = 32768, MCLK = SMCLK = Selectable at 1, 8, 12 or 16Mhz // //* External watch crystal installed on XIN XOUT is required for ACLK *// // //* By default, the MSP430 uses XT1 to source ACLK; P2.6/7 configured // //* automatically. // MSP430G2xx2 // ----------------- // /|\| P2.6/XIN|- // | | | 32kHz // --|RST P2.7/XOUT|- // | | // | P1.4/SMCLK|-->SMCLK = Default DCO // | P1.1|-->MCLK/10 = DCO/10 // | P1.0/ACLK|-->ACLK = 32kHz // D. Dang // Texas Instruments Inc. // December 2010 // Built with IAR Embedded Workbench Version: 3.42A //****************************************************************************** #include <msp430.h> int main(void) { WDTCTL = WDTPW +WDTHOLD; // Stop Watchdog Timer //1Mhz if (CALBC1_1MHZ==0xFF) // If calibration constants erased { while(1); // do not load, trap CPU!! } DCOCTL = 0; // Select lowest DCOx and MODx settings BCSCTL1 = CALBC1_1MHZ; // Set range DCOCTL = CALDCO_1MHZ; // Set DCO step + modulation */ /* //8Mhz if (CALBC1_8MHZ==0xFF) // If calibration constants erased { while(1); // do not load, trap CPU!! } DCOCTL = 0; // Select lowest DCOx and MODx settings BCSCTL1 = CALBC1_8MHZ; // Set range DCOCTL = CALDCO_8MHZ; // Set DCO step + modulation */ /* //12Mhz if (CALBC1_12MHZ==0xFF) // If calibration constants erased { while(1); // do not load, trap CPU!! } DCOCTL = 0; // Select lowest DCOx and MODx settings BCSCTL1 = CALBC1_12MHZ; // Set range DCOCTL = CALDCO_12MHZ; // Set DCO step + modulation*/ /* //16Mhz if (CALBC1_16MHZ==0xFF) // If calibration constants erased { while(1); // do not load, trap CPU!! } DCOCTL = 0; // Select lowest DCOx and MODx settings BCSCTL1 = CALBC1_16MHZ; // Set range DCOCTL = CALDCO_16MHZ; // Set DCO step + modulation*/ P1DIR |= 0x13; // P1.0,1 and P1.4 outputs P1SEL |= 0x11; // P1.0,4 ACLK, SMCLK output while(1) { P1OUT |= 0x02; // P1.1 = 1 P1OUT &= ~0x02; // P1.1 = 0 } }