This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f2274未用IO的处理



按照手册和网上查询的办法,未用IO的推荐方法之一为设置为“输出”,不但抗干扰,而且低功耗。但是,我用下面的程序设置后:

/*

未用的IO包括:

1、P1.1 P1.2 P1.3 P1.4 P1.5 P1.6 P1.7           11111110:0XFE

2、P2.0 P2.1 P2.2 P2.3 P2.4 P2.5                00111111:0X3F

3、P3.7                                         10000000:0X80

4、P4.0 P4.1 P4.2 P4.3 P4.4 P4.5 P4.6 P4.7      11111111:0XFF

*/

void unused_io(void)

{

   P1DIR |= 0xFE;

   P2DIR |= 0x3F;

   P3DIR |= 0x80;

   P4DIR |= 0xFF;

}

在LPM4模式下,不但功耗没有降低,反而增加了十几个微安,什么原因?

未用IO该如何处理能降低功耗?

谢谢