This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的MSP430F6638板子上自带板载仿真器,仿真器部分电路和TI官网的5529开发板一样
MSP430F6638工作电压3.3V
通过板载仿真器供电时,6638的TEST脚为2.8V, RESET脚为3.3V
按下复位键时,RESET脚被拉低为0V,但是此时6638正常工作,没有被复位,
请问这是什么问题呢?
顺便,如果仍通过,板载仿真器供电,6638工作电压3.3V
但是此时如果将TEST的跳线拔除,
6638的TEST脚上的电压为0V,
此时按下RESET键,6638能被正常复位。