Other Parts Discussed in Thread: MSP430G2452
错误信息如下所示:
"../lnk_msp430g2452.cmd", line 93: error #10099-D: program will not fit into available memory. run placement with alignment fails for section ".stack" size 0x50 . Available memory ranges:
RAM size: 0x100 unused: 0x40 max hole: 0x40
remark #10371-D: (ULP 1.1) Detected no uses of low power mode state changing instructions
error #10010: errors encountered during linking; "000.out" not built
根据错误提示,是程序不能写入可用的内存。
经过比对2452余2553两个的cmd文件,发现内存确实不是一样大的。查看官方资料2452的内存为256字节。刚好是0x100
修改cmd试试,将默认的0x100修改大一点看看效果。
改成了0x150编译成功了。原来刚刚超额了一点点。
MSP430: Flash/FRAM usage is 664 bytes. RAM usage is 272 bytes.
试试运行效果。不行,所以可以根据这个结果进行优化程序。事实证明,不能做欺骗编译器的事情,实际是多少就是多少。。。