This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2系列默认DCO的频率默认的多少?

看到官方的很多例子,都是没有对时钟频率进行设置。如下所示。

#include <msp430.h>

int main(void)
{
  WDTCTL = WDTPW + WDTHOLD;                 // Stop watchdog timer
  P1DIR |= 0x01;                            // Set P1.0 to output direction

  while (1)                                 // Test P1.4
  {
    if ((0x10 & P1IN)) P1OUT |= 0x01;       // if P1.4 set, set P1.0
    else P1OUT &= ~0x01;                    // else reset
  }
}

#include <msp430.h>

int main(void)
{
  WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
  P1DIR |= 0x01;                            // P1.0 output
  CCTL0 = CCIE;                             // CCR0 interrupt enabled
  CCR0 = 50000;
  TACTL = TASSEL_2 + MC_2;                  // SMCLK, contmode

  __bis_SR_register(LPM0_bits + GIE);       // Enter LPM0 w/ interrupt
}

// Timer A0 interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=TIMER0_A0_VECTOR
__interrupt void Timer_A (void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(TIMER0_A0_VECTOR))) Timer_A (void)
#else
#error Compiler not supported!
#endif
{
  P1OUT ^= 0x01;                            // Toggle P1.0
  CCR0 += 50000;                            // Add Offset to CCR0
}

这些都没有进行配置,那么默认频率是多少呢?

430上电后默认DCO设置为RSELx = 7, DCOx = 3, MODx = 0,其频率范围是0.8~1.5MHz(3V电压)
这就有问题了,到底是多少呢?有两种说法最常见:800KHz和1MHZ

难道上电后的默认DCO频率真的是不确定的?

必须要通过校准指令实现频率确定?如下代码所示

//运行以下代码可将DCO校准至精准的1MHz
DCOCTL=0;
BCSCTL1=CALBC1_1MHZ;
DCOCTL=CALDCO_1MHZ;

对这个有了解的一起讨论一下