This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430g系列 USI 模块 SPI 模式请问底层函数



请问官方有给出msp430g系列 USI模块的SPI底层函数代码吗?我想深入学习一下430的spi.

  • 我们有官方例程可以供您参考,里面提供了一些函数

    dev.ti.com/.../node
  • msp430g系列是没有库函数的,都是直接操作寄存器。所以官网的例程没有所谓底层函数的说法。

    上传两个例程,你参考下

    //******************************************************************************
    //   MSP430G2xx3 Demo - USCI_A0, SPI 3-Wire Slave multiple byte RX/TX
    //
    //   Description: SPI master communicates to SPI slave sending and receiving
    //   3 different messages of different length. SPI slave will enter LPM0
    //   while waiting for the messages to be sent/receiving using SPI interrupt.
    //   ACLK = NA, MCLK = SMCLK = DCO 16MHz.
    //
    //
    //                   MSP430G2553
    //                 -----------------
    //            /|\ |             P2.0|<- Master's GPIO (Chip Select)
    //             |  |                 |
    //             ---|RST          RST |<- Master's GPIO (To reset slave)
    //                |                 |
    //                |             P1.2|<- Data In (UCA0SIMO)
    //                |                 |
    //                |             P1.1|-> Data Out (UCA0SOMI)
    //                |                 |
    //                |             P1.4|<- Serial Clock In (UCA0CLK)
    //
    //   Nima Eskandari
    //   Texas Instruments Inc.
    //   April 2017
    //   Built with CCS V7.0
    //******************************************************************************
    
    #include <msp430.h> 
    #include <stdint.h>
    
    //******************************************************************************
    // Example Commands ************************************************************
    //******************************************************************************
    
    #define DUMMY   0xFF
    
    #define SLAVE_CS_IN     P2IN
    #define SLAVE_CS_DIR    P2DIR
    #define SLAVE_CS_PIN    BIT0
    
    /* CMD_TYPE_X_SLAVE are example commands the master sends to the slave.
     * The slave will send example SlaveTypeX buffers in response.
     *
     * CMD_TYPE_X_MASTER are example commands the master sends to the slave.
     * The slave will initialize itself to receive MasterTypeX example buffers.
     * */
    
    #define CMD_TYPE_0_SLAVE              0
    #define CMD_TYPE_1_SLAVE              1
    #define CMD_TYPE_2_SLAVE              2
    
    #define CMD_TYPE_0_MASTER              3
    #define CMD_TYPE_1_MASTER              4
    #define CMD_TYPE_2_MASTER              5
    
    #define TYPE_0_LENGTH              1
    #define TYPE_1_LENGTH              2
    #define TYPE_2_LENGTH              6
    
    #define MAX_BUFFER_SIZE     20
    
    /* MasterTypeX are example buffers initialized in the master, they will be
     * sent by the master to the slave.
     * SlaveTypeX are example buffers initialized in the slave, they will be
     * sent by the slave to the master.
     * */
    
    uint8_t MasterType2 [TYPE_2_LENGTH] = {0};
    uint8_t MasterType1 [TYPE_1_LENGTH] = { 0, 0};
    uint8_t MasterType0 [TYPE_0_LENGTH] = { 0};
    
    uint8_t SlaveType2 [TYPE_2_LENGTH] = {'A', 'B', 'C', 'D', '1', '2'};
    uint8_t SlaveType1 [TYPE_1_LENGTH] = {0x15, 0x16};
    uint8_t SlaveType0 [TYPE_0_LENGTH] = {12};
    
    //******************************************************************************
    // General SPI State Machine ***************************************************
    //******************************************************************************
    
    typedef enum SPI_ModeEnum{
        IDLE_MODE,
        TX_REG_ADDRESS_MODE,
        RX_REG_ADDRESS_MODE,
        TX_DATA_MODE,
        RX_DATA_MODE,
        TIMEOUT_MODE
    } SPI_Mode;
    
    /* Used to track the state of the software state machine*/
    SPI_Mode SlaveMode = RX_REG_ADDRESS_MODE;
    
    /* The Register Address/Command to use*/
    uint8_t ReceiveRegAddr = 0;
    
    /* ReceiveBuffer: Buffer used to receive data in the ISR
     * RXByteCtr: Number of bytes left to receive
     * ReceiveIndex: The index of the next byte to be received in ReceiveBuffer
     * TransmitBuffer: Buffer used to transmit data in the ISR
     * TXByteCtr: Number of bytes left to transfer
     * TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer
     * */
    uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0};
    uint8_t RXByteCtr = 0;
    uint8_t ReceiveIndex = 0;
    uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0};
    uint8_t TXByteCtr = 0;
    uint8_t TransmitIndex = 0;
    
    /* Initialized the software state machine according to the received cmd
     *
     * cmd: The command/register address received
     * */
    void SPI_Slave_ProcessCMD(uint8_t cmd);
    
    /* The transaction between the slave and master is completed. Uses cmd
     * to do post transaction operations. (Place data from ReceiveBuffer
     * to the corresponding buffer based in the last received cmd)
     *
     * cmd: The command/register address corresponding to the completed
     * transaction
     */
    void SPI_Slave_TransactionDone(uint8_t cmd);
    void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count);
    void SendUCA0Data(uint8_t val);
    
    void SendUCA0Data(uint8_t val)
    {
        while (!(IFG2 & UCA0TXIFG));              // USCI_A0 TX buffer ready?
        UCA0TXBUF = val;
    }
    
    void SPI_Slave_ProcessCMD(uint8_t cmd)
    {
        ReceiveIndex = 0;
        TransmitIndex = 0;
        RXByteCtr = 0;
        TXByteCtr = 0;
    
        switch (cmd)
        {
            case (CMD_TYPE_0_SLAVE):                        //Send slave device id (This device's id)
                SlaveMode = TX_DATA_MODE;
                TXByteCtr = TYPE_0_LENGTH;
                //Fill out the TransmitBuffer
                CopyArray(SlaveType0, TransmitBuffer, TYPE_0_LENGTH);
                //Send First Byte
                SendUCA0Data(TransmitBuffer[TransmitIndex++]);
                TXByteCtr--;
                break;
            case (CMD_TYPE_1_SLAVE):                      //Send slave device time (This device's time)
                SlaveMode = TX_DATA_MODE;
                TXByteCtr = TYPE_1_LENGTH;
                //Fill out the TransmitBuffer
                CopyArray(SlaveType1, TransmitBuffer, TYPE_1_LENGTH);
                //Send First Byte
                SendUCA0Data(TransmitBuffer[TransmitIndex++]);
                TXByteCtr--;
                break;
            case (CMD_TYPE_2_SLAVE):                  //Send slave device location (This device's location)
                SlaveMode = TX_DATA_MODE;
                TXByteCtr = TYPE_2_LENGTH;
                //Fill out the TransmitBuffer
                CopyArray(SlaveType2, TransmitBuffer, TYPE_2_LENGTH);
                //Send First Byte
                SendUCA0Data(TransmitBuffer[TransmitIndex++]);
                TXByteCtr--;
                break;
            case (CMD_TYPE_0_MASTER):
                SlaveMode = RX_DATA_MODE;
                RXByteCtr = TYPE_0_LENGTH;
                break;
            case (CMD_TYPE_1_MASTER):
                SlaveMode = RX_DATA_MODE;
                RXByteCtr = TYPE_1_LENGTH;
                break;
            case (CMD_TYPE_2_MASTER):
                SlaveMode = RX_DATA_MODE;
                RXByteCtr = TYPE_2_LENGTH;
                break;
            default:
                __no_operation();
                break;
        }
    }
    
    
    void SPI_Slave_TransactionDone(uint8_t cmd)
    {
        switch (cmd)
        {
            case (CMD_TYPE_0_SLAVE):                        //Slave device id was sent(This device's id)
                break;
            case (CMD_TYPE_1_SLAVE):                      //Slave device time was sent(This device's time)
                break;
            case (CMD_TYPE_2_SLAVE):                  //Send slave device location (This device's location)
                break;
            case (CMD_TYPE_0_MASTER):
                CopyArray(ReceiveBuffer, MasterType0, TYPE_0_LENGTH);
                break;
            case (CMD_TYPE_1_MASTER):
                CopyArray(ReceiveBuffer, MasterType1, TYPE_1_LENGTH);
                break;
            case (CMD_TYPE_2_MASTER):
                CopyArray(ReceiveBuffer, MasterType2, TYPE_2_LENGTH);
                break;
            default:
                __no_operation();
                break;
        }
    }
    
    void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
    {
        uint8_t copyIndex = 0;
        for (copyIndex = 0; copyIndex < count; copyIndex++)
        {
            dest[copyIndex] = source[copyIndex];
        }
    }
    
    //******************************************************************************
    // Device Initialization *******************************************************
    //******************************************************************************
    
    void initClockTo16MHz()
    {
        if (CALBC1_16MHZ==0xFF)                  // If calibration constant erased
        {
            while(1);                               // do not load, trap CPU!!
        }
        DCOCTL = 0;                               // Select lowest DCOx and MODx settings
        BCSCTL1 = CALBC1_16MHZ;                    // Set DCO
        DCOCTL = CALDCO_16MHZ;
    }
    
    void initGPIO()
    {
      //SPI Pins
      P1SEL = BIT1 + BIT2 + BIT4;
      P1SEL2 = BIT1 + BIT2 + BIT4;
    
      //LEDs
      P1DIR |= BIT0 + BIT6;
      P1OUT &= ~(BIT0 + BIT6);
    }
    
    void initSPI()
    {
      UCA0CTL1 = UCSWRST;                       // **Put state machine in reset**
      UCA0CTL0 |= UCCKPL + UCMSB + UCSYNC;      // 3-pin, 8-bit SPI Slave
      UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
      IE2 |= UCA0RXIE;                          // Enable USCI0 RX interrupt
    
      SLAVE_CS_DIR &= ~(SLAVE_CS_PIN);
    }
    
    //******************************************************************************
    // Main ************************************************************************
    // Enters LPM0 and waits for SPI interrupts. The data sent from the master is  *
    // then interpreted and the device will respond accordingly                    *
    //******************************************************************************
    
    int main(void)
    {
      WDTCTL = WDTPW + WDTHOLD;                 // Stop watchdog timer
      while (!(P1IN & BIT4));                   // If clock sig from mstr stays low,
                                                // it is not yet in SPI mode
      initClockTo16MHz();
      initGPIO();
      initSPI();
    
      __bis_SR_register(LPM0_bits + GIE);       // Enter LPM4, enable interrupts
      __no_operation();
      return 0;
    }
    
    
    //******************************************************************************
    // SPI Interrupt ***************************************************************
    //******************************************************************************
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=USCIAB0RX_VECTOR
    __interrupt void USCI0RX_ISR (void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(USCIAB0RX_VECTOR))) USCI0RX_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
        if (IFG2 & UCA0RXIFG)
        {
            unsigned char uca0_rx_val = UCA0RXBUF;
            if (!(SLAVE_CS_IN & SLAVE_CS_PIN))
            {
                switch (SlaveMode)
                {
                      case (RX_REG_ADDRESS_MODE):
                          ReceiveRegAddr = uca0_rx_val;
                          SPI_Slave_ProcessCMD(ReceiveRegAddr);
                          break;
                      case (RX_DATA_MODE):
                          ReceiveBuffer[ReceiveIndex++] = uca0_rx_val;
                          RXByteCtr--;
                          if (RXByteCtr == 0)
                          {
                              //Done Receiving MSG
                              SlaveMode = RX_REG_ADDRESS_MODE;
                              SPI_Slave_TransactionDone(ReceiveRegAddr);
                          }
                          break;
                      case (TX_DATA_MODE):
                          if (TXByteCtr > 0)
                          {
                              SendUCA0Data(TransmitBuffer[TransmitIndex++]);
                              TXByteCtr--;
                          }
                          if (TXByteCtr == 0)
                          {
                              //Done Transmitting MSG
                              SlaveMode = RX_REG_ADDRESS_MODE;
                              SPI_Slave_TransactionDone(ReceiveRegAddr);
                          }
                          break;
                      default:
                          __no_operation();
                          break;
                }
            }
    
        }
    }
    

    //******************************************************************************
    //   MSP430G2xx3 Demo - USCI_A0, SPI 3-Wire Master multiple byte RX/TX
    //
    //   Description: SPI master communicates to SPI slave sending and receiving
    //   3 different messages of different length. SPI master will enter LPM0 mode
    //   while waiting for the messages to be sent/receiving using SPI interrupt.
    //   SPI Master will initially wait for a port interrupt in LPM0 mode before
    //   starting the SPI communication.
    //   ACLK = NA, MCLK = SMCLK = DCO 16MHz.
    //
    //
    //                   MSP430G2553
    //                 -----------------
    //            /|\ |             P2.0|-> Slave Chip Select (GPIO)
    //             |  |                 |
    //             ---|RST          P1.5|-> Slave Reset (GPIO)
    //                |                 |
    //                |             P1.2|-> Data Out (UCA0SIMO)
    //                |                 |
    //       Button ->|P1.3         P1.1|<- Data In (UCA0SOMI)
    //                |                 |
    //                |             P1.4|-> Serial Clock Out (UCA0CLK)
    //
    //   Nima Eskandari
    //   Texas Instruments Inc.
    //   April 2017
    //   Built with CCS V7.0
    //******************************************************************************
    
    #include <msp430.h>
    #include <stdint.h>
    
    //******************************************************************************
    // Example Commands ************************************************************
    //******************************************************************************
    
    #define DUMMY   0xFF
    
    #define SLAVE_CS_OUT    P2OUT
    #define SLAVE_CS_DIR    P2DIR
    #define SLAVE_CS_PIN    BIT0
    
    /* CMD_TYPE_X_SLAVE are example commands the master sends to the slave.
     * The slave will send example SlaveTypeX buffers in response.
     *
     * CMD_TYPE_X_MASTER are example commands the master sends to the slave.
     * The slave will initialize itself to receive MasterTypeX example buffers.
     * */
    
    #define CMD_TYPE_0_SLAVE              0
    #define CMD_TYPE_1_SLAVE              1
    #define CMD_TYPE_2_SLAVE              2
    
    #define CMD_TYPE_0_MASTER              3
    #define CMD_TYPE_1_MASTER              4
    #define CMD_TYPE_2_MASTER              5
    
    #define TYPE_0_LENGTH              1
    #define TYPE_1_LENGTH              2
    #define TYPE_2_LENGTH              6
    
    #define MAX_BUFFER_SIZE     20
    
    /* MasterTypeX are example buffers initialized in the master, they will be
     * sent by the master to the slave.
     * SlaveTypeX are example buffers initialized in the slave, they will be
     * sent by the slave to the master.
     * */
    
    uint8_t MasterType0 [TYPE_0_LENGTH] = {0x11};
    uint8_t MasterType1 [TYPE_1_LENGTH] = {8, 9};
    uint8_t MasterType2 [TYPE_2_LENGTH] = {'F', '4' , '1' , '9', '2', 'B'};
    
    uint8_t SlaveType2 [TYPE_2_LENGTH] = {0};
    uint8_t SlaveType1 [TYPE_1_LENGTH] = {0};
    uint8_t SlaveType0 [TYPE_0_LENGTH] = {0};
    
    //******************************************************************************
    // General SPI State Machine ***************************************************
    //******************************************************************************
    
    typedef enum SPI_ModeEnum{
        IDLE_MODE,
        TX_REG_ADDRESS_MODE,
        RX_REG_ADDRESS_MODE,
        TX_DATA_MODE,
        RX_DATA_MODE,
        TIMEOUT_MODE
    } SPI_Mode;
    
    /* Used to track the state of the software state machine*/
    SPI_Mode MasterMode = IDLE_MODE;
    
    /* The Register Address/Command to use*/
    uint8_t TransmitRegAddr = 0;
    
    /* ReceiveBuffer: Buffer used to receive data in the ISR
     * RXByteCtr: Number of bytes left to receive
     * ReceiveIndex: The index of the next byte to be received in ReceiveBuffer
     * TransmitBuffer: Buffer used to transmit data in the ISR
     * TXByteCtr: Number of bytes left to transfer
     * TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer
     * */
    uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0};
    uint8_t RXByteCtr = 0;
    uint8_t ReceiveIndex = 0;
    uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0};
    uint8_t TXByteCtr = 0;
    uint8_t TransmitIndex = 0;
    
    /* SPI Write and Read Functions */
    
    /* For slave device, writes the data specified in *reg_data
     *
     * reg_addr: The register or command to send to the slave.
     *           Example: CMD_TYPE_0_MASTER
     * *reg_data: The buffer to write
     *           Example: MasterType0
     * count: The length of *reg_data
     *           Example: TYPE_0_LENGTH
     *  */
    SPI_Mode SPI_Master_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count);
    
    /* For slave device, read the data specified in slaves reg_addr.
     * The received data is available in ReceiveBuffer
     *
     * reg_addr: The register or command to send to the slave.
     *           Example: CMD_TYPE_0_SLAVE
     * count: The length of data to read
     *           Example: TYPE_0_LENGTH
     *  */
    SPI_Mode SPI_Master_ReadReg(uint8_t reg_addr, uint8_t count);
    void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count);
    void SendUCA0Data(uint8_t val);
    
    void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
    {
        uint8_t copyIndex = 0;
        for (copyIndex = 0; copyIndex < count; copyIndex++)
        {
            dest[copyIndex] = source[copyIndex];
        }
    }
    
    
    SPI_Mode SPI_Master_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
    {
        MasterMode = TX_REG_ADDRESS_MODE;
        TransmitRegAddr = reg_addr;
    
        //Copy register data to TransmitBuffer
        CopyArray(reg_data, TransmitBuffer, count);
    
        TXByteCtr = count;
        RXByteCtr = 0;
        ReceiveIndex = 0;
        TransmitIndex = 0;
    
        SLAVE_CS_OUT &= ~(SLAVE_CS_PIN);
        SendUCA0Data(TransmitRegAddr);
    
        __bis_SR_register(CPUOFF + GIE);              // Enter LPM0 w/ interrupts
    
        SLAVE_CS_OUT |= SLAVE_CS_PIN;
        return MasterMode;
    }
    
    SPI_Mode SPI_Master_ReadReg(uint8_t reg_addr, uint8_t count)
    {
        MasterMode = TX_REG_ADDRESS_MODE;
        TransmitRegAddr = reg_addr;
        RXByteCtr = count;
        TXByteCtr = 0;
        ReceiveIndex = 0;
        TransmitIndex = 0;
    
        SLAVE_CS_OUT &= ~(SLAVE_CS_PIN);
        SendUCA0Data(TransmitRegAddr);
    
        __bis_SR_register(CPUOFF + GIE);              // Enter LPM0 w/ interrupts
    
        SLAVE_CS_OUT |= SLAVE_CS_PIN;
        return MasterMode;
    }
    
    void SendUCA0Data(uint8_t val)
    {
        while (!(IFG2 & UCA0TXIFG));              // USCI_A0 TX buffer ready?
        UCA0TXBUF = val;
    }
    
    //******************************************************************************
    // Device Initialization *******************************************************
    //******************************************************************************
    
    void initClockTo16MHz()
    {
        if (CALBC1_16MHZ==0xFF)                  // If calibration constant erased
        {
            while(1);                               // do not load, trap CPU!!
        }
        DCOCTL = 0;                               // Select lowest DCOx and MODx settings
        BCSCTL1 = CALBC1_16MHZ;                    // Set DCO
        DCOCTL = CALDCO_16MHZ;
    }
    
    void initGPIO()
    {
      //LEDs
      P1OUT = 0x00;                             // P1 setup for LED & reset output
      P1DIR |= BIT0 + BIT5 + BIT6;
    
      //SPI Pins
      P1SEL = BIT1 + BIT2 + BIT4;
      P1SEL2 = BIT1 + BIT2 + BIT4;
    
      //Button to initiate transfer
      P1DIR &= ~(BIT3);
      P1OUT |= BIT3;                            // P1.3 pull up
      P1REN |= BIT3;                            // P1.3 pull up/down resistor enable
      P1IE  |= BIT3;                            // P1.3 interrupt enabled
      P1IES |= BIT3;                            // P1.3 Hi/lo edge
      P1IFG &= ~BIT3;                           // P1.3 IFG cleared
    }
    
    void initSPI()
    {
      //Clock Polarity: The inactive state is high
      //MSB First, 8-bit, Master, 3-pin mode, Synchronous
      UCA0CTL0 |= UCCKPL + UCMSB + UCMST + UCSYNC;
      UCA0CTL1 |= UCSSEL_2;                     // SMCLK
      UCA0BR0 |= 0x20;                          // /2
      UCA0BR1 = 0;                              //
      UCA0MCTL = 0;                             // No modulation must be cleared for SPI
      UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
      IE2 |= UCA0RXIE;                          // Enable USCI0 RX interrupt
    
      SLAVE_CS_DIR |= SLAVE_CS_PIN;
      SLAVE_CS_OUT |= SLAVE_CS_PIN;
    
    }
    
    //******************************************************************************
    // Main ************************************************************************
    // Send and receive three messages containing the example commands *************
    //******************************************************************************
    
    int main(void)
    {
      WDTCTL = WDTPW + WDTHOLD;                 // Stop watchdog timer
    
      initClockTo16MHz();
      initGPIO();
      initSPI();
    
      P1OUT &= ~BIT5;                           // Now with SPI signals initialized,
      __delay_cycles(100000);
      P1OUT |= BIT5;                            // reset slave
      __delay_cycles(100000);                   // Wait for slave to initialize
    
      P1OUT |= BIT0;
    
      __bis_SR_register(LPM0_bits + GIE);       // CPU off, enable interrupts
    
      SPI_Master_ReadReg(CMD_TYPE_2_SLAVE, TYPE_2_LENGTH);
      CopyArray(ReceiveBuffer, SlaveType2, TYPE_2_LENGTH);
    
      SPI_Master_ReadReg(CMD_TYPE_1_SLAVE, TYPE_1_LENGTH);
      CopyArray(ReceiveBuffer, SlaveType1, TYPE_1_LENGTH);
    
      SPI_Master_ReadReg(CMD_TYPE_0_SLAVE, TYPE_0_LENGTH);
      CopyArray(ReceiveBuffer, SlaveType0, TYPE_0_LENGTH);
    
      SPI_Master_WriteReg(CMD_TYPE_2_MASTER, MasterType2, TYPE_2_LENGTH);
      SPI_Master_WriteReg(CMD_TYPE_1_MASTER, MasterType1, TYPE_1_LENGTH);
      SPI_Master_WriteReg(CMD_TYPE_0_MASTER, MasterType0, TYPE_0_LENGTH);
      __bis_SR_register(LPM0_bits + GIE);
    }
    
    //******************************************************************************
    // SPI Interrupt ***************************************************************
    //******************************************************************************
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=USCIAB0RX_VECTOR
    __interrupt void USCIA0RX_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(USCIAB0RX_VECTOR))) USCIA0RX_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
        if (IFG2 & UCA0RXIFG)
        {
            uint8_t uca0_rx_val = UCA0RXBUF;
            switch (MasterMode)
            {
                case TX_REG_ADDRESS_MODE:
                    if (RXByteCtr)
                    {
                        MasterMode = RX_DATA_MODE;   // Need to start receiving now
                        //Send Dummy To Start
                        __delay_cycles(2000);
                        SendUCA0Data(DUMMY);
                    }
                    else
                    {
                        MasterMode = TX_DATA_MODE;        // Continue to transmision with the data in Transmit Buffer
                        //Send First
                        SendUCA0Data(TransmitBuffer[TransmitIndex++]);
                        TXByteCtr--;
                    }
                    break;
    
                case TX_DATA_MODE:
                    if (TXByteCtr)
                    {
                      SendUCA0Data(TransmitBuffer[TransmitIndex++]);
                      TXByteCtr--;
                    }
                    else
                    {
                      //Done with transmission
                      MasterMode = IDLE_MODE;
                      __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
                    }
                    break;
    
                case RX_DATA_MODE:
                    if (RXByteCtr)
                    {
                        ReceiveBuffer[ReceiveIndex++] = uca0_rx_val;
                        //Transmit a dummy
                        RXByteCtr--;
                    }
                    if (RXByteCtr == 0)
                    {
                        MasterMode = IDLE_MODE;
                        __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
                    }
                    else
                    {
                        SendUCA0Data(DUMMY);
                    }
                    break;
    
                default:
                    __no_operation();
                    break;
            }
            __delay_cycles(50);
        }
    }
    
    
    //******************************************************************************
    // PORT1 Interrupt *************************************************************
    // Interrupt occurs on button press and initiates the SPI data transfer ********
    //******************************************************************************
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=PORT1_VECTOR
    __interrupt void Port_1(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(PORT1_VECTOR))) Port_1 (void)
    #else
    #error Compiler not supported!
    #endif
    {
        P1OUT |= BIT6;
        P1IFG &= ~BIT3;                           // P1.3 IFG cleared
        P1IE &= ~BIT3;
        //Initiate
        __bic_SR_register_on_exit(LPM0_bits);      // Exit LPM0
    }