您好,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问您JP1 JP2是如何连接的?您是如何供电的?另外您的图片有些模糊,我无法看清您的设置。
JP1 OFF 5V circuitry is not used. Provides power to AFE circuitry. Can be used for power measurement.
JP2 3.3VTX Enables 3.3-V circuitry. 5-V circuitry is not used
不知您是否参考下面的文档

在4 AFE Configuration 中有相关描述
对于AFE电路的供电:To use the same voltage source as the MCU, set JP3. To use an external voltage source, remove the jumper from JP3 and apply voltage to TP1 (V+) and TP2 (GND)
4.3 5-V Enable
The AFE includes a DC/DC step-up converter to enable 5-V TX voltage. To enable the step up converter, set JP1. For 5-V operation, also set JP2 for 5-V operation