This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问是否有FFT.c的类似注释文件(或设计文件)

Other Parts Discussed in Thread: MSP430FR5994, MSP430F149, MSP430F5438A

大家好:

    我们购买了M430F5438A几套开发板,希望进行FFT的开发, 但当使用TI提供的MSP-EXP430F5438_User_Expertience(slac2271)时,看到5438UE_1_52_00/src/UserExperienceDemo/FFT.c, 我们希望采用的正弦信号(频率:1545HZ; 相位:0; 幅值:100mv)。

    可以通过修改FFT.c实现吗?(例如:通过修改bit_rev_index[]的内容)

  • 请参考附件

    /*******************************************************************************
     *
     *  FFT.c
     *
     *  Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/
     *
     *  Redistribution and use in source and binary forms, with or without
     *  modification, are permitted provided that the following conditions
     *  are met:
     *
     *    Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     *    Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the
     *    distribution.
     *
     *    Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
     *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
     *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
     *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
     *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
     *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
     *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
     *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
     *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
     *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     ******************************************************************************/
    
    #include "msp430.h"
    #include "hal_MSP-EXP430F5438.h"
    #include "UserExperience_F5438A.h"
    #include "FFT.h"
    #include "FFT_430.h"
    
    int FBuff[512], outer;
    unsigned short index1;
    
    unsigned int voice_data[1024];
    unsigned int index;
    const int bit_rev_index[] = {0x00, 0x80, 0x40, 0xC0, 0x20, 0xA0, 0x60, 0xE0, 0x10, 0x90, 0x50,
                                 0xD0, 0x30, 0xB0, 0x70, 0xF0, 0x08, 0x88, 0x48, 0xC8, 0x28, 0xA8,
                                 0x68, 0xE8, 0x18, 0x98, 0x58, 0xD8, 0x38, 0xB8, 0x78, 0xF8, 0x04,
                                 0x84, 0x44, 0xC4, 0x24, 0xA4, 0x64, 0xE4, 0x14, 0x94, 0x54, 0xD4,
                                 0x34, 0xB4, 0x74, 0xF4, 0x0C, 0x8C, 0x4C, 0xCC, 0x2C, 0xAC, 0x6C,
                                 0xEC, 0x1C, 0x9C, 0x5C, 0xDC, 0x3C, 0xBC, 0x7C, 0xFC, 0x02, 0x82,
                                 0x42, 0xC2, 0x22, 0xA2, 0x62, 0xE2, 0x12, 0x92, 0x52, 0xD2, 0x32,
                                 0xB2, 0x72, 0xF2, 0x0A, 0x8A, 0x4A, 0xCA, 0x2A, 0xAA, 0x6A, 0xEA,
                                 0x1A, 0x9A, 0x5A, 0xDA, 0x3A, 0xBA, 0x7A, 0xFA, 0x06, 0x86, 0x46,
                                 0xC6, 0x26, 0xA6, 0x66, 0xE6, 0x16, 0x96, 0x56, 0xD6, 0x36, 0xB6,
                                 0x76, 0xF6, 0x0E, 0x8E, 0x4E, 0xCE, 0x2E, 0xAE, 0x6E, 0xEE, 0x1E,
                                 0x9E, 0x5E, 0xDE, 0x3E, 0xBE, 0x7E, 0xFE, 0x01, 0x81, 0x41, 0xC1,
                                 0x21, 0xA1, 0x61, 0xE1, 0x11, 0x91, 0x51, 0xD1, 0x31, 0xB1, 0x71,
                                 0xF1, 0x09, 0x89, 0x49, 0xC9, 0x29, 0xA9, 0x69, 0xE9, 0x19, 0x99,
                                 0x59, 0xD9, 0x39, 0xB9, 0x79, 0xF9, 0x05, 0x85, 0x45, 0xC5, 0x25,
                                 0xA5, 0x65, 0xE5, 0x15, 0x95, 0x55, 0xD5, 0x35, 0xB5, 0x75, 0xF5,
                                 0x0D, 0x8D, 0x4D, 0xCD, 0x2D, 0xAD, 0x6D, 0xED, 0x1D, 0x9D, 0x5D,
                                 0xDD, 0x3D, 0xBD, 0x7D, 0xFD, 0x03, 0x83, 0x43, 0xC3, 0x23, 0xA3,
                                 0x63, 0xE3, 0x13, 0x93, 0x53, 0xD3, 0x33, 0xB3, 0x73, 0xF3, 0x0B,
                                 0x8B, 0x4B, 0xCB, 0x2B, 0xAB, 0x6B, 0xEB, 0x1B, 0x9B, 0x5B, 0xDB,
                                 0x3B, 0xBB, 0x7B, 0xFB, 0x07, 0x87, 0x47, 0xC7, 0x27, 0xA7, 0x67,
                                 0xE7, 0x17, 0x97, 0x57, 0xD7, 0x37, 0xB7, 0x77, 0xF7, 0x0F, 0x8F,
                                 0x4F, 0xCF, 0x2F, 0xAF, 0x6F, 0xEF, 0x1F, 0x9F, 0x5F, 0xDF, 0x3F,
                                 0xBF, 0x7F, 0xFF};
    
    
    int imag, real, real_abs, imag_abs, mag, max, min;
    int FFT_data[512];
    
    unsigned int FFT_Image[1344];
    
    /**********************************************************************//**
     * @brief  Sets up board for recording from microphone
     *
     * @param  none
     *
     * @return none
     *************************************************************************/
    
    void shutdownRecorder(void)
    {
        halLcdSetBackLight(lcdBackLightLevelSettingLOCAL);
    
        // Power-down MSP430 modules
        TBCTL = 0;                        // Disable Timer_B
        ADC12CTL1 &= ~ADC12CONSEQ_2;      // Stop conversion immediately
        ADC12CTL0 &= ~ADC12ENC;           // Disable ADC12 conversion
        ADC12CTL0 = 0x00;                 // Switch off ADC12
        ADC12IE = 0x00;
    
        AUDIO_PORT_OUT &= ~MIC_POWER_PIN; // Turn of MIC
        AUDIO_PORT_SEL &= ~MIC_INPUT_PIN;
    }
    
    void setupRecorder()
    {
        AUDIO_PORT_OUT |= MIC_POWER_PIN;
        AUDIO_PORT_OUT &= ~MIC_INPUT_PIN;
        AUDIO_PORT_SEL |= MIC_INPUT_PIN;
    
        UCSCTL8 |= MODOSCREQEN;
        ADC12CTL0 &= ~ADC12ENC;           // Disable conversions to configure ADC12
        ADC12CTL0 = ADC12ON + ADC12SHT02; // Configure ADC12 to sample a sequence of channels, once
        ADC12CTL1 = ADC12SHP + ADC12CONSEQ_2 + ADC12SSEL_2 + ADC12SHS_3;
        ADC12CTL2 = ADC12RES_0;           // Select 8-bit resolution
        ADC12MCTL0 = MIC_INPUT_CHAN | ADC12EOS;
        ADC12CTL0 |= ADC12ENC;            // Enable
        ADC12IE = BIT0;
    
        // Initialize Timer_B to be used as ADC12 trigger
        TBCTL = TBSSEL_2 + TBCLR;         // Use SMCLK as Timer_B source
        TBCCR0 = 2047;                    // Initialize TBCCR0 (period register)
        TBCCR1 = 2047 - 100;              // Initialize TBCCR1 (ADC12 trigger)
        TBCCTL0 = 0x0000;
        TBCCTL1 = OUTMOD_7;
        TBCCTL2 = 0x0000;
        TBCCTL3 = 0x0000;
        TBCCTL4 = 0x0000;
        TBCCTL5 = 0x0000;
        TBCCTL6 = 0x0000;
    }
    
    /**********************************************************************//**
     * @brief  Runs the FFT app. Performs the FFT and displays it to the screen.
     *
     * @param  none
     *
     * @return none
     *************************************************************************/
    
    void FFTrecorder(void)
    {
        unsigned int i, j;
        unsigned int mask = 0x0000;
    
        fftISR = 1;
    
        // Initialize FFT variables
        buf_index = 0;
        for (i = 0; i < 1344; i++){
            FFT_Image[i] = 0x0000;
        }
    
        halLcdClearScreen();
        halLcdPrintLine("    FFT DEMO   ", 0, 0);
        halLcdPrintLine("0", 8, 0);
        halLcdPrintLineCol("Fs 2", 8, 13, 0);
        halLcdLine(120, 107, 126, 97, PIXEL_ON);
        halLcdHLine(0, 138, 96, PIXEL_ON);
    
        halButtonsInit(BUTTON_ALL);
        halButtonsInterruptEnable(BUTTON_ALL);
        buttonsPressed = 0;
    
        setupRecorder();
    
        while (!buttonsPressed)
        {
            TBCCTL1 &= ~CCIFG;
            TBCTL |= MC0;   //start timer B
            __bis_SR_register(LPM0_bits + GIE);
            __no_operation();
            TBCTL &= ~MC0;
    
            if (buf_index == 512)
                for (i = 0; i < 512; i++)
                    voice_data[i] = buffer[i];
            else
                for (i = 0; i < 512; i++)
                    voice_data[i] = buffer[i + 512];
    
            FFT_prog();     // Perform FFT and store
    
            for (i = 0; i < 256; i++)
            {
                index = bit_rev_index[i];
                real = FBuff[2 * index];
                imag = FBuff[2 * index + 1];
                if (real < 0)
                    real_abs = ~real + 1;
                else
                    real_abs = real;
                if (imag < 0)
                    imag_abs = ~imag + 1;
                else
                    imag_abs = imag;
                if (real_abs >= imag_abs)
                {
                    max = real_abs;
                    min = imag_abs;
                }
                else
                {
                    max = imag_abs;
                    min = real_abs;
                }
                mag = max + 3 * (min >> 3);
                FFT_data[i] = mag;
            }
    
            //prepare the image of the FFT for display
            for (i = 1; i < 128; i++)
            {
                switch (i % 8)
                {
                    case 1: mask = 0x0003; break;
                    case 2: mask = 0x000C; break;
                    case 3: mask = 0x0030; break;
                    case 4: mask = 0x00C0; break;
                    case 5: mask = 0x0300; break;
                    case 6: mask = 0x0C00; break;
                    case 7: mask = 0x3000; break;
                    case 0: mask = 0xC000; break;
                    default: mask = 0x0000; break;
                }
                for (j = 0; j < 84; j++)
                {
                    if (j < (84 - FFT_data[i] * 2))
                        FFT_Image[((i - 1) / 8) + j * 16] &= ~mask;
                    else
                        FFT_Image[((i - 1) / 8) + j * 16] |= mask;
                }
            }
            halLcdImage(FFT_Image, 16, 84, 1, 12); //display the image
        }
        fftISR = 0;
        shutdownRecorder();
    }
    
    

  • 您可以下载 www.ti.com/.../MSP-DSPLIB 并参考链接

    software-dl.ti.com/.../transform_ex1_fft_fixed_q15_8c-example.html

    This example demonstrates how to use the msp_fir_q15 API and circular buffer feature to filter 16-bit input data. The input signal is composed of two generated sinusoidal signals added together, one sinusoid with a frequency that will pass though the filter and one with a frequency that will be filtered out. The inputs are copied into a circular buffer with twice the length of the filter and allows input history from previous filter operations to be reused without allocating and copying additional samples to the start of the input data. The generated input and result can be compared to see the effect of the filter.

    如果您要使用FFT ,建议您选择MSP430FR5994会更好。由于MSP430FR5994具有LEA,将以较低的能量使FFT更快。
  • 谢谢!

    我将在MSP430F5438A开发板和MSP430F149开发板上尝试.....

  • 期待您的反馈!

  • 现问题如下:

       我们希望在MSP430F149开发板上使用IAR运行“transform_ex1_fft_fixed_q15”

           编译报错如下:“Error[Pe020]: identifier "TIMER_A0_BASE" is undefined D:\Project\Code\FFT_Code\main.c 871“

           根据文件目录提示,我们修了“C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\430\inc\msp430f149.h”

                     "#if 1
                      #define __MSP430_BASEADDRESS_T0A5__ TACTL
                      #define TIMER_A0_BASE __MSP430_BASEADDRESS_T0A5__
                      #endif"

           2个问题:

          1). 真正运行编译链接时,msp430f149.h却没有改,我们应该修改哪个文件?

           2) “TIMER_A0_BASE“ 的定义在msp430f149.h里需要被改进吗?

                           

  • msp430f149是比较早的msp430型号了。他的内部功能模块和msp430f5438A还是有差别的。
    比如楼主说的TIMER_A0,msp430f149内部的定时器是Timer_A3和Timer_B7,在功能和寄存器名称上都是有差别的。如果想运行在msp430f149上,是需要移植的。
  • 谢谢回答的问题2!(我用的是Timer_A3)

    哪位能帮看一下问题1吗? (“根据文件目录提示,我们修改了“C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\430\inc\msp430f149.h””; 但IAR真正运行编译链接时,msp430f149.h却没有改,

    我们应该修改哪个文件?我们修改错了吗?

    修改的内容如下:

                      " #if 1
                        #define __MSP430_BASEADDRESS_T0A5__ TACTL
                        #define TIMER_A0_BASE __MSP430_BASEADDRESS_T0A5__
                       #endif "

  • 是的,修改错了。msp430f149.h文件是由官方或者开发环境提供的和msp430f149器件硬件寄存器相关的文件,我们不要修改。
    要修改UserExperienceDemo文件夹下的文件。
    还有就是例程中用的msp430f5438A,如果改成其他msp430,需要修改工程配置等
  • Susan, 您好:

        现我们希望用MSP430F149开发板(公司旧开发板)运行FFT(transform_ex1_fft_fixed_q15.c为基础的DSP库包),现在程序只能运行在MSP430F5438A开发板上,您看我们怎样使transform_ex1_fft_fixed_q15.c运行在MSP430F149开发板呢?

  • 如之前楼上 灰小子 所说,您是需要进行程序移植的

    这两款差别有些大,需要对照后针对不同模块具体移植