This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问M430F5438A开发板如何实现AD信号的多路单次运行

大家好:

    我们购买了M430F5438A几套开发板,希望进行FFT的开发!

    采用两路正弦信号:    a). 频率:1500HZ; 相位:0; 幅值:1V, 信号连接到P6.7,A7 ADC输入;

                                      b). 频率:1500HZ; 相位:35度; 幅值:10mV,信号输入端口MIC(M1)信号连接到P6.5,A5 ADC输入----内含运算放大器;

    现初始化程序如下:

         P6OUT |= MIC_POWER_PIN + 0x80;

         P6DIR &= ~(MIC_INPUT_PIN + 0x80);
         P6SEL |= MIC_INPUT_PIN + 0x80;

         UCSCTL8 |= MODOSCREQEN;
         ADC12CTL0 &= ~ADC12ENC; // Disable conversions to configure ADC12

         ADC12CTL0 = ADC12ON + ADC12SHT02 ; // Configure ADC12 to sample a sequence of channels, once
         ADC12CTL1 = ADC12SHP + ADC12CONSEQ_3 + ADC12SSEL_2 + ADC12SHS_3 + ADC12MEM1 + ADC12MEM0 ;

         ADC12CTL2 = ADC12RES_2; // Select 12-bit resolution
        ADC12MCTL0 = MIC_INPUT_CHAN;
        ADC12MCTL1 = ADC12INCH_7 | ADC12EOS;

       ADC12CTL0 |= ADC12ENC; // Enable

       ADC12IE = BIT0 + 0x80;

       // Initialize Timer_B to be used as ADC12 trigger
       TBCTL = TBSSEL_2 + TBCLR; // Use SMCLK as Timer_B source
       TBCCR0 = 2047; // Initialize TBCCR0 (period register)
       TBCCR1 = 2047 - 100; // Initialize TBCCR1 (ADC12 trigger)
       TBCCTL0 = 0x0000;
       TBCCTL1 = OUTMOD_7;
       TBCCTL2 = 0x0000;
       TBCCTL3 = 0x0000;
       TBCCTL4 = 0x0000;
       TBCCTL5 = 0x0000;
       TBCCTL6 = 0x0000;

       现ADC12CTL1 = ADC12SHP + ADC12CONSEQ_3 + ADC12SSEL_2 + ADC12SHS_3 + ADC12MEM1 + ADC12MEM0 时会死机,

       是ADC12CONSEQ_3的问题吗?该如何实现AD信号的多路单次运行?

  • 多路单次的话,一般是序列采样。也可以参考我之前回复的其他贴

    https://e2echina.ti.com/question_answer/microcontrollers/msp430/f/55/p/189444/581153#581153

    您可以参考下面的例程

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2012, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     * 
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //  MSP430F543xA Demo - ADC12_A, Sequence of Conversions (non-repeated)
    //
    //  Description: This example shows how to perform A/D conversions on a sequence
    //  of channels. A single sequence of conversions is performed - one conversion
    //  each on channels A0, A1, A2, and A3. Each conversion uses AVcc and AVss for
    //  the references. The conversion results are stored in ADC12MEM0, ADC12MEM1,
    //  ADC12MEM2, and ADC12MEM3 respectively and are moved to 'results[]' upon
    //  completion of the sequence. Test by applying voltages to pins A0, A1, A2,
    //  and A3, then setting and running to a break point at the "_BIC..."
    //  instruction in the ISR. To view the conversion results, open a watch window
    //  in debugger and view 'results' or view ADC12MEM0, ADC12MEM1, ADC12MEM2, and
    //  ADC12MEM3 in an ADC12 SFR window.
    //  This can run even in LPM4 mode as ADC has its own clock
    //  Note that a sequence has no restrictions on which channels are converted.
    //  For example, a valid sequence could be A0, A3, A2, A4, A2, A1, A0, and A7.
    //  See the 5xx User's Guide for instructions on using the ADC12.
    //
    //                MSP430F5438A
    //             -----------------
    //         /|\|                 |
    //          | |                 |
    //          --|RST              |
    //            |                 |
    //    Vin0 -->|P6.0/A0          |
    //    Vin1 -->|P6.1/A1          |
    //    Vin2 -->|P6.2/A2          |
    //    Vin3 -->|P6.3/A3          |
    //            |                 |
    //
    //   M Morales
    //   Texas Instruments Inc.
    //   June 2009
    //   Built with CCE Version: 3.2.2 and IAR Embedded Workbench Version: 4.11B
    //******************************************************************************
    
    #include <msp430.h>
    
    volatile unsigned int results[4];           // Needs to be global in this example
                                                // Otherwise, the compiler removes it
                                                // because it is not used for anything.
    
    int main(void)
    {
      WDTCTL = WDTPW+WDTHOLD;                   // Stop watchdog timer
      
      P6SEL = 0x0F;                             // Enable A/D channel inputs
      
      /* Initialize ADC12_A */ 
      ADC12CTL0 = ADC12ON+ADC12MSC+ADC12SHT0_2; // Turn on ADC12, set sampling time
      ADC12CTL1 = ADC12SHP+ADC12CONSEQ_1;       // Use sampling timer, single sequence
      ADC12MCTL0 = ADC12INCH_0;                 // ref+=AVcc, channel = A0
      ADC12MCTL1 = ADC12INCH_1;                 // ref+=AVcc, channel = A1
      ADC12MCTL2 = ADC12INCH_2;                 // ref+=AVcc, channel = A2
      ADC12MCTL3 = ADC12INCH_3+ADC12EOS;        // ref+=AVcc, channel = A3, end seq.
      ADC12IE = 0x08;                           // Enable ADC12IFG.3
      ADC12CTL0 |= ADC12ENC;                    // Enable conversions
    
      while(1)
      {
        ADC12CTL0 |= ADC12SC;                   // Start convn - software trigger
        
        __bis_SR_register(LPM4_bits + GIE);     // Enter LPM4, Enable interrupts
        __no_operation();                       // For debugger    
      }
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=ADC12_VECTOR
    __interrupt void ADC12ISR (void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      switch(__even_in_range(ADC12IV,34))
      {
      case  0: break;                           // Vector  0:  No interrupt
      case  2: break;                           // Vector  2:  ADC overflow
      case  4: break;                           // Vector  4:  ADC timing overflow
      case  6: break;                           // Vector  6:  ADC12IFG0
      case  8: break;                           // Vector  8:  ADC12IFG1
      case 10: break;                           // Vector 10:  ADC12IFG2
      case 12:                                  // Vector 12:  ADC12IFG3
        results[0] = ADC12MEM0;                 // Move results, IFG is cleared
        results[1] = ADC12MEM1;                 // Move results, IFG is cleared
        results[2] = ADC12MEM2;                 // Move results, IFG is cleared
        results[3] = ADC12MEM3;                 // Move results, IFG is cleared
        __bic_SR_register_on_exit(LPM4_bits);   // Exit active CPU, SET BREAKPOINT HERE  
      case 14: break;                           // Vector 14:  ADC12IFG4
      case 16: break;                           // Vector 16:  ADC12IFG5
      case 18: break;                           // Vector 18:  ADC12IFG6
      case 20: break;                           // Vector 20:  ADC12IFG7
      case 22: break;                           // Vector 22:  ADC12IFG8
      case 24: break;                           // Vector 24:  ADC12IFG9
      case 26: break;                           // Vector 26:  ADC12IFG10
      case 28: break;                           // Vector 28:  ADC12IFG11
      case 30: break;                           // Vector 30:  ADC12IFG12
      case 32: break;                           // Vector 32:  ADC12IFG13
      case 34: break;                           // Vector 34:  ADC12IFG14
      default: break; 
      }
    }