This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI_SETDCO MSPAFE253几个芯片出来的频率差异很大

Other Parts Discussed in Thread: MSP430AFE253

为了保证我一批产品UART波特率的一致性,我使用了 DCO_Library.s43 的库 函数,代码在下面,但是测试下来,3块板子,一个SMCLK 输出1.93M ,一个1.66M 一个1.87M  UART口根本没办法配置才能保证3个板子UART都出9600的波特率,请问一下,我程序哪里不对么,


  WDTCTL = WDTPW + WDTHOLD;
  Init_Clk();  
  Init_IO();   
//  BCSCTL3 = LFXT1S1;
//  P1DIR |= 0x1; // P1.1 and P1.4 outputs
//  P1SEL |= 0x01;//P1.4 SMCLK output
//  P1SEL2= 0x01;// P1.4 SMCLK output  

  Delay_ms(100);
  
  result = TI_SetDCO(TI_DCO_5MHZ);
  
  if( result == TI_DCO_SET_TO_SLOWEST ) // returned result if DCO registers hit min
  {
  while(1); // trap the CPU if hit
  }
  else if( result == TI_DCO_SET_TO_FASTEST ) // returned result if DCO registers hit max
  {
  while(1); // trap the CPU if hit
  }
  else if( result == TI_DCO_TIMEOUT_ERROR ) // result if DCO takes >10000 loops
  {
  while(1); // trap the CPU if hit
  }  
  
  Init_Uart();


//****************************************************
//Shanghai GanKun Co., Ltd.
//designed  by hank
//Main fuction
//****************************************************
void Init_Clk(void)
{
  
//  DCOCTL = DCO0 + DCO1 ;              // DCO  = 3
//  BCSCTL1 = XT2OFF + RSEL2 + RSEL3 ;          //  RSEL= 12   CLK = 5.8MHZ   XT2 OFF
  DCOCTL = DCO0 + DCO1  + DCO2 ;              // DCO  = 3
  BCSCTL1 = XT2OFF + RSEL0  + RSEL1  + RSEL2 + RSEL3 ;          //  RSEL= 12   CLK = 5.8MHZ   XT2 OFF
  
  
  BCSCTL2 = 0;                          // SMCLK = DCO   MCL = DCO
  BCSCTL3 =LFXT1S1;            //LFXT = VLOCLK  
   
}

//****************************************************
//Shanghai GanKun Co., Ltd.
//designed  by hank
//Main fuction
//****************************************************
void Init_IO(void)
{
    P1DIR =BIT0+BIT3+BIT4;
    P1REN = 0;
    P1SEL = BIT0+ BIT3+BIT4;                       // P1.3,P1.4 = USART0 TXD/RXD   
    P1SEL2 = BIT0;
   
    P2DIR = 0X01;
    P2REN = 0X00;
    P2SEL = 0X00;   
    P2SEL2 = 0X00;      
   
    P2OUT = 0x00;

    SET_RS485_READ;   
   
}

x 出现错误。请重试或与管理员联系。