This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6043上是否支持直径为0.8米的管道气体测量

Other Parts Discussed in Thread: EVM430-FR6043

您好,我现在用EVM430-FR6043板和2个200KHZ的换能器进行测试,当换能器距离大于15CM时就采集不到信号了,换做5V驱动后,只能增加1-2CM,测量距离不能再增加了。

请问:EVM430-FR6043是否支持直径为0.8米的管道气体测量?如果换能器插入角为30度,两个超声波传感器的距离约1米,这时,EVM430-FR6043能提供测量吗?并气体流速范围是多少?   那么应该采用多少V P-P的驱动源,功率多少?

  • 已经assign给了相关的专家,之后会给您回复
  • 您好,

    我们EVM430-FR6043板子上只支持3.3V和5V的换能器,一般两个换能器距离最大也就是在15cm左右,因为超声在气体中传播衰减比较大,而且频率越大,衰减越快。您所描述的两个换能器间距1m测量,这个我们是不支持的,可能需要您自己对信号进行放大,我们没有做过这一块的测试。
    对于气体流速范围,这个我们是通过计算绝对飞行时间和相对飞行时间来计量的,可以测量到很低/很高的气体流速。具体的技术资料可以参考:www.ti.com/.../slaa889.pdf

    Update some information :

    问一下您是做哪种大口径气表? 常压下还是中压(比如0.5MP),或者高压?

    常压下很难做到,一般需要200V甚至更高的才能正常传输那么远的距离,0.5Mp的话,信号应该还可以,放大到12V情况下应该会更好。高压下的话应该3.3V/5V就可以直接驱动同时检测到不错的波形。


    Best Regards
    Johnson

  • 感谢您的答复,我们是做管道气体流量表,压力3-8MP。我也看到了其他的高压驱动方案,为了方便快速应用,是想采用TI此类成熟远距离检测的应用方案,谢谢,
  • 您好,

    根据您的描述 在3-8MP下应该是可以正常接收到波形的。您现在的测试应该是在一个大气压下测的 因此得不到波形数据。建议您可以在实际3-8MPa环境下进行测试。

    Best Regards

    Johnson

  • 是的,我现在的大气压下测试的,我准备好后在试验台上测试下,谢谢