问题1:我现在用USS软件调试开发板EVM-MSP430FR6047,请问如何设置换能器激励脉冲频率到200K和500K。我设置了一下,软件最低只能到772K.不知道该如何操作,看说明文档里,MSP430FR6047最低可以设置到33K的.
问题2:驱动换能器的参考设计有没有高电压的,我现在的换能器需要100多V的电压激励,并且需要做隔离,有没有相应的参考设计
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题1:我现在用USS软件调试开发板EVM-MSP430FR6047,请问如何设置换能器激励脉冲频率到200K和500K。我设置了一下,软件最低只能到772K.不知道该如何操作,看说明文档里,MSP430FR6047最低可以设置到33K的.
问题2:驱动换能器的参考设计有没有高电压的,我现在的换能器需要100多V的电压激励,并且需要做隔离,有没有相应的参考设计
您好,
For Q1:
你可以在下面的User's Guide中看到,我们GUI上在水表模式下,配置激励换能器频率最低是772K,最高是2500K。
问一下,对于水表的设计,一般换能器使用的是100KHz的,对于200KHz,500KHz换能器一般使用FR6043去做。你们使用FR6047是做哪一个应用呢?
For Q2:
我们有把电压放大到+-12V去驱动换能器的参考设计:
www.ti.com/.../TIDA-01486
Best Regards
Johnson