MSP430F2274利用CC2500模块进行无线发送的时候,通过msg数组进行发送温度和电压数据,我这边想在msg数组多增加一组内容 ,多发送一个电压数据,但始终第三组电压数据为0,不论是直接赋值第三组数据,还是ADC检测,第三组数据都没有值,想问一下是不是这套组件无线收发传输数据的带宽限制了只能发送两组数据,求解答,谢谢。程序源码是基于官方的源码修改的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MSP430F2274利用CC2500模块进行无线发送的时候,通过msg数组进行发送温度和电压数据,我这边想在msg数组多增加一组内容 ,多发送一个电压数据,但始终第三组电压数据为0,不论是直接赋值第三组数据,还是ADC检测,第三组数据都没有值,想问一下是不是这套组件无线收发传输数据的带宽限制了只能发送两组数据,求解答,谢谢。程序源码是基于官方的源码修改的
您是指下面的msg?
/* message format, UB = upper Byte, LB = lower Byte
-------------------------------
|degC LB | degC UB | volt LB |
-------------------------------
0 1 2
*/
temp = results[1];
volt = (temp*25)/512;
msg[0] = degC&0xFF;
msg[1] = (degC>>8)&0xFF;
msg[2] = volt;
哦哦 那请问这个10是什么意思呢 限制了Msg能发多少字节呢?谢谢