单片机MSP430F2274进入低功耗LPM3,是不是一定要外接晶振,才能进入LPM3模式,进入LPM3时候,测到的电流不是手册上的1.4uA.同时,
另外一个问题,F2274外接晶振的时候,按照引脚的定义只能接P2.6和P2.7,但是这两个管教已经被套件定义控制和CC2500连接,能否使得这个IO功能复用,既接受晶振信号,又控制CC2500呢?8270.新建 DOC 文档.doc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
单片机MSP430F2274进入低功耗LPM3,是不是一定要外接晶振,才能进入LPM3模式,进入LPM3时候,测到的电流不是手册上的1.4uA.同时,
另外一个问题,F2274外接晶振的时候,按照引脚的定义只能接P2.6和P2.7,但是这两个管教已经被套件定义控制和CC2500连接,能否使得这个IO功能复用,既接受晶振信号,又控制CC2500呢?8270.新建 DOC 文档.doc
测功耗这个问题 ,我想标定他处于LPM3模式的时间长度,怎么测呢,电流只有几微安,串联电阻用示波器也看不了,本身示波器悬空就有10几毫伏电压。请问️什么方法吗,因为我程序里面设置了几种不同模式,所以想要标定时间
那有没有传统的测试方法呢 用示波器和其他设备 你这个方法还得再买仪器设备
我这边有MSP430-FET,请问有具体测量方法,你好像没具体说到结合FET怎么做到energy trace,谢谢
在LMP3下,ACLK remains active.
您可以使用定时器timer将ACLK设为时钟源,产生定时中断来从LPM3模式下唤醒芯片
例程中给出的是WDT来唤醒,您可以参考一下
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430F22x4 Demo - Basic Clock, LPM3 Using WDT ISR, 32kHz ACLK
//
// Description: This program operates MSP430 normally in LPM3, pulsing P1.0
// at 4 second intervals. WDT ISR used to wake-up system. All I/O configured
// as low outputs to eliminate floating inputs. Current consumption does
// increase when LED is powered on P1.0. Demo for measuring LPM3 current.
// ACLK = LFXT1/4 = 32768/4, MCLK = SMCLK = default DCO ~1.2MHz
// //* External watch crystal on XIN XOUT is required for ACLK *//
//
// MSP430F22x4
// ---------------
// /|\| XIN|-
// | | | 32kHz
// --|RST XOUT|-
// | |
// | P1.0|-->LED
//
// A. Dannenberg
// Texas Instruments Inc.
// April 2006
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.41A
//******************************************************************************
#include <msp430.h>
volatile unsigned int i;
int main(void)
{
BCSCTL1 |= DIVA_2; // ACLK/4
WDTCTL = WDT_ADLY_1000; // WDT 1s/4 interval timer
IE1 |= WDTIE; // Enable WDT interrupt
P1DIR = 0xFF; // All P1.x outputs
P1OUT = 0; // All P1.x reset
P2DIR = 0xFF; // All P2.x outputs
P2OUT = 0; // All P2.x reset
P3DIR = 0xFF; // All P3.x outputs
P3OUT = 0; // All P3.x reset
P4DIR = 0xFF; // All P4.x outputs
P4OUT = 0; // All P4.x reset
while(1)
{
__bis_SR_register(LPM3_bits + GIE); // Enter LPM3, enable interrupts
P1OUT |= 0x01; // Set P1.0 LED on
for (i = 5000; i > 0; i--); // Delay
P1OUT &= ~0x01; // Clear P1.0 LED off
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = WDT_VECTOR
__interrupt void watchdog_timer(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(WDT_VECTOR))) watchdog_timer (void)
#else
#error Compiler not supported!
#endif
{
__bic_SR_register_on_exit(LPM3_bits); // Clear LPM3 bits from 0(SR)
}
请问IAR可以做energy trace不 还是说一定要用CCS软件呢
应该是浏览器问题,我这边使用的是谷歌浏览器,可以打开的
不需要安装插件,那您点击Emulator是否可以点击下面的选项?
• State Log
• Power Log
• Timeline
• Function Profiler