This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5418通过io口窃取Rx8025备用电池电流问题



最近做了一个手持设备,用RX8025做外部RTC,但是在测试时发现在430开始运行后,断掉主电源后,发现单片机旁路电容两端仍存在2V左右电压,按复位键依然没有消失,去掉RTC的备用电池后,电压才逐步降了下来。但是,当板子上所有电容都不存在电压是,装上备用电池,单片机旁路电容却没有电压。

 rx8025和430的接口包括 iic 和两个中断信号,都加了上拉接到单片机主电源上,另外一个rx8025时钟管脚输入到XT1in。

请教高手帮忙指点迷津啊,找了一周的方法了,还是没解决啊。

联系邮箱:375020581@qq.com

  • Weiguang Fan, 我曾经测试过,即使不给MSP430直接供电,由于MSP430低功耗和本身的特性,只要与MSP430相连的作为MSP430输入管脚的管脚上有高电平存在或者是电平的周期变化(只要不是一直保持低电平),那么MSP430就可以工作起来。如你所说,

    Weiguang Fan 说:
     rx8025和430的接口包括 iic 和两个中断信号,都加了上拉接到单片机主电源上,另外一个rx8025时钟管脚输入到XT1in。

    你可以检查一下,在你断掉主电源后,这些管脚中间,作为MSP430输入的管脚上,哪些仍旧有电压或波形,用示波器测测,然后可以试着切断这些管脚,看看MSP430是否还有电压。如果没有了,这个就是你要解决问题的方向了。

  • 你的纽扣电池有没有加二级管?

    请确保用外电源的时候切断纽扣电池