This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助!MSP430F5438A如何换成调整晶振工作模式?

Other Parts Discussed in Thread: MSP430F5438A

    MSP430的时钟系统确实是非常强大,但同时了十分复杂。现在我想将MSP430换成LXT2上的高速晶振都摸不着门路。看了一下 User's Guide,里面关于时钟系统的有10个寄存器,而且不是设置几个就能达到目地……然后找了个CCS里自带的例子,如下。问题是根本找不到 hal_pmm.h 文件。对于这个例子希望能得到些大家的解释或者提供一个可行的方法。谢谢!

//MSP430F5438A
// -----------------
// /|\| |
// | |          P11.0|-->ACLK
// --|RST P11.1|-->MCLK
// |            P11.2|-->SMCLK
// | |
// |            P1.0|-->LED

// In order to run the system at up to 12MHz, VCore must be set at 1.6V
// or higher. This is done by invoking function SetVCore(), which requires
// 2 files, hal_pmm.c and hal_pmm.h, to be included in the project.
// hal_pmm.c and hal_pmm.h are located in the same folder as the code
// example.

#include "msp430x54xA.h"
#include "hal_pmm.h"
void main(void)
{
WDTCTL = WDTPW+WDTHOLD; // Stop WDT
SetVCore(PMMCOREV_1); // Set VCore = 1.6V for 12MHz clock
P1DIR |= BIT0; // P1.0 output
P11DIR |= 0x07; // ACLK, MCLK, SMCLK set out to pins
P11SEL |= 0x07; // P11.0,1,2 for debugging purposes.

UCSCTL3 |= SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_2; // Set ACLK = REFO

__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_5; // Select DCO range 24MHz operation
UCSCTL2 = FLLD_1 + 374; // Set DCO Multiplier for 12MHz
// (N + 1) * FLLRef = Fdco
// (374 + 1) * 32768 = 12MHz
// Set FLL Div = fDCOCLK/2
__bic_SR_register(SCG0); // Enable the FLL control loop

// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 12 MHz / 32,768 Hz = 375000 = MCLK cycles for DCO to settle
__delay_cycles(375000);

// Loop until XT1,XT2 & DCO fault flag is cleared
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + XT1HFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag

while(1)
{
P1OUT ^= BIT0; // Toggle P1.0
__delay_cycles(600000); // Delay
}
}

  • Qingcui Lu,

    你找的这个例子,使用了MSP430 core library, 你找不到的文件 hal_pmm.h,就是库文件中的一个,你可以直接从下面链接下载core lib的说明文档和对应库源文件。将core library源文件加入你的工程后,就可以直接用了。因为若想让MCLK跑在较高主频的话,首先应该设置较高的core level.

    http://www.ti.com/mcu/docs/litabsmultiplefilelist.tsp?sectionId=96&tabId=1502&literatureNumber=slaa448c&docCategoryId=1&familyId=1615

    http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=slaa448c&fileType=zip

    关于单独只是想设置XT2 sources MCLK & SMCLK,MSP430Ware中就有对应例程,见下面附件,

  • 另外,对于MSP430F5438A而言,默认是Vcore 为level 0,故最高MCLK可跑至8MHz,如果你想让MCLK>8MHz,,首先设置Vcore level,且同时注意Vcc供电也必须满足条件,下面两个图均从datasheet来,你可以参考一下。

  • 单独只是想设置XT2 sources MCLK & SMCLK 和之前说的让MCLK跑较高的主频有什么区别吗?意思是,单独只是想设置XT2的话,其它硬件部分可以使用XT2而MCLK受core level限制无法使用XT2?

  • MCLK要跑高的主频(>8MHz),那么必须设置较高的core level;如果MCLK从XT2来,例如XT2是16MHz, 而你又没有设置core level,即还是core level0,此时其实还是可以从XT2引入的,只要使用分频,使得XT2-> XT2/N 再给MCLK即可。如果此时直接将16MHz的XT2直接作为MCLK时钟源,而此时core level 为0,这样肯定是不行的。都提出来,只是为了说明两点:

    1. 如果设置XT2作为MCLK or SMCLK 时钟源;

    2. 使用较高MCLK时,不要忘记先设置core level。顺便对你找到的例子中调用库函数进行一下解释和说明。

  • 抱歉,纠正一下,O(∩_∩)O~ 1. 如何设置XT2作为MCLK or SMCLK 时钟源;

  • 我不建议在应用时死死的钻牛角尖。能完成所要求的功能即可。

  • 呵,谢谢了,我知道怎么用了。