This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529 定时器中断向量

Other Parts Discussed in Thread: MSP430F5529

#define TIMER2_A1_VECTOR        (43 * 1u)       /* 0xFFD6 Timer2_A5 CC1-4, TA */

#define TIMER2_A0_VECTOR        (44 * 1u)       /* 0xFFD8 Timer2_A5 CC0 */

#define TIMER1_A1_VECTOR        (48 * 1u)        /* 0xFFE0 Timer1_A3 CC1-2, TA1 */

#define TIMER1_A0_VECTOR        (49 * 1u)       /* 0xFFE2 Timer1_A3 CC0 */

#define TIMER0_A1_VECTOR        (52 * 1u)       /* 0xFFE8 Timer0_A5 CC1-4, TA */

#define TIMER0_A0_VECTOR        (53 * 1u)       /* 0xFFEA Timer0_A5 CC0 */

上面的语句是从 msp430f5529.h 中粘贴的

我设置  P1.4 为(TA0.CCI3A)捕获输入口,应该使用哪个中断向量?

  • 应该使用 TIMER0_A1_VECTOR (52 * 1u) /* 0xFFE8 Timer0_A5 CC1-4, TA */

    F5529没有直接的例程capture 频率,但是F51x2系列有,因为F51x2系列有TImerD支持256-MHz / 4-ns 分辨率。

    具体文档请参考: “”“Using the MSP430 Timer_D Module in Hi-Resolution Mode”

    www.ti.com/.../slaa601.pdf

    Code可以见MSP430F51x2 code example, 在MSP430Ware里就有。

    MSP430F51x2_td0_24.c Timer0_D3, Single Input Capture mode, Normal Timer Mode
    MSP430F51x2_td0_25.c Timer0_D3, Dual Input Capture mode, Normal timer mode, Period Measurement
    MSP430F51x2_td0_26.c Timer0_D3, Dual Input Capture mode, Normal timer mode, DutyCycle Measurement
  • 多谢,请问根据哪些参数判断是 TIMER0_A1_VECTOR 的?
  • 您好,请问还在吗?
  • 我好像知道了
    CCR0中断 是用 TIMERX_A0_VECTOR ; 定时器溢出中断和CCRX中断用 TIMERX_A1_VECTOR 。
    对不?
  • TIMER0_A1_VECTOR 和 TIMER0_A0_VECTOR    是TA0的中断向量

    TIMER0_A5 是TIMER0_A 5CCR,意思是有5个独立比较器寄存器

    MSP430中,不同的型号拥有不同的硬件配置,因此中断源也有所差别,TIMER0_A0_VECTOR表示定时器0 A0的中断源,0代表硬件上的定时器,有定时器0 定时器1等;A0代表定时器n内的A0寄存器,通常会有A0 A1等,他们都计数源都来自同一个定时器,但对计数源的数据可以进行不同的处理,从而产生不同的中断。

    TIMER0_A0_VECTOR是计时器0的CCR0的中断寄存器

    TIMER0_A1_VECTOR是计时器0的CCR1-CCR4、TA的寄存器