This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6972 LCDCAP 引脚悬空



你好,这个引脚悬空带来了那些影响能说明一下吗
  • CAUTION: LCDCAP/R33 must be connected to DVSS if not used.

    关于悬空问题,请参考一下下面的帖子

    e2e.ti.com/.../3382143

    The capacitor on LCDCAP only needs to be populated if you are using the LCD charge pump. If the charge pump starts up without a capacitor present, this can damage the device. If you are not using the charge pump, it is recommended to connect this pin to ground. If the charge pump is not turned on, there should not be risk of damage to the device, but current consumption could be higher since you have a floating pin.

    Please also note that the LCD_C on this device includes a protection to disable the charge pump if it is started and the LCDCAP is not present. See the LCDNOCAPIFG in the users guide.