Other Parts Discussed in Thread: MSP430F6779
请问在MSP430F6779的UART通信中,UCAxRXBUF能接收的数据是多大,我在实验使用过程中,发现并不能完整接收返回的字符串,只能接收一半。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F6779
请问在MSP430F6779的UART通信中,UCAxRXBUF能接收的数据是多大,我在实验使用过程中,发现并不能完整接收返回的字符串,只能接收一半。
请您试一下下面的程序,我之前在5529上测试的
示例显示如何配置UCA0 TX和RX中断向量以自动处理字节(字符)接收和发送。收到字节后,它将自动将字节复制到缓冲区。您必须在代码的其他位置设置缓冲区和指针。同样,当您要传输字符串时,请在代码中的某处创建一个缓冲区,并为其分配一个指针。准备好传输字符串时,请启用UCTXIE,ISR将自动处理其余部分。
#include <msp430.h>
#include <stdio.h>
#include <string.h>
//******************************************************************************
// UART Initialization *********************************************************
//******************************************************************************
#define LED_OUT P1OUT
#define LED_DIR P1DIR
#define LED_PIN BIT0
#define SMCLK_115200 0
#define SMCLK_9600 1
#define UART_MODE SMCLK_115200//SMCLK_9600//
unsigned char RXDataBuffer[64];
unsigned char TXDataBuffer[64] = "Hello world\r\n\0";
unsigned char* pTXBuffer = &TXDataBuffer[0];
unsigned char* pRXBuffer = &RXDataBuffer[0];
unsigned int bytesToSend;
unsigned int bytesReceived;
/*
* UART timing based on 8MHz SMCLK
*/
void initUART()
{
// Configure USCI_A0 for UART mode
UCA0CTLW0 |= UCSWRST; // Put eUSCI in reset
#if UART_MODE == SMCLK_115200
UCA0CTLW0 |= UCSSEL__SMCLK; // CLK = SMCLK
// Baud Rate Setting
// Use Table 21-5
UCA0BRW = 4;
UCA0MCTL |= UCOS16 | UCBRF_3 | UCBRS_5;
#elif UART_MODE == SMCLK_9600
UCA0CTLW |= UCSSEL__SMCLK; // CLK = SMCLK
// Baud Rate Setting
// Use Table 21-5
UCA0BRW = 52;
UCA0MCTL |= UCOS16 | UCBRF_1 | UCBRS_0;
#else
# error "Please specify baud rate to 115200 or 9600"
#endif
UCA0CTLW0 &= ~UCSWRST; // Initialize eUSCI
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
}
//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************
void initGPIO()
{
// Configure GPIO
P3SEL &= ~(BIT3 | BIT4); // USCI_A0 UART operation on FF5529LP
P3SEL |= (BIT3 | BIT4);
}
void initClockTo16MHz()
{
UCSCTL3 = SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_2; // Set ACLK = REFO
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
// Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL1 = DCORSEL_5; // Select DCO range 16MHz operation
UCSCTL2 |= 249; // Set DCO Multiplier for 8MHz
// (N + 1) * FLLRef = Fdco
// (249 + 1) * 32768 = 8MHz
__bic_SR_register(SCG0); // Enable the FLL control loop
// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 8 MHz / 32,768 Hz = 250000 = MCLK cycles for DCO to settle
__delay_cycles(250000);
}
void TransmitData(unsigned char* string, unsigned int length)
{
pTXBuffer = string;
bytesToSend = strlen((const char*) string);
UCA0IE |= UCTXIE; // Enable USCI_A0 TX interrupt
}
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
initGPIO();
initClockTo16MHz();
initUART();
/*
* Use timer to demonstrate automatic tranmission.
* Configure timer to periodically transmit a string.
*/
TA0CCTL0 |= CCIE; // TACCR0 interrupt enabled
TA0CCR0 = 50000;
TA0CTL |= TASSEL__SMCLK | MC__CONTINUOUS | ID__8; // SMCLK, continuous mode
__bis_SR_register(GIE);
while (1)
{
__bis_SR_register(LPM0_bits | GIE); // Enter LPM0
__no_operation(); // For debugger
}
}
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
{
switch(__even_in_range(UCA0IV,4))
{
case 0: break;
case 2:
UCA0IFG &=~ UCRXIFG; // Clear interrupt
*pRXBuffer = UCA0RXBUF; // Clear buffer
break;
case 4:
UCA0TXBUF = *pTXBuffer++;
if(--bytesToSend == 0)
UCA0IE &= ~UCTXIE; // Disable USCI_A0 TX interrupt after string has been transmitted.
break;
default:
break;
}
__bic_SR_register_on_exit(LPM0_bits); // Exit LPM0 on reti
}
// Timer A0 interrupt service routine
#pragma vector = TIMER0_A0_VECTOR
__interrupt void Timer_A (void)
{
static int count = 10;
if(--count == 0)
{
count = 10;
TransmitData(&TXDataBuffer[0], sizeof(TXDataBuffer));
_no_operation();
}
}