This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

430外接看门狗芯片



公司里设计用430的时候都外界看门狗芯片,内部的看门狗不可靠嘛?

  • 一般情况下,内部看门狗就够用了.实际上MSP430的绝大部分应用是没有用外部看门狗的.

    内部看门狗失效的原因可能有以下三点:

    1.看门狗时钟失效

    2.用户软件关掉看门狗

    3.MCU死锁

    对策

    1.对MSP430内部看门狗(WDT+)来讲,由于存在时钟失效检测机制和时钟自动切换机制.时钟失效不会影响到看门狗功能.

    2.用户软件注意全程打开WDT即可. 由于MSP430的看门狗寄存器存在密码保护,不存在程序跑飞造成WDT误关的情况

    3. MCU死锁的是一种极限情况, 跟系统EMC性能有关系,通常系统EMC性能过关,不会出现这种情况.