我现用的pic18f4455想转用msp430,不知用哪个型号?有没有选型工具?
要求:1.低功耗;2.两个串口,一个用作转usb;3.最好封装相近和兼容;4.资源丰富;5.性价比高 谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现用的pic18f4455想转用msp430,不知用哪个型号?有没有选型工具?
要求:1.低功耗;2.两个串口,一个用作转usb;3.最好封装相近和兼容;4.资源丰富;5.性价比高 谢
我查了一下PIC18F4455,
资源: 24K Flash,2K RAM, 12 MHz, 10 bit ADC,USB 2.0, 1 UART, 1SPI/I2C, 40 pin 封装。
可以使用MSP430F5509,48LQFP脚封装。
资源:24K Flash,4K RAM,2 Uart,1 SPI/I2C, RTC, Comparatator, 10 bit ADC, USB, DMA, SVS, 4 X 16 bit Timer.
TI官方网站1K参考报价:1.85美金
价廉物美啊。