This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I2C通信是用MSP430F5529作为主机,向外设AD5274(数字电位器)发送两个字节的数据。用的MSP430F55XX系列的例程,只有从机地址改成外设的固定地址。但是开始条件产生后,SDA和SCL都只是被拉低,没有波形的变化,一直到结束条件STP产生后,SDA和SCL空闲拉高。时钟是SMCLK,时钟源用4M的外部晶振,用IO口显示SMCLK,时钟源信号正常。想请教大家有没有碰到这种情况,问题有可能会出在哪里呢?
#include <msp430.h>
unsigned char *PTxData; // Pointer to TX data
unsigned char TXByteCtr;
const unsigned char TxData[] = // Table of data to transmit
{ 0x1C,0x02 };
int main(void)
{
unsigned int i;
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P3SEL |= 0x03; // Assign I2C pins to USCI_B0
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C Master, synchronous mode
UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
UCB0BR0 = 40; // fSCL = SMCLK/40 = ~100kHz
UCB0BR1 = 0;
UCB0I2CSA = 0x2E; // Slave Address is 048h
UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
UCB0IE |= UCTXIE; // Enable TX interrupt
while (1)
{
for(i=0;i<10;i++); // Delay required between transaction
PTxData = (unsigned char *)TxData; // TX array start address
// Place breakpoint here to see each
// transmit operation.
TXByteCtr = sizeof TxData; // Load TX byte counter
UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0, enable interrupts
__no_operation(); // Remain in LPM0 until all data
// is TX'd
while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent
}
}
//------------------------------------------------------------------------------
// The USCIAB0TX_ISR is structured such that it can be used to transmit any
// number of bytes by pre-loading TXByteCtr with the byte count. Also, TXData
// points to the next byte to transmit.
//------------------------------------------------------------------------------
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCI_B0_VECTOR
__interrupt void USCI_B0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_B0_VECTOR))) USCI_B0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCB0IV,12))
{
case 0: break; // Vector 0: No interrupts
case 2: break; // Vector 2: ALIFG
case 4: break; // Vector 4: NACKIFG
case 6: break; // Vector 6: STTIFG
case 8: break; // Vector 8: STPIFG
case 10: break; // Vector 10: RXIFG
case 12: // Vector 12: TXIFG
if (TXByteCtr) // Check TX byte counter
{
UCB0TXBUF = *PTxData++; // Load TX buffer
TXByteCtr--; // Decrement TX byte counter
}
else
{
UCB0CTL1 |= UCTXSTP; // I2C stop condition
UCB0IFG &= ~UCTXIFG; // Clear USCI_B0 TX int flag
__bic_SR_register_on_exit(LPM0_bits); // Exit LPM0
}
default: break;
}
}
//****************************************************************************** // MSP430F552x Demo - USCI_B0 I2C Master TX multiple bytes to MSP430 Slave // // Description: This demo connects two MSP430's via the I2C bus. The master // transmits to the slave. This is the MASTER CODE. It cntinuously // transmits an array of data and demonstrates how to implement an I2C // master transmitter sending multiple bytes using the USCI_B0 TX interrupt. // ACLK = n/a, MCLK = SMCLK = BRCLK = default DCO = ~1.045MHz // // ***to be used with "MSP430F55xx_uscib0_i2c_09.c" *** // // /|\ /|\ // MSP430F5529 10k 10k MSP430F5529 // slave | | master // ----------------- | | ----------------- // -|XIN P3.0/UCB0SDA|<-|----+->|P3.0/UCB0SDA XIN|- // | | | | | // -|XOUT | | | XOUT|- // | P3.1/UCB0SCL|<-+------>|P3.1/UCB0SCL | // | | | | // // Bhargavi Nisarga // Texas Instruments Inc. // April 2009 // Built with CCSv4 and IAR Embedded Workbench Version: 4.21 //******************************************************************************
您是使用2块板子测试的?是否有外接电阻?