This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
硬件条件是SEED-EXP430F5529 V1,.0 程序如下:
#include <msp430.h>
int main(void)
{
volatile unsigned int i;
WDTCTL = WDTPW+WDTHOLD; // Stop WDT
P1DIR |= BIT0; // P1.0 set as output
while(1) // continuous loop
{
P1OUT ^= BIT0; // XOR P1.0
for(i=50000;i>0;i--); // Delay
}
}
问题:观察这段程序,很明显是P1DIR是寄存器,既然是寄存器就应该有物理地址,当我打开头文件的时候却并未发现,只是发现以下两条信息:
SFR_8BIT(PADIR_L); /* Port A Direction */ 1504行
#define P1DIR (PADIR_L) /* Port 1 Direction */ 1530行 在CC35.3下观察
就在无发现其它有用的信息。按我的理解头文件不应该是按照如下书写嘛?
SFR_8BIT (PADIR_L)=0X020004 ; /* Port A Direction */
#define P1DIR (PADIR_L) /* Port 1 Direction */
这样才指向了PI的寄存器吧?
物理地址来源于:
追问关于volatile是什么意思,这类的定义可以在那里看到呢?谢谢
xiaolu liao1,其中关于头文件zho中的 SFR_8BIT(PADIR_L); 应该按照头文件开头的,
/* External references resolved by a device-specific linker command file */
#define SFR_8BIT(address) extern volatile unsigned char address
来解析,应该对应为:
SFR_8BIT(PADIR_L) extern volatile unsigned char PADIR_L
而关于PADIR_L,如果你使用的是CCS的话,其实在.cmd 文件中有一句 (此处以msp430g2553为例)
/****************************************************************************/
/* INCLUDE PERIPHERALS MEMORY MAP */
/****************************************************************************/
-l msp430g2553.cmd
故各个寄存器的地址指明其实是在msp430g2553.cmd文件中,在安装路径,
C:\ti\CCS5_3_0\ccsv5\ccs_base\msp430\include
下可以找到。
下面是msp430g2553.cmd的内容,你可以找找msp430f5529的。
/******************************************************************************/
/* msp430g2533.cmd */
/* - Linker Command File for defintions in the header file */
/* Please do not change ! */
/* */
/******************************************************************************/
/************************************************************
* STANDARD BITS
************************************************************/
/************************************************************
* STATUS REGISTER BITS
************************************************************/
/************************************************************
* PERIPHERAL FILE MAP
************************************************************/
/************************************************************
* SPECIAL FUNCTION REGISTER ADDRESSES + CONTROL BITS
************************************************************/
IE1 = 0x0000;
IFG1 = 0x0002;
IE2 = 0x0001;
IFG2 = 0x0003;
/************************************************************
* ADC10
************************************************************/
ADC10DTC0 = 0x0048;
ADC10DTC1 = 0x0049;
ADC10AE0 = 0x004A;
ADC10CTL0 = 0x01B0;
ADC10CTL1 = 0x01B2;
ADC10MEM = 0x01B4;
ADC10SA = 0x01BC;
/************************************************************
* Basic Clock Module
************************************************************/
DCOCTL = 0x0056;
BCSCTL1 = 0x0057;
BCSCTL2 = 0x0058;
BCSCTL3 = 0x0053;
/*************************************************************
* Flash Memory
*************************************************************/
FCTL1 = 0x0128;
FCTL2 = 0x012A;
FCTL3 = 0x012C;
/************************************************************
* DIGITAL I/O Port1/2 Pull up / Pull down Resistors
************************************************************/
P1IN = 0x0020;
P1OUT = 0x0021;
P1DIR = 0x0022;
P1IFG = 0x0023;
P1IES = 0x0024;
P1IE = 0x0025;
P1SEL = 0x0026;
P1SEL2 = 0x0041;
P1REN = 0x0027;
P2IN = 0x0028;
P2OUT = 0x0029;
P2DIR = 0x002A;
P2IFG = 0x002B;
P2IES = 0x002C;
P2IE = 0x002D;
P2SEL = 0x002E;
P2SEL2 = 0x0042;
P2REN = 0x002F;
/************************************************************
* DIGITAL I/O Port3 Pull up / Pull down Resistors
************************************************************/
P3IN = 0x0018;
P3OUT = 0x0019;
P3DIR = 0x001A;
P3SEL = 0x001B;
P3SEL2 = 0x0043;
P3REN = 0x0010;
/************************************************************
* Timer0_A3
************************************************************/
TA0IV = 0x012E;
TA0CTL = 0x0160;
TA0CCTL0 = 0x0162;
TA0CCTL1 = 0x0164;
TA0CCTL2 = 0x0166;
TA0R = 0x0170;
TA0CCR0 = 0x0172;
TA0CCR1 = 0x0174;
TA0CCR2 = 0x0176;
/************************************************************
* Timer1_A3
************************************************************/
TA1IV = 0x011E;
TA1CTL = 0x0180;
TA1CCTL0 = 0x0182;
TA1CCTL1 = 0x0184;
TA1CCTL2 = 0x0186;
TA1R = 0x0190;
TA1CCR0 = 0x0192;
TA1CCR1 = 0x0194;
TA1CCR2 = 0x0196;
/************************************************************
* USCI
************************************************************/
UCA0CTL0 = 0x0060;
UCA0CTL1 = 0x0061;
UCA0BR0 = 0x0062;
UCA0BR1 = 0x0063;
UCA0MCTL = 0x0064;
UCA0STAT = 0x0065;
UCA0RXBUF = 0x0066;
UCA0TXBUF = 0x0067;
UCA0ABCTL = 0x005D;
UCA0IRTCTL = 0x005E;
UCA0IRRCTL = 0x005F;
UCB0CTL0 = 0x0068;
UCB0CTL1 = 0x0069;
UCB0BR0 = 0x006A;
UCB0BR1 = 0x006B;
UCB0I2CIE = 0x006C;
UCB0STAT = 0x006D;
UCB0RXBUF = 0x006E;
UCB0TXBUF = 0x006F;
UCB0I2COA = 0x0118;
UCB0I2CSA = 0x011A;
/************************************************************
* WATCHDOG TIMER
************************************************************/
WDTCTL = 0x0120;
/************************************************************
* Calibration Data in Info Mem
************************************************************/
CALDCO_16MHZ = 0x10F8;
CALBC1_16MHZ = 0x10F9;
CALDCO_12MHZ = 0x10FA;
CALBC1_12MHZ = 0x10FB;
CALDCO_8MHZ = 0x10FC;
CALBC1_8MHZ = 0x10FD;
CALDCO_1MHZ = 0x10FE;
CALBC1_1MHZ = 0x10FF;
/************************************************************
* Interrupt Vectors (offset from 0xFFE0)
************************************************************/
/************************************************************
* End of Modules
************************************************************/
/******************************************************************************/
/* lnk_msp430f5529.cmd - LINKER COMMAND FILE FOR LINKING MSP430F5529 PROGRAMS */
/* */
/* Usage: lnk430 <obj files...> -o <out file> -m <map file> lnk.cmd */
/* cl430 <src files...> -z -o <out file> -m <map file> lnk.cmd */
/* */
/*----------------------------------------------------------------------------*/
/* These linker options are for command line linking only. For IDE linking, */
/* you should set your linker options in Project Properties */
/* -c LINK USING C CONVENTIONS */
/* -stack 0x0100 SOFTWARE STACK SIZE */
/* -heap 0x0100 HEAP AREA SIZE */
/* */
/*----------------------------------------------------------------------------*/
/****************************************************************************/
/* SPECIFY THE SYSTEM MEMORY MAP */
/****************************************************************************/
MEMORY
{
SFR : origin = 0x0000, length = 0x0010
PERIPHERALS_8BIT : origin = 0x0010, length = 0x00F0
PERIPHERALS_16BIT : origin = 0x0100, length = 0x0100
RAM : origin = 0x2400, length = 0x2000
USBRAM : origin = 0x1C00, length = 0x0800
INFOA : origin = 0x1980, length = 0x0080
INFOB : origin = 0x1900, length = 0x0080
INFOC : origin = 0x1880, length = 0x0080
INFOD : origin = 0x1800, length = 0x0080
FLASH : origin = 0x4400, length = 0xBB80
FLASH2 : origin = 0x10000,length = 0x14400
INT00 : origin = 0xFF80, length = 0x0002
INT01 : origin = 0xFF82, length = 0x0002
INT02 : origin = 0xFF84, length = 0x0002
INT03 : origin = 0xFF86, length = 0x0002
INT04 : origin = 0xFF88, length = 0x0002
INT05 : origin = 0xFF8A, length = 0x0002
INT06 : origin = 0xFF8C, length = 0x0002
INT07 : origin = 0xFF8E, length = 0x0002
INT08 : origin = 0xFF90, length = 0x0002
INT09 : origin = 0xFF92, length = 0x0002
INT10 : origin = 0xFF94, length = 0x0002
INT11 : origin = 0xFF96, length = 0x0002
INT12 : origin = 0xFF98, length = 0x0002
INT13 : origin = 0xFF9A, length = 0x0002
INT14 : origin = 0xFF9C, length = 0x0002
INT15 : origin = 0xFF9E, length = 0x0002
INT16 : origin = 0xFFA0, length = 0x0002
INT17 : origin = 0xFFA2, length = 0x0002
INT18 : origin = 0xFFA4, length = 0x0002
INT19 : origin = 0xFFA6, length = 0x0002
INT20 : origin = 0xFFA8, length = 0x0002
INT21 : origin = 0xFFAA, length = 0x0002
INT22 : origin = 0xFFAC, length = 0x0002
INT23 : origin = 0xFFAE, length = 0x0002
INT24 : origin = 0xFFB0, length = 0x0002
INT25 : origin = 0xFFB2, length = 0x0002
INT26 : origin = 0xFFB4, length = 0x0002
INT27 : origin = 0xFFB6, length = 0x0002
INT28 : origin = 0xFFB8, length = 0x0002
INT29 : origin = 0xFFBA, length = 0x0002
INT30 : origin = 0xFFBC, length = 0x0002
INT31 : origin = 0xFFBE, length = 0x0002
INT32 : origin = 0xFFC0, length = 0x0002
INT33 : origin = 0xFFC2, length = 0x0002
INT34 : origin = 0xFFC4, length = 0x0002
INT35 : origin = 0xFFC6, length = 0x0002
INT36 : origin = 0xFFC8, length = 0x0002
INT37 : origin = 0xFFCA, length = 0x0002
INT38 : origin = 0xFFCC, length = 0x0002
INT39 : origin = 0xFFCE, length = 0x0002
INT40 : origin = 0xFFD0, length = 0x0002
INT41 : origin = 0xFFD2, length = 0x0002
INT42 : origin = 0xFFD4, length = 0x0002
INT43 : origin = 0xFFD6, length = 0x0002
INT44 : origin = 0xFFD8, length = 0x0002
INT45 : origin = 0xFFDA, length = 0x0002
INT46 : origin = 0xFFDC, length = 0x0002
INT47 : origin = 0xFFDE, length = 0x0002
INT48 : origin = 0xFFE0, length = 0x0002
INT49 : origin = 0xFFE2, length = 0x0002
INT50 : origin = 0xFFE4, length = 0x0002
INT51 : origin = 0xFFE6, length = 0x0002
INT52 : origin = 0xFFE8, length = 0x0002
INT53 : origin = 0xFFEA, length = 0x0002
INT54 : origin = 0xFFEC, length = 0x0002
INT55 : origin = 0xFFEE, length = 0x0002
INT56 : origin = 0xFFF0, length = 0x0002
INT57 : origin = 0xFFF2, length = 0x0002
INT58 : origin = 0xFFF4, length = 0x0002
INT59 : origin = 0xFFF6, length = 0x0002
INT60 : origin = 0xFFF8, length = 0x0002
INT61 : origin = 0xFFFA, length = 0x0002
INT62 : origin = 0xFFFC, length = 0x0002
RESET : origin = 0xFFFE, length = 0x0002
}
/****************************************************************************/
/* SPECIFY THE SECTIONS ALLOCATION INTO MEMORY */
/****************************************************************************/
SECTIONS
{
.bss : {} > RAM /* GLOBAL & STATIC VARS */
.data : {} > RAM /* GLOBAL & STATIC VARS */
.sysmem : {} > RAM /* DYNAMIC MEMORY ALLOCATION AREA */
.stack : {} > RAM (HIGH) /* SOFTWARE SYSTEM STACK */
.text : {}>> FLASH | FLASH2 /* CODE */
.text:_isr : {} > FLASH /* ISR CODE SPACE */
.cinit : {} > FLASH /* INITIALIZATION TABLES */
//#ifdef (__LARGE_DATA_MODEL__)
.const : {} > FLASH | FLASH2 /* CONSTANT DATA */
//#else
// .const : {} > FLASH /* CONSTANT DATA */
//#endif
.cio : {} > RAM /* C I/O BUFFER */
.pinit : {} > FLASH /* C++ CONSTRUCTOR TABLES */
.init_array : {} > FLASH /* C++ CONSTRUCTOR TABLES */
.mspabi.exidx : {} > FLASH /* C++ CONSTRUCTOR TABLES */
.mspabi.extab : {} > FLASH /* C++ CONSTRUCTOR TABLES */
.infoA : {} > INFOA /* MSP430 INFO FLASH MEMORY SEGMENTS */
.infoB : {} > INFOB
.infoC : {} > INFOC
.infoD : {} > INFOD
/* MSP430 INTERRUPT VECTORS */
.int00 : {} > INT00
.int01 : {} > INT01
.int02 : {} > INT02
.int03 : {} > INT03
.int04 : {} > INT04
.int05 : {} > INT05
.int06 : {} > INT06
.int07 : {} > INT07
.int08 : {} > INT08
.int09 : {} > INT09
.int10 : {} > INT10
.int11 : {} > INT11
.int12 : {} > INT12
.int13 : {} > INT13
.int14 : {} > INT14
.int15 : {} > INT15
.int16 : {} > INT16
.int17 : {} > INT17
.int18 : {} > INT18
.int19 : {} > INT19
.int20 : {} > INT20
.int21 : {} > INT21
.int22 : {} > INT22
.int23 : {} > INT23
.int24 : {} > INT24
.int25 : {} > INT25
.int26 : {} > INT26
.int27 : {} > INT27
.int28 : {} > INT28
.int29 : {} > INT29
.int30 : {} > INT30
.int31 : {} > INT31
.int32 : {} > INT32
.int33 : {} > INT33
.int34 : {} > INT34
.int35 : {} > INT35
.int36 : {} > INT36
.int37 : {} > INT37
.int38 : {} > INT38
.int39 : {} > INT39
.int40 : {} > INT40
RTC : { * ( .int41 ) } > INT41 type = VECT_INIT
PORT2 : { * ( .int42 ) } > INT42 type = VECT_INIT
TIMER2_A1 : { * ( .int43 ) } > INT43 type = VECT_INIT
TIMER2_A0 : { * ( .int44 ) } > INT44 type = VECT_INIT
USCI_B1 : { * ( .int45 ) } > INT45 type = VECT_INIT
USCI_A1 : { * ( .int46 ) } > INT46 type = VECT_INIT
PORT1 : { * ( .int47 ) } > INT47 type = VECT_INIT
TIMER1_A1 : { * ( .int48 ) } > INT48 type = VECT_INIT
TIMER1_A0 : { * ( .int49 ) } > INT49 type = VECT_INIT
DMA : { * ( .int50 ) } > INT50 type = VECT_INIT
USB_UBM : { * ( .int51 ) } > INT51 type = VECT_INIT
TIMER0_A1 : { * ( .int52 ) } > INT52 type = VECT_INIT
TIMER0_A0 : { * ( .int53 ) } > INT53 type = VECT_INIT
ADC12 : { * ( .int54 ) } > INT54 type = VECT_INIT
USCI_B0 : { * ( .int55 ) } > INT55 type = VECT_INIT
USCI_A0 : { * ( .int56 ) } > INT56 type = VECT_INIT
WDT : { * ( .int57 ) } > INT57 type = VECT_INIT
TIMER0_B1 : { * ( .int58 ) } > INT58 type = VECT_INIT
TIMER0_B0 : { * ( .int59 ) } > INT59 type = VECT_INIT
COMP_B : { * ( .int60 ) } > INT60 type = VECT_INIT
UNMI : { * ( .int61 ) } > INT61 type = VECT_INIT
SYSNMI : { * ( .int62 ) } > INT62 type = VECT_INIT
.reset : {} > RESET /* MSP430 RESET VECTOR */
}
/****************************************************************************/
/* INCLUDE PERIPHERALS MEMORY MAP */
/****************************************************************************/
-l msp430f5529.cmd
Lina Lian 对的,我是利用CCS5.3,以上是我打开MSP430F5529.CMD,但是并没有出现你说的,为啥这两个CMD文件区别这么大?能有关于CMD的说明和关于MSP430的编译器说明? 谢谢
xiaolu liao1,你打开的是 lnk_msp430f5529.cmd file,而非msp430f5529.cmd file.
在lnk_msp430f5529.cmd file 的最后一句‘-l msp430f5529.cmd’ 中提到了msp430f5529.cmd,请到下列路径中寻找。
C:\ti\CCS5_3_0\ccsv5\ccs_base\msp430\include
Lina Lian 谢谢,嗯 找到了,为什么TI不这个直接放在头文件里面还要另外建立一个CMD文件,请问这样有什么好处,另外TI官网上有关MSP430编译器说明不
xiaolu liao1, 这是因为, lnk_msp430f5529.cmd file 说明了 system memory map,即flash,ram的划分,已及.data, .text等的分配和放置,客户可以按照你的想法和应用来更改 lnk_msp430f5529.cmd file。
但是msp430f5529.cmd file 是说明了PERIPHERALS MEMORY MAP ,对每个device而言是固定不变的。且为了防止客户不小心更改,故没有直接放在头文件中,而是以link的方式出现的。
这些是我的理解。可能不太全面,如果有什么补充和建议,可以提出来。O(∩_∩)O~
另外关于MSP430 compiler的文档的话,可以参考,MSP430 Optimizing C/C++ Compiler v 4.1 User's Guide,链接如下。
http://www.ti.com/lit/ug/slau132g/slau132g.pdf
Code Composer Studio™ v5.3 User's Guide for MSP430 User's Guide,这个是讲CCS的。
Lina Lian 继续头文件,打开<msp430.h>,即进入
#ifndef __msp430
#define __msp430
#if defined (__MSP430C111__)
#include "msp430c111.h"
#elif defined (__MSP430C1111__)
#include "msp430c1111.h"
#elif defined (__MSP430C112__)
#include "msp430c112.h"
#elif defined (__MSP430C1121__)
#include "msp430c1121.h"
#elif defined (__MSP430C1331__)
#include "msp430c1331.h"
#elif defined (__MSP430C1351__)
#include "msp430c1351.h"
#elif defined (__MSP430C311S__)
#include "msp430c311s.h"
#elif defined (__MSP430C312__)
#include "msp430c312.h"
#elif defined (__MSP430C313__)
#include "msp430c313.h"
#elif defined (__MSP430C314__)
#include "msp430c314.h"
#elif defined (__MSP430C315__)
#include "msp430c315.h"
#elif defined (__MSP430C323__)
#include "msp430c323.h"
#elif defined (__MSP430C325__)
#include "msp430c325.h"
#elif defined (__MSP430C336__)
#include "msp430c336.h"
#elif defined (__MSP430C337__)
#include "msp430c337.h"
#elif defined (__MSP430C412__)
#include "msp430c412.h"
#elif defined (__MSP430C413__)
#include "msp430c413.h"
#elif defined (__MSP430CG4616__)
#include "msp430cg4616.h"
#elif defined (__MSP430CG4617__)
#include "msp430cg4617.h"
#elif defined (__MSP430CG4618__)
#include "msp430cg4618.h"
#elif defined (__MSP430CG4619__)
#include "msp430cg4619.h"
#elif defined (__MSP430E112__)
#include "msp430e112.h"
#elif defined (__MSP430E313__)
#include "msp430e313.h"
#elif defined (__MSP430E315__)
#include "msp430e315.h"
#elif defined (__MSP430E325__)
#include "msp430e325.h"
#elif defined (__MSP430E337__)
#include "msp430e337.h"
#elif defined (__MSP430F110__)
#include "msp430f110.h"
#elif defined (__MSP430F1101__)
#include "msp430f1101.h"
#elif defined (__MSP430F1101A__)
#include "msp430f1101a.h"
#elif defined (__MSP430F1111__)
#include "msp430f1111.h"
#elif defined (__MSP430F1111A__)
#include "msp430f1111a.h"
#elif defined (__MSP430F112__)
#include "msp430f112.h"
#elif defined (__MSP430F1121__)
#include "msp430f1121.h"
#elif defined (__MSP430F1121A__)
#include "msp430f1121a.h"
#elif defined (__MSP430F1122__)
#include "msp430f1122.h"
#elif defined (__MSP430F1132__)
#include "msp430f1132.h"
#elif defined (__MSP430F122__)
#include "msp430f122.h"
#elif defined (__MSP430F1222__)
#include "msp430f1222.h"
#elif defined (__MSP430F123__)
#include "msp430f123.h"
#elif defined (__MSP430F1232__)
#include "msp430f1232.h"
#elif defined (__MSP430F133__)
#include "msp430f133.h"
#elif defined (__MSP430F135__)
#include "msp430f135.h"
#elif defined (__MSP430F147__)
#include "msp430f147.h"
#elif defined (__MSP430F148__)
#include "msp430f148.h"
#elif defined (__MSP430F149__)
#include "msp430f149.h"
#elif defined (__MSP430F1471__)
#include "msp430f1471.h"
#elif defined (__MSP430F1481__)
#include "msp430f1481.h"
#elif defined (__MSP430F1491__)
#include "msp430f1491.h"
#elif defined (__MSP430F155__)
#include "msp430f155.h"
#elif defined (__MSP430F156__)
#include "msp430f156.h"
#elif defined (__MSP430F157__)
#include "msp430f157.h"
#elif defined (__MSP430F167__)
#include "msp430f167.h"
#elif defined (__MSP430F168__)
#include "msp430f168.h"
#elif defined (__MSP430F169__)
#include "msp430f169.h"
#elif defined (__MSP430F1610__)
#include "msp430f1610.h"
#elif defined (__MSP430F1611__)
#include "msp430f1611.h"
#elif defined (__MSP430F1612__)
#include "msp430f1612.h"
#elif defined (__MSP430F2001__)
#include "msp430f2001.h"
#elif defined (__MSP430F2011__)
#include "msp430f2011.h"
#elif defined (__MSP430F2002__)
#include "msp430f2002.h"
#elif defined (__MSP430F2012__)
#include "msp430f2012.h"
#elif defined (__MSP430F2003__)
#include "msp430f2003.h"
#elif defined (__MSP430F2013__)
#include "msp430f2013.h"
#elif defined (__MSP430F2101__)
#include "msp430f2101.h"
#elif defined (__MSP430F2111__)
#include "msp430f2111.h"
#elif defined (__MSP430F2121__)
#include "msp430f2121.h"
#elif defined (__MSP430F2131__)
#include "msp430f2131.h"
#elif defined (__MSP430F2112__)
#include "msp430f2112.h"
#elif defined (__MSP430F2122__)
#include "msp430f2122.h"
#elif defined (__MSP430F2132__)
#include "msp430f2132.h"
#elif defined (__MSP430F2232__)
#include "msp430f2232.h"
#elif defined (__MSP430F2252__)
#include "msp430f2252.h"
#elif defined (__MSP430F2272__)
#include "msp430f2272.h"
#elif defined (__MSP430F2234__)
#include "msp430f2234.h"
#elif defined (__MSP430F2254__)
#include "msp430f2254.h"
#elif defined (__MSP430F2274__)
#include "msp430f2274.h"
#elif defined (__MSP430F2330__)
#include "msp430f2330.h"
#elif defined (__MSP430F2350__)
#include "msp430f2350.h"
#elif defined (__MSP430F2370__)
#include "msp430f2370.h"
#elif defined (__MSP430F233__)
#include "msp430f233.h"
#elif defined (__MSP430F235__)
#include "msp430f235.h"
#elif defined (__MSP430F247__)
#include "msp430f247.h"
#elif defined (__MSP430F248__)
#include "msp430f248.h"
#elif defined (__MSP430F249__)
#include "msp430f249.h"
#elif defined (__MSP430F2410__)
#include "msp430f2410.h"
#elif defined (__MSP430F2471__)
#include "msp430f2471.h"
#elif defined (__MSP430F2481__)
#include "msp430f2481.h"
#elif defined (__MSP430F2491__)
#include "msp430f2491.h"
#elif defined (__MSP430F2416__)
#include "msp430f2416.h"
#elif defined (__MSP430F2417__)
#include "msp430f2417.h"
#elif defined (__MSP430F2418__)
#include "msp430f2418.h"
#elif defined (__MSP430F2419__)
#include "msp430f2419.h"
#elif defined (__MSP430F2616__)
#include "msp430f2616.h"
#elif defined (__MSP430F2617__)
#include "msp430f2617.h"
#elif defined (__MSP430F2618__)
#include "msp430f2618.h"
#elif defined (__MSP430F2619__)
#include "msp430f2619.h"
#elif defined (__MSP430F412__)
#include "msp430f412.h"
#elif defined (__MSP430F413__)
#include "msp430f413.h"
#elif defined (__MSP430F415__)
#include "msp430f415.h"
#elif defined (__MSP430F417__)
#include "msp430f417.h"
#elif defined (__MSP430F4132__)
#include "msp430f4132.h"
#elif defined (__MSP430F4152__)
#include "msp430f4152.h"
#elif defined (__MSP430F423__)
#include "msp430f423.h"
#elif defined (__MSP430F425__)
#include "msp430f425.h"
#elif defined (__MSP430F427__)
#include "msp430f427.h"
#elif defined (__MSP430F423A__)
#include "msp430f423a.h"
#elif defined (__MSP430F425A__)
#include "msp430f425a.h"
#elif defined (__MSP430F427A__)
#include "msp430f427a.h"
#elif defined (__MSP430F435__)
#include "msp430f435.h"
#elif defined (__MSP430F436__)
#include "msp430f436.h"
#elif defined (__MSP430F437__)
#include "msp430f437.h"
#elif defined (__MSP430F4351__)
#include "msp430f4351.h"
#elif defined (__MSP430F4361__)
#include "msp430f4361.h"
#elif defined (__MSP430F4371__)
#include "msp430f4371.h"
#elif defined (__MSP430F4481__)
#include "msp430f4481.h"
#elif defined (__MSP430F4491__)
#include "msp430f4491.h"
#elif defined (__MSP430F447__)
#include "msp430f447.h"
#elif defined (__MSP430F448__)
#include "msp430f448.h"
#elif defined (__MSP430F449__)
#include "msp430f449.h"
#elif defined (__MSP430FE423__)
#include "msp430fe423.h"
#elif defined (__MSP430FE425__)
#include "msp430fe425.h"
#elif defined (__MSP430FE427__)
#include "msp430fe427.h"
#elif defined (__MSP430FE423A__)
#include "msp430fe423a.h"
#elif defined (__MSP430FE425A__)
#include "msp430fe425a.h"
#elif defined (__MSP430FE427A__)
#include "msp430fe427a.h"
#elif defined (__MSP430FE4232__)
#include "msp430fe4232.h"
#elif defined (__MSP430FE4242__)
#include "msp430fe4242.h"
#elif defined (__MSP430FE4252__)
#include "msp430fe4252.h"
#elif defined (__MSP430FE4272__)
#include "msp430fe4272.h"
#elif defined (__MSP430F4783__)
#include "msp430f4783.h"
#elif defined (__MSP430F4793__)
#include "msp430f4793.h"
#elif defined (__MSP430F4784__)
#include "msp430f4784.h"
#elif defined (__MSP430F4794__)
#include "msp430f4794.h"
#elif defined (__MSP430F47126__)
#include "msp430f47126.h"
#elif defined (__MSP430F47127__)
#include "msp430f47127.h"
#elif defined (__MSP430F47163__)
#include "msp430f47163.h"
#elif defined (__MSP430F47173__)
#include "msp430f47173.h"
#elif defined (__MSP430F47183__)
#include "msp430f47183.h"
#elif defined (__MSP430F47193__)
#include "msp430f47193.h"
#elif defined (__MSP430F47166__)
#include "msp430f47166.h"
#elif defined (__MSP430F47176__)
#include "msp430f47176.h"
#elif defined (__MSP430F47186__)
#include "msp430f47186.h"
#elif defined (__MSP430F47196__)
#include "msp430f47196.h"
#elif defined (__MSP430F47167__)
#include "msp430f47167.h"
#elif defined (__MSP430F47177__)
#include "msp430f47177.h"
#elif defined (__MSP430F47187__)
#include "msp430f47187.h"
#elif defined (__MSP430F47197__)
#include "msp430f47197.h"
#elif defined (__MSP430F4250__)
#include "msp430f4250.h"
#elif defined (__MSP430F4260__)
#include "msp430f4260.h"
#elif defined (__MSP430F4270__)
#include "msp430f4270.h"
#elif defined (__MSP430FG4250__)
#include "msp430fg4250.h"
#elif defined (__MSP430FG4260__)
#include "msp430fg4260.h"
#elif defined (__MSP430FG4270__)
#include "msp430fg4270.h"
#elif defined (__MSP430FW423__)
#include "msp430fw423.h"
#elif defined (__MSP430FW425__)
#include "msp430fw425.h"
#elif defined (__MSP430FW427__)
#include "msp430fw427.h"
#elif defined (__MSP430FW428__)
#include "msp430fw428.h"
#elif defined (__MSP430FW429__)
#include "msp430fw429.h"
#elif defined (__MSP430FG437__)
#include "msp430fg437.h"
#elif defined (__MSP430FG438__)
#include "msp430fg438.h"
#elif defined (__MSP430FG439__)
#include "msp430fg439.h"
#elif defined (__MSP430F438__)
#include "msp430f438.h"
#elif defined (__MSP430F439__)
#include "msp430f439.h"
#elif defined (__MSP430F477__)
#include "msp430f477.h"
#elif defined (__MSP430F478__)
#include "msp430f478.h"
#elif defined (__MSP430F479__)
#include "msp430f479.h"
#elif defined (__MSP430FG477__)
#include "msp430fg477.h"
#elif defined (__MSP430FG478__)
#include "msp430fg478.h"
#elif defined (__MSP430FG479__)
#include "msp430fg479.h"
#elif defined (__MSP430F46161__)
#include "msp430f46161.h"
#elif defined (__MSP430F46171__)
#include "msp430f46171.h"
#elif defined (__MSP430F46181__)
#include "msp430f46181.h"
#elif defined (__MSP430F46191__)
#include "msp430f46191.h"
#elif defined (__MSP430F4616__)
#include "msp430f4616.h"
#elif defined (__MSP430F4617__)
#include "msp430f4617.h"
#elif defined (__MSP430F4618__)
#include "msp430f4618.h"
#elif defined (__MSP430F4619__)
#include "msp430f4619.h"
#elif defined (__MSP430FG4616__)
#include "msp430fg4616.h"
#elif defined (__MSP430FG4617__)
#include "msp430fg4617.h"
#elif defined (__MSP430FG4618__)
#include "msp430fg4618.h"
#elif defined (__MSP430FG4619__)
#include "msp430fg4619.h"
#elif defined (__MSP430F5418__)
#include "msp430f5418.h"
#elif defined (__MSP430F5419__)
#include "msp430f5419.h"
#elif defined (__MSP430F5435__)
#include "msp430f5435.h"
#elif defined (__MSP430F5436__)
#include "msp430f5436.h"
#elif defined (__MSP430F5437__)
#include "msp430f5437.h"
#elif defined (__MSP430F5438__)
#include "msp430f5438.h"
#elif defined (__MSP430F5418A__)
#include "msp430f5418a.h"
#elif defined (__MSP430F5419A__)
#include "msp430f5419a.h"
#elif defined (__MSP430F5435A__)
#include "msp430f5435a.h"
#elif defined (__MSP430F5436A__)
#include "msp430f5436a.h"
#elif defined (__MSP430F5437A__)
#include "msp430f5437a.h"
#elif defined (__MSP430F5438A__)
#include "msp430f5438a.h"
#elif defined (__MSP430F5212__)
#include "msp430f5212.h"
#elif defined (__MSP430F5213__)
#include "msp430f5213.h"
#elif defined (__MSP430F5214__)
#include "msp430f5214.h"
#elif defined (__MSP430F5217__)
#include "msp430f5217.h"
#elif defined (__MSP430F5218__)
#include "msp430f5218.h"
#elif defined (__MSP430F5219__)
#include "msp430f5219.h"
#elif defined (__MSP430F5222__)
#include "msp430f5222.h"
#elif defined (__MSP430F5223__)
#include "msp430f5223.h"
#elif defined (__MSP430F5224__)
#include "msp430f5224.h"
#elif defined (__MSP430F5227__)
#include "msp430f5227.h"
#elif defined (__MSP430F5228__)
#include "msp430f5228.h"
#elif defined (__MSP430F5229__)
#include "msp430f5229.h"
#elif defined (__MSP430F5304__)
#include "msp430f5304.h"
#elif defined (__MSP430F5308__)
#include "msp430f5308.h"
#elif defined (__MSP430F5309__)
#include "msp430f5309.h"
#elif defined (__MSP430F5310__)
#include "msp430f5310.h"
#elif defined (__MSP430F5340__)
#include "msp430f5340.h"
#elif defined (__MSP430F5341__)
#include "msp430f5341.h"
#elif defined (__MSP430F5342__)
#include "msp430f5342.h"
#elif defined (__MSP430F5324__)
#include "msp430f5324.h"
#elif defined (__MSP430F5325__)
#include "msp430f5325.h"
#elif defined (__MSP430F5326__)
#include "msp430f5326.h"
#elif defined (__MSP430F5327__)
#include "msp430f5327.h"
#elif defined (__MSP430F5328__)
#include "msp430f5328.h"
#elif defined (__MSP430F5329__)
#include "msp430f5329.h"
#elif defined (__MSP430F5500__)
#include "msp430f5500.h"
#elif defined (__MSP430F5501__)
#include "msp430f5501.h"
#elif defined (__MSP430F5502__)
#include "msp430f5502.h"
#elif defined (__MSP430F5503__)
#include "msp430f5503.h"
#elif defined (__MSP430F5504__)
#include "msp430f5504.h"
#elif defined (__MSP430F5505__)
#include "msp430f5505.h"
#elif defined (__MSP430F5506__)
#include "msp430f5506.h"
#elif defined (__MSP430F5507__)
#include "msp430f5507.h"
#elif defined (__MSP430F5508__)
#include "msp430f5508.h"
#elif defined (__MSP430F5509__)
#include "msp430f5509.h"
#elif defined (__MSP430F5510__)
#include "msp430f5510.h"
#elif defined (__MSP430F5513__)
#include "msp430f5513.h"
#elif defined (__MSP430F5514__)
#include "msp430f5514.h"
#elif defined (__MSP430F5515__)
#include "msp430f5515.h"
#elif defined (__MSP430F5517__)
#include "msp430f5517.h"
#elif defined (__MSP430F5519__)
#include "msp430f5519.h"
#elif defined (__MSP430F5521__)
#include "msp430f5521.h"
#elif defined (__MSP430F5522__)
#include "msp430f5522.h"
#elif defined (__MSP430F5524__)
#include "msp430f5524.h"
#elif defined (__MSP430F5525__)
#include "msp430f5525.h"
#elif defined (__MSP430F5526__)
#include "msp430f5526.h"
#elif defined (__MSP430F5527__)
#include "msp430f5527.h"
#elif defined (__MSP430F5528__)
#include "msp430f5528.h"
#elif defined (__MSP430F5529__)
#include "msp430f5529.h"
#elif defined (__MSP430P112__)
#include "msp430p112.h"
#elif defined (__MSP430P313__)
#include "msp430p313.h"
#elif defined (__MSP430P315__)
#include "msp430p315.h"
#elif defined (__MSP430P315S__)
#include "msp430p315s.h"
#elif defined (__MSP430P325__)
#include "msp430p325.h"
#elif defined (__MSP430P337__)
#include "msp430p337.h"
#elif defined (__CC430F5133__)
#include "cc430f5133.h"
#elif defined (__CC430F5135__)
#include "cc430f5135.h"
#elif defined (__CC430F5137__)
#include "cc430f5137.h"
#elif defined (__CC430F6125__)
#include "cc430f6125.h"
#elif defined (__CC430F6126__)
#include "cc430f6126.h"
#elif defined (__CC430F6127__)
#include "cc430f6127.h"
#elif defined (__CC430F6135__)
#include "cc430f6135.h"
#elif defined (__CC430F6137__)
#include "cc430f6137.h"
#elif defined (__CC430F5123__)
#include "cc430f5123.h"
#elif defined (__CC430F5125__)
#include "cc430f5125.h"
#elif defined (__CC430F5143__)
#include "cc430f5143.h"
#elif defined (__CC430F5145__)
#include "cc430f5145.h"
#elif defined (__CC430F5147__)
#include "cc430f5147.h"
#elif defined (__CC430F6143__)
#include "cc430f6143.h"
#elif defined (__CC430F6145__)
#include "cc430f6145.h"
#elif defined (__CC430F6147__)
#include "cc430f6147.h"
#elif defined (__MSP430F5333__)
#include "msp430f5333.h"
#elif defined (__MSP430F5335__)
#include "msp430f5335.h"
#elif defined (__MSP430F5336__)
#include "msp430f5336.h"
#elif defined (__MSP430F5338__)
#include "msp430f5338.h"
#elif defined (__MSP430F5630__)
#include "msp430f5630.h"
#elif defined (__MSP430F5631__)
#include "msp430f5631.h"
#elif defined (__MSP430F5632__)
#include "msp430f5632.h"
#elif defined (__MSP430F5633__)
#include "msp430f5633.h"
#elif defined (__MSP430F5634__)
#include "msp430f5634.h"
#elif defined (__MSP430F5635__)
#include "msp430f5635.h"
#elif defined (__MSP430F5636__)
#include "msp430f5636.h"
#elif defined (__MSP430F5637__)
#include "msp430f5637.h"
#elif defined (__MSP430F5638__)
#include "msp430f5638.h"
#elif defined (__MSP430F6433__)
#include "msp430f6433.h"
#elif defined (__MSP430F6435__)
#include "msp430f6435.h"
#elif defined (__MSP430F6436__)
#include "msp430f6436.h"
#elif defined (__MSP430F6438__)
#include "msp430f6438.h"
#elif defined (__MSP430F6630__)
#include "msp430f6630.h"
#elif defined (__MSP430F6631__)
#include "msp430f6631.h"
#elif defined (__MSP430F6632__)
#include "msp430f6632.h"
#elif defined (__MSP430F6633__)
#include "msp430f6633.h"
#elif defined (__MSP430F6634__)
#include "msp430f6634.h"
#elif defined (__MSP430F6635__)
#include "msp430f6635.h"
#elif defined (__MSP430F6636__)
#include "msp430f6636.h"
#elif defined (__MSP430F6637__)
#include "msp430f6637.h"
#elif defined (__MSP430F6638__)
#include "msp430f6638.h"
#elif defined (__MSP430F5358__)
#include "msp430f5358.h"
#elif defined (__MSP430F5359__)
#include "msp430f5359.h"
#elif defined (__MSP430F5658__)
#include "msp430f5658.h"
#elif defined (__MSP430F5659__)
#include "msp430f5659.h"
#elif defined (__MSP430F6458__)
#include "msp430f6458.h"
#elif defined (__MSP430F6459__)
#include "msp430f6459.h"
#elif defined (__MSP430F6658__)
#include "msp430f6658.h"
#elif defined (__MSP430F6659__)
#include "msp430f6659.h"
#elif defined (__MSP430L092__)
#include "msp430l092.h"
#elif defined (__MSP430C091__)
#include "msp430c091.h"
#elif defined (__MSP430C092__)
#include "msp430c092.h"
#elif defined (__MSP430XGENERIC__)
#include "msp430xgeneric.h"
#elif defined (__MSP430F5131__)
#include "msp430f5131.h"
#elif defined (__MSP430F5151__)
#include "msp430f5151.h"
#elif defined (__MSP430F5171__)
#include "msp430f5171.h"
#elif defined (__MSP430F5132__)
#include "msp430f5132.h"
#elif defined (__MSP430F5152__)
#include "msp430f5152.h"
#elif defined (__MSP430F5172__)
#include "msp430f5172.h"
#elif defined (__MSP430F6720__)
#include "msp430f6720.h"
#elif defined (__MSP430F6721__)
#include "msp430f6721.h"
#elif defined (__MSP430F6723__)
#include "msp430f6723.h"
#elif defined (__MSP430F6724__)
#include "msp430f6724.h"
#elif defined (__MSP430F6725__)
#include "msp430f6725.h"
#elif defined (__MSP430F6726__)
#include "msp430f6726.h"
#elif defined (__MSP430F6730__)
#include "msp430f6730.h"
#elif defined (__MSP430F6731__)
#include "msp430f6731.h"
#elif defined (__MSP430F6733__)
#include "msp430f6733.h"
#elif defined (__MSP430F6734__)
#include "msp430f6734.h"
#elif defined (__MSP430F6735__)
#include "msp430f6735.h"
#elif defined (__MSP430F6736__)
#include "msp430f6736.h"
#elif defined (__MSP430F67451__)
#include "msp430f67451.h"
#elif defined (__MSP430F67651__)
#include "msp430f67651.h"
#elif defined (__MSP430F67751__)
#include "msp430f67751.h"
#elif defined (__MSP430F67461__)
#include "msp430f67461.h"
#elif defined (__MSP430F67661__)
#include "msp430f67661.h"
#elif defined (__MSP430F67761__)
#include "msp430f67761.h"
#elif defined (__MSP430F67471__)
#include "msp430f67471.h"
#elif defined (__MSP430F67671__)
#include "msp430f67671.h"
#elif defined (__MSP430F67771__)
#include "msp430f67771.h"
#elif defined (__MSP430F67481__)
#include "msp430f67481.h"
#elif defined (__MSP430F67681__)
#include "msp430f67681.h"
#elif defined (__MSP430F67781__)
#include "msp430f67781.h"
#elif defined (__MSP430F67491__)
#include "msp430f67491.h"
#elif defined (__MSP430F67691__)
#include "msp430f67691.h"
#elif defined (__MSP430F67791__)
#include "msp430f67791.h"
#elif defined (__MSP430F6745__)
#include "msp430f6745.h"
#elif defined (__MSP430F6765__)
#include "msp430f6765.h"
#elif defined (__MSP430F6775__)
#include "msp430f6775.h"
#elif defined (__MSP430F6746__)
#include "msp430f6746.h"
#elif defined (__MSP430F6766__)
#include "msp430f6766.h"
#elif defined (__MSP430F6776__)
#include "msp430f6776.h"
#elif defined (__MSP430F6747__)
#include "msp430f6747.h"
#elif defined (__MSP430F6767__)
#include "msp430f6767.h"
#elif defined (__MSP430F6777__)
#include "msp430f6777.h"
#elif defined (__MSP430F6748__)
#include "msp430f6748.h"
#elif defined (__MSP430F6768__)
#include "msp430f6768.h"
#elif defined (__MSP430F6778__)
#include "msp430f6778.h"
#elif defined (__MSP430F6749__)
#include "msp430f6749.h"
#elif defined (__MSP430F6769__)
#include "msp430f6769.h"
#elif defined (__MSP430F6779__)
#include "msp430f6779.h"
#elif defined (__MSP430FR5720__)
#include "msp430fr5720.h"
#elif defined (__MSP430FR5721__)
#include "msp430fr5721.h"
#elif defined (__MSP430FR5722__)
#include "msp430fr5722.h"
#elif defined (__MSP430FR5723__)
#include "msp430fr5723.h"
#elif defined (__MSP430FR5724__)
#include "msp430fr5724.h"
#elif defined (__MSP430FR5725__)
#include "msp430fr5725.h"
#elif defined (__MSP430FR5726__)
#include "msp430fr5726.h"
#elif defined (__MSP430FR5727__)
#include "msp430fr5727.h"
#elif defined (__MSP430FR5728__)
#include "msp430fr5728.h"
#elif defined (__MSP430FR5729__)
#include "msp430fr5729.h"
#elif defined (__MSP430FR5730__)
#include "msp430fr5730.h"
#elif defined (__MSP430FR5731__)
#include "msp430fr5731.h"
#elif defined (__MSP430FR5732__)
#include "msp430fr5732.h"
#elif defined (__MSP430FR5733__)
#include "msp430fr5733.h"
#elif defined (__MSP430FR5734__)
#include "msp430fr5734.h"
#elif defined (__MSP430FR5735__)
#include "msp430fr5735.h"
#elif defined (__MSP430FR5736__)
#include "msp430fr5736.h"
#elif defined (__MSP430FR5737__)
#include "msp430fr5737.h"
#elif defined (__MSP430FR5738__)
#include "msp430fr5738.h"
#elif defined (__MSP430FR5739__)
#include "msp430fr5739.h"
#elif defined (__MSP430G2211__)
#include "msp430g2211.h"
#elif defined (__MSP430G2201__)
#include "msp430g2201.h"
#elif defined (__MSP430G2111__)
#include "msp430g2111.h"
#elif defined (__MSP430G2101__)
#include "msp430g2101.h"
#elif defined (__MSP430G2001__)
#include "msp430g2001.h"
#elif defined (__MSP430G2231__)
#include "msp430g2231.h"
#elif defined (__MSP430G2221__)
#include "msp430g2221.h"
#elif defined (__MSP430G2131__)
#include "msp430g2131.h"
#elif defined (__MSP430G2121__)
#include "msp430g2121.h"
#elif defined (__MSP430AFE221__)
#include "msp430afe221.h"
#elif defined (__MSP430AFE231__)
#include "msp430afe231.h"
#elif defined (__MSP430AFE251__)
#include "msp430afe251.h"
#elif defined (__MSP430AFE222__)
#include "msp430afe222.h"
#elif defined (__MSP430AFE232__)
#include "msp430afe232.h"
#elif defined (__MSP430AFE252__)
#include "msp430afe252.h"
#elif defined (__MSP430AFE223__)
#include "msp430afe223.h"
#elif defined (__MSP430AFE233__)
#include "msp430afe233.h"
#elif defined (__MSP430AFE253__)
#include "msp430afe253.h"
#elif defined (__MSP430G2102__)
#include "msp430g2102.h"
#elif defined (__MSP430G2202__)
#include "msp430g2202.h"
#elif defined (__MSP430G2302__)
#include "msp430g2302.h"
#elif defined (__MSP430G2402__)
#include "msp430g2402.h"
#elif defined (__MSP430G2132__)
#include "msp430g2132.h"
#elif defined (__MSP430G2232__)
#include "msp430g2232.h"
#elif defined (__MSP430G2332__)
#include "msp430g2332.h"
#elif defined (__MSP430G2432__)
#include "msp430g2432.h"
#elif defined (__MSP430G2112__)
#include "msp430g2112.h"
#elif defined (__MSP430G2212__)
#include "msp430g2212.h"
#elif defined (__MSP430G2312__)
#include "msp430g2312.h"
#elif defined (__MSP430G2412__)
#include "msp430g2412.h"
#elif defined (__MSP430G2152__)
#include "msp430g2152.h"
#elif defined (__MSP430G2252__)
#include "msp430g2252.h"
#elif defined (__MSP430G2352__)
#include "msp430g2352.h"
#elif defined (__MSP430G2452__)
#include "msp430g2452.h"
#elif defined (__MSP430G2113__)
#include "msp430g2113.h"
#elif defined (__MSP430G2213__)
#include "msp430g2213.h"
#elif defined (__MSP430G2313__)
#include "msp430g2313.h"
#elif defined (__MSP430G2413__)
#include "msp430g2413.h"
#elif defined (__MSP430G2513__)
#include "msp430g2513.h"
#elif defined (__MSP430G2153__)
#include "msp430g2153.h"
#elif defined (__MSP430G2253__)
#include "msp430g2253.h"
#elif defined (__MSP430G2353__)
#include "msp430g2353.h"
#elif defined (__MSP430G2453__)
#include "msp430g2453.h"
#elif defined (__MSP430G2553__)
#include "msp430g2553.h"
#elif defined (__MSP430G2203__)
#include "msp430g2203.h"
#elif defined (__MSP430G2303__)
#include "msp430g2303.h"
#elif defined (__MSP430G2403__)
#include "msp430g2403.h"
#elif defined (__MSP430G2233__)
#include "msp430g2233.h"
#elif defined (__MSP430G2333__)
#include "msp430g2333.h"
#elif defined (__MSP430G2433__)
#include "msp430g2433.h"
#elif defined (__MSP430G2533__)
#include "msp430g2533.h"
#elif defined (__MSP430G2230__)
#include "msp430g2230.h"
#elif defined (__MSP430G2210__)
#include "msp430g2210.h"
#elif defined (__MSP430BT5190__)
#include "msp430bt5190.h"
#elif defined (__MSP430FR5949__)
#include "msp430fr5949.h"
#elif defined (__MSP430FR5969__)
#include "msp430fr5969.h"
#elif defined (__MSP430SL5438A__)
#include "msp430sl5438a.h"
/********************************************************************
* msp430 generic
********************************************************************/
#elif defined (__)
#error "msp430 generic device does not have a default include file"
#elif defined (__)
#error " generic device does not have a default include file"
/********************************************************************
*
********************************************************************/
#else
#error "Failed to match a default include file"
#endif
#endif /* #ifndef __msp430 */
我的理解是if 没有定义msp430,即定义msp430,进行下面的条件编译,但是这段
#elif defined (__MSP430F5529__)
#include "msp430f5529.h"
定义了(__MSP430F5529__),则打开头文件#include "msp430f5529.h" ,
可是在哪里有定义了这段呢?
请问是不是在文件建立之初的时候已经在哪里建立连接了,还是...?
另问:SEED-EXP430F5529 V1.0的板子,在拿到板子的时候下载一段程序,请问这段程序在哪里可以找到。辛苦了Lina Lian
关于MSP430F5529板子的初始例程,从下面链接下载对应安装包:MSP-EXP430F5529_UE-1.30.00.00-Setup.exe,安装后即可看到,默认路径应该为:C:\ti\msp430\MSP-EXP430F5529_UE_1_30_00_00\src
http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSPEXP430F5529UE/latest/index_FDS.html
另外,其实关于MSP430F5529板子的所有资料在下列文档均有提到:MSP-EXP430F5529 Experimenter Board User's Guide.