This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

430输出电压为2.26V



430F4270与三片SN74LV244的输出端连接,同时与两片SN74LV373的输入端连接,没有接上或下拉电阻。目的实现输入和输出的管理,但在测量时发现,VCC用的是AMS117,稳压后是3.27V,而4270的输出端口在高电平时是2.26V,低电平达到0.4V左右。好象不正常,并且此时的部电流达到73毫安。想咨询一下这其中是否电路上有需要注意的地方才出现这种情况或器件是否因手工焊接而有所损坏的可能。谢谢。

  • 这种情况不正常,F4270的高电平输出电压和负载电流大小有关系。负载电流越大,高电平输出电压越低。

    比如负载1.5mA, VOH=VCC-0.3V.当负载到了6mA时, VOH=VCC-0.6V.

    所以有可能是负载太大造成。