This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1 开发板上有一个RF1 + RF2 Header,根据手册说明
Used to connect a standard TI Wireless Evaluation Module Kit (EMK) such as the CC2530 or CC3000
无线模块的话,您可以在 该链接 查看详细信息
2 您可以在此获取BOM表,表内说明 TI 160 Segment LCD,型号是 ADKOM FH-1152P LCD
3 Complete metrology source code is provided and can be downloaded from www.ti.com/lit/zip/slaa517 for the MSP430F6736-based software and from www.ti.com/tool/TIDM-1PHMTR-ESD for the MSP430F6736A software.
user6611094 说:首先,那个RF1和RF2在手册中只有简单的描述,没有相关器件连接(CC2530连接在哪)。
CC2530EMK上也是有一个connector的,您可以看一下 该手册 的 Table 1 - CC2530EM pin-out
The table below shows the pin-out from the CC2530 to the two connectors on the backside of the evaluation module
user6611094 说:其次,我需要CC2530传输模块的外围电路;
您可以参考EMK的详细原理图,也是在上面的文档内有的
user6611094 说:该型号LCD的资料我没有找到,希望您能给我提供一下。
这个LCD不是TI的,您需要自行联系对应的厂商获取相关资料
user6611094 说:最后,手册里面的代码文件emeter-toolkit/DEBUG是不是只能用IAR打开,不能用CCS打开.
您可以看一下该链接的解决方案