This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-F6736资料需求

Other Parts Discussed in Thread: EVM430-F6736, CC2530, MSP430F6736A, TIDM-1PHMTR-ESD, CC2530EMK, CC2530EM
Hi team
Good day
客户需要一些资料,能否帮忙提供:
1、需要与EVM430-F6736能够连接的无线传输模块(WIFI或ZIGBEE)的资料
2、需要EVM430-F6736评估版的LCD(44引脚)相关资料
3、需要基于EVM430-F6736评估版的单相电表(能够实现用户手册里的电气参数的测量,包括电流、电压、有功无功功率、有功和无功电能、功率因数,频率等)的相关代码,需要整个project。多谢
Regards
Aosker
  • 1 开发板上有一个RF1 + RF2 Header,根据手册说明

    Used to connect a standard TI Wireless Evaluation Module Kit (EMK) such as the CC2530 or CC3000

    无线模块的话,您可以在 该链接 查看详细信息

    2 您可以在此获取BOM表,表内说明 TI 160 Segment LCD,型号是 ADKOM FH-1152P LCD

    3 Complete metrology source code is provided and can be downloaded from www.ti.com/lit/zip/slaa517 for the MSP430F6736-based software and from www.ti.com/tool/TIDM-1PHMTR-ESD for the MSP430F6736A software.

  • 非常感谢您的解答,我还有一点疑惑您解答一下。
    首先,那个RF1和RF2在手册中只有简单的描述,没有相关器件连接(CC2530连接在哪)。
    其次,我需要CC2530传输模块的外围电路;该型号LCD的资料我没有找到,希望您能给我提供一下。
    最后,手册里面的代码文件emeter-toolkit/DEBUG是不是只能用IAR打开,不能用CCS打开.
  • user6611094 说:
    首先,那个RF1和RF2在手册中只有简单的描述,没有相关器件连接(CC2530连接在哪)。

    CC2530EMK上也是有一个connector的,您可以看一下 该手册 的 Table 1 - CC2530EM pin-out

    The table below shows the pin-out from the CC2530 to the two connectors on the backside of the evaluation module

    user6611094 说:
    其次,我需要CC2530传输模块的外围电路;

    您可以参考EMK的详细原理图,也是在上面的文档内有的

    user6611094 说:
    该型号LCD的资料我没有找到,希望您能给我提供一下。

    这个LCD不是TI的,您需要自行联系对应的厂商获取相关资料

    user6611094 说:
    最后,手册里面的代码文件emeter-toolkit/DEBUG是不是只能用IAR打开,不能用CCS打开.

    您可以看一下该链接的解决方案