This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2418: 关于ADC12 通道1的问题

Part Number: MSP430F2418


我想使用ADC12的通道1来测量电池电压,芯片的ADC12通道1对应的引脚为P6.1

 硬件电路如图,VCC为12V,P6.1脚上的分压为2V

使用例程为MSP430x261x_adc12_05.c

 我将例程的io口改为从默认的P6.0改为P6.1,但是中断标志中通道1的标志一直没有置位

是我少改了什么地方吗?