This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2433: MSP430FR2433的RTC配置万年历

Part Number: MSP430FR2433

RTC是不是不支持万年历的制作?如果支持,有相关例程参考吗

  • RTC是不是不支持万年历的制作?

    可以做万年历的,但是目前没有直接的例程

    在之前的MSP430FR5xx/6xx 器件为其 RTC 内置了日历功能,但是FR2系列是没有内置日历功能的,您需要自己实现

  • 2433的RTC当前是否只支持计数器模式,为何参照例程RTC无法进入中断呢,

  • 2433的RTC当前是否只支持计数器模式

    是的,根据手册说明,目前只有计数器模式

    为何参照例程RTC无法进入中断呢,

    能否详细说明下?哪一个例程?

  • 您是使用开发板测试的?自己板子的话,是否有外接32768Hz晶振?

  • 我是用自己的板子,貌似是没有外接。

  • 这个例程是需要外接的

  • 好的,谢谢,除此之外还有别的RTC例程吗,我貌似没有找到

  • 就只有2个例程,都是需要外接晶振的

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2014, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     *
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //   MSP430FR243x Demo - RTC, device enter LPM3.5 and toggle P1.0 in RTC
    //                       interrupt handling every 1s
    //
    //
    //   Description: Device enter LPM3.5 after configuring the RTC. The RTC wakes
    //   the device up from LPM3.5 every second and toggles P1.0.
    //   It also stores the state of P0OUT in the Backup RAM Registers.
    //
    //   XT1 = 32kHz, ACLK = default, MCLK = SMCLK = default, DCODIV = ~1MHz.
    //
    //            MSP430FR2433
    //         -----------------
    //     /|\|                 |
    //      | |                 |
    //      | |        XIN(P2.0)|--
    //      --|RST              |  ~32768Hz
    //        |       XOUT(P2.1)|--
    //        |                 |
    //        |             P1.0|-->LED
    //
    //  Ling Zhu
    //  Texas Instruments Inc.
    //  Jan 2014
    //  Built with IAR Embedded Workbench v6.20 & Code Composer Studio v6.0.1
    //******************************************************************************
    #include <msp430.h>
    
    void initGpio(void);
    
    int main(void)
    {
        WDTCTL = WDTPW | WDTHOLD;               // Stop WDT
    
        initGpio();                             // Configure GPIO
    
        // Initialize XT1 32kHz crystal
        P2SEL0 |= BIT0 | BIT1;                  // set XT1 pin as second function
        do
        {
            CSCTL7 &= ~(XT1OFFG | DCOFFG);      // Clear XT1 and DCO fault flag
            SFRIFG1 &= ~OFIFG;
        } while (SFRIFG1 & OFIFG);              // Test oscillator fault flag
    
        // First determine whether we are coming out of an LPMx.5 or a regular RESET.
        if (SYSRSTIV == SYSRSTIV_LPM5WU)        // When woken up from LPM3.5, reinit
        {
            // If MCU wakes up from LPM3.5, re-init and then return to LPM3.5 again.
    
            // Restore P1OUT value from backup RAM memory, keep P1OUT after LPMx.5 reset
            P1OUT = *(unsigned int *)BKMEM_BASE;
    
            __enable_interrupt();               // The RTC interrupt should trigger now...
        }
        else
        {
            // Device powered up from a cold start.
            // It configures the device and puts the device into LPM3.5
    
            // Configure backup memory
            *(unsigned int *)BKMEM_BASE = 0;
    
            // Initialize RTC
            // Interrupt and reset happen every 1024/32768 * 32 = 1 sec.
            RTCMOD = 32-1;
            RTCCTL = RTCSS__XT1CLK | RTCSR | RTCPS__1024 | RTCIE;
    
            // Store P1OUT value in backup memory register before enter LPM3.5
            *(unsigned int *)BKMEM_BASE = P1OUT;
        }
    
        // Enter LPM3.5 mode with interrupts enabled. Note that this operation does
        // not return. The LPM3.5 will exit through a RESET event, resulting in a
        // re-start of the code.
        PMMCTL0_H = PMMPW_H;                    // Open PMM Registers for write
        PMMCTL0_L |= PMMREGOFF;                 // and set PMMREGOFF
        __bis_SR_register(LPM3_bits | GIE);
        __no_operation();
    
        return 0;
    }
    
    void initGpio(void)
    {
        P1DIR = 0xFF; P2DIR = 0xFF; P3DIR = 0xFF;
        P1REN = 0xFF; P2REN = 0xFF; P3REN = 0xFF;
        P1OUT = 0x00; P2OUT = 0x00; P3OUT = 0x00;
    
        // Disable the GPIO power-on default high-impedance mode
        // to activate previously configured port settings
        PM5CTL0 &= ~LOCKLPM5;
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector = RTC_VECTOR
    __interrupt void RTC_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(RTC_VECTOR))) RTC_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
        switch(__even_in_range(RTCIV, RTCIV_RTCIF))
        {
            case RTCIV_NONE : break;            // No interrupt pending
            case RTCIV_RTCIF:                   // RTC Overflow
                // Toggle LED on P1.0
                P1OUT ^= BIT0;
    
                // Store P1OUT value in backup memory register
                *(unsigned int *)BKMEM_BASE = P1OUT;
                break;
            default:          break;
        }
    }