This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

430所有系列中引脚都可以耐压5v输入吗?



430所有系列中都可以耐压5v输入吗?

5v输入到430引脚上到底会不会损坏430呢?有的朋友说耐压5v有的说不能。。。

  • 如果单片机支持5V供电引脚耐5V没有问题。

    不支持5V工作电压的单片机,如果记忆没错的话,一般AD功能引脚耐压高些,可以耐5V。安全方法是引脚上串联200R左右电阻就可以接5V信号了

  • 楼主你好!

    1、只有msp430F51X1 MSP430F51X2 部分IO可以5V耐压。任何过压都会有可能导致IO击穿。作为产品,不推荐任何超过手册范围的应用。

    如果需要电平转换,请使用电平转换IC。

    2、在做实验的过程中,并不是所有的超过极限指标的使用都会导致IC损坏。但是这种实验,并不能作为产品设计的依据。

  • 最好别,这样有很多问题,我最近在pic上都遇到这样的问题。430就不仅仅是功能实现的问题,还有烧毁硬件的风险,建议不要这么做。

  • 你好:

    MSP430有些系列是支持5V GPIO耐压,所以一定要看清楚你所选择的系列,如果不是,那么一定要采取措施,电阻分压或者电平转换芯片,这个根据具体应用。

    谢谢。