Part Number: MSP430FR2433
Other Parts Discussed in Thread: MSP-EXP430FR2433
msp430fr243x_euscia0_spi_09.c (ti.com)
msp430fr243x_euscia0_spi_10.c (ti.com)
我们使用两个MSP-EXP430FR2433模块测试上述两个示例代码功能,但是在CCS内查看对应参数配置,好像没有数据传输?可以解释一下这两个示例代码吗?我们该怎样查看示例代码是否工作正常?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR2433
Other Parts Discussed in Thread: MSP-EXP430FR2433
msp430fr243x_euscia0_spi_09.c (ti.com)
msp430fr243x_euscia0_spi_10.c (ti.com)
我们使用两个MSP-EXP430FR2433模块测试上述两个示例代码功能,但是在CCS内查看对应参数配置,好像没有数据传输?可以解释一下这两个示例代码吗?我们该怎样查看示例代码是否工作正常?
可以解释一下这两个示例代码吗?
示例说明可以在您给出的链接内查看
//******************************************************************************
// MSP430FR243x Demo - eUSCI_A0, SPI 3-Wire Master Incremented Data
//
// Description: SPI master talks to SPI slave using 3-wire mode. Incrementing
// data is sent by the master starting at 0x01. Received data is expected to
// be same as the previous transmission TXData = RXData-1.
//******************************************************************************
// MSP430FR243x Demo - eUSCI_A0, SPI 3-Wire Slave Data Echo
//
// Description: SPI slave talks to SPI master using 3-wire mode. Data received
// from master is echoed back.
但是在CCS内查看对应参数配置,好像没有数据传输
您是按照图示来连接两个板子的?观察的是 RXData 和 TXData?
Hi Susan Yang
我使用两个个MSP-EXP430FR2433模块分别烧录msp430fr243x_euscia0_spi_09.c和msp430fr243x_euscia0_spi_10.c示例代码。
我尝试在master这端添加断点参数打印,读取到的RXData和UCA0TXBUF不会有任何改变,RXData一直是255,UCA0TXBUF一直是0x00050E,。我保证从设备先于主设备工作。
附上我的测试代码
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2014, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430FR243x Demo - eUSCI_A0, SPI 3-Wire Master Incremented Data
//
// Description: SPI master talks to SPI slave using 3-wire mode. Incrementing
// data is sent by the master starting at 0x01. Received data is expected to
// be same as the previous transmission TXData = RXData-1.
// USCI RX ISR is used to handle communication with the CPU, normally in LPM0.
// ACLK = ~32.768kHz, MCLK = SMCLK = DCO ~ 1MHz. BRCLK = SMCLK/2.
//
//
// MSP430FR2433
// -----------------
// /|\| |
// | | |
// --|RST |
// | |
// | P1.4|-> Data In (UCA0SIMO)
// | |
// | P1.5|<- Data OUT (UCA0SOMI)
// | |
// | P1.6|-> Serial Clock Out (UCA0CLK)
//
//
// Ling Zhu
// Texas Instruments Inc.
// Sept 2015
// Built with IAR Embedded Workbench v6.20 & Code Composer Studio v6.0.1
//******************************************************************************
#include <msp430.h>
unsigned char RXData = 0;
unsigned char TXData;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
P1SEL0 |= BIT4 | BIT5 | BIT6; // set 3-SPI pin as second function
UCA0CTLW0 |= UCSWRST; // **Put state machine in reset**
UCA0CTLW0 |= UCMST|UCSYNC|UCCKPL|UCMSB; // 3-pin, 8-bit SPI master
// Clock polarity high, MSB
UCA0CTLW0 |= UCSSEL__SMCLK; // SMCLK
UCA0BR0 = 0x01; // /1, fBitClock = fBRCLK/UCBRx
UCA0BR1 = 0; //
UCA0MCTLW = 0; // No modulation
UCA0CTLW0 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
TXData = 0x01; // Holds TX data
PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode
// to activate previously configured port settings
while(1)
{
UCA0IE |= UCTXIE; // Enable TX interrupt
__bis_SR_register(LPM0_bits | GIE); // enable global interrupts, enter LPM0
__no_operation(); // For debug,Remain in LPM0
__delay_cycles(2000); // Delay before next transmission
TXData++; // Increment transmit data
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA0IV,USCI_SPI_UCTXIFG))
{
case USCI_NONE: break; // Vector 0 - no interrupt
case USCI_SPI_UCRXIFG:
RXData = UCA0RXBUF;
UCA0IFG &= ~UCRXIFG;
__bic_SR_register_on_exit(LPM0_bits);// Wake up to setup next TX
break;
case USCI_SPI_UCTXIFG:
UCA0TXBUF = TXData; // Transmit characters
UCA0IE &= ~UCTXIE;
break;
default: break;
}
}