Part Number: MSP430F5529
在设置TA 2定时器捕获的时候,同时使能了TA2CCR1和TA2CCR2捕获中断,但设置断点检查isr 中TA2CCR2的中断始终进不去,只能进CCR1,即使单独使能CCR2捕获中断也不能进,二者使用的是完全相同的driverlib库函数进行配置,在使用TB0.5和TB0.6的时候也遇到了相同的问题,只有前者能够进入中断,请问是什么原因呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F5529
在设置TA 2定时器捕获的时候,同时使能了TA2CCR1和TA2CCR2捕获中断,但设置断点检查isr 中TA2CCR2的中断始终进不去,只能进CCR1,即使单独使能CCR2捕获中断也不能进,二者使用的是完全相同的driverlib库函数进行配置,在使用TB0.5和TB0.6的时候也遇到了相同的问题,只有前者能够进入中断,请问是什么原因呢?
即使单独使能CCR2捕获中断也不能进,
是不是您的中断向量没有设置正确?若是可以,请给出单独使用TA2CCR2的相关代码
void TimerA2_Init()
{
//Set 2.5 to capture input direction
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P2,
GPIO_PIN5
);
//Start timer in continuous mode sourced by SMCLK=1.048MHz
Timer_A_clearTimerInterrupt(TIMER_A2_BASE);
Timer_A_initContinuousModeParam initContParam = {0};
initContParam.clockSource = TIMER_A_CLOCKSOURCE_SMCLK;
initContParam.clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_1;
initContParam.timerInterruptEnable_TAIE = TIMER_A_TAIE_INTERRUPT_ENABLE;
initContParam.timerClear = TIMER_A_DO_CLEAR;
initContParam.startTimer = false;
Timer_A_initContinuousMode(TIMER_A2_BASE, &initContParam);
//Initiate capture mode --TA2.2
Timer_A_initCaptureModeParam initCapParam1 = {0};
initCapParam1.captureRegister=TIMER_A_CAPTURECOMPARE_REGISTER_2; //根据管脚选择
initCapParam1.captureMode=TIMER_A_CAPTUREMODE_RISING_EDGE;
initCapParam1.captureInputSelect=TIMER_A_CAPTURE_INPUTSELECT_CCIxA;
initCapParam1.synchronizeCaptureSource=TIMER_A_CAPTURE_SYNCHRONOUS;
initCapParam1.captureInterruptEnable=TIMER_A_CAPTURECOMPARE_INTERRUPT_ENABLE;
initCapParam1.captureOutputMode=TIMER_A_OUTPUTMODE_OUTBITVALUE;
Timer_A_initCaptureMode(TIMER_A2_BASE, &initCapParam1);
Timer_A_enableCaptureCompareInterrupt(TIMER_A2_BASE,
TIMER_A_CAPTURECOMPARE_REGISTER_2);
Timer_A_startCounter( TIMER_A2_BASE,
TIMER_A_CONTINUOUS_MODE
);
}
// Timer A2 interrupt service routine
#pragma vector=TIMER2_A1_VECTOR
__interrupt void TIMER2_A1_ISR (void)
{
switch(__even_in_range(TA2IV,14)){
case TA2IV_TA2CCR1: //捕获中断
if(getspeed_L){
if(!flag_cap_A2){
caphead_A2=TA2CCR1;
flag_cap_A2=1;
TA2CCTL1&=~0x03; //COV和标志位清零
break;
}
if(flag_cap_A2){
captail_A2=TA2CCR1;
capgap_A2=captail_A2-caphead_A2;
flag_cap_A2=0;
capfinished_A2=1;
TA2CCTL1&=~0x03; //COV和标志位清零
break;
}
}
TA2CCTL1&=~0x03; //COV和标志位清零
break;
case TA2IV_TA2CCR2: //捕获中断
//count_impulse++;
if(getspeed_R){
if(!flag_cap_A2){
caphead_A2=TA2CCR2;
flag_cap_A2=1;
TA2CCTL2&=~0x03; //COV和标志位清零
break;
}
if(flag_cap_A2){
captail_A2=TA2CCR2;
capgap_A2=captail_A2-caphead_A2;
flag_cap_A2=0;
capfinished_A2=1;
TA2CCTL2&=~0x03; //COV和标志位清零
break;
}
}
TA2CCTL2&=~0x03; //COV和标志位清零
break;
case TA2IV_TAIFG: //溢出中断
if(flag_cap_A2)
ovcount_A2++;
break;
default: break;
}
}
单独使用的代码如上
当前测试工程如上,使用的是msp4305529launchpad开发板,刚刚测试还是相同的问题,同时检查发现P2.5(即TA2.2)始终为接地状态,导致无法触发捕获中断(已排除外部电路连接)
目前我是使用寄存器的例程来修改的,您可以在开发板上连接 P2.2 和 P2.4
因为目前对MSP430,我还是比较习惯寄存器例程
代码如下,请您对照一下相关配置
#include <msp430.h>
volatile unsigned int counter;
volatile unsigned int prev_counter;
unsigned int difference;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD;
// CAPTURE INPUT
P2DIR &= ~BIT4;
P2SEL |= BIT4;
//PWM OUTPUT
P2DIR |= BIT0+BIT1; // P2.0 and P2.1 output
P2SEL |= BIT0+BIT1; // P2.0 and P2.1 options select
TA1CCR0 = 512-1; // PWM Period
TA1CCTL1 = OUTMOD_7; // CCR1 reset/set
TA1CCR1 = 384; // CCR1 PWM duty cycle
TA1CCTL2 = OUTMOD_7; // CCR2 reset/set
TA1CCR2 = 128; // CCR2 PWM duty cycle
TA1CTL = TASSEL_2 + MC_1 + TACLR; // SMCLK, up mode, clear TAR
//capture config
TA2CTL = TASSEL_2 + MC_2;
TA2CCTL1 = CM_3+SCS+CAP+CCIS_0+CCIE;
while(1) {
__bis_SR_register(LPM0_bits + GIE);
__no_operation();
// break point here
difference = counter - prev_counter;
if(TA2CCTL1 & COV) {
TA2CCTL1 &= ~COV;
}
}
}
#pragma vector = TIMER2_A1_VECTOR
__interrupt void TIMER2_A1_ISR (void)
{
switch(__even_in_range(TA2IV,14))
{
case TA2IV_NONE: break;
case TA2IV_TACCR1:
prev_counter = counter;
counter = TA2CCR1;
__bic_SR_register_on_exit(LPM0_bits + GIE);
break;
case TA2IV_TACCR2: break;
case TA2IV_5: break;
case TA2IV_6: break;
case TA2IV_TAIFG: break;
default: break;
}
}