为什么我从FRAM存储器的地址读取值一直读取不到,麻烦可以提供一下FRAM读取操作的正确代码吗
Fullscreen
1
2
3
4
5
void FRAMRead_str (char index)
{
char *Fram_ptr = ((char *)FRAM_TEST_START) + index;
return *Fram_ptr;
}
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
为什么我从FRAM存储器的地址读取值一直读取不到,麻烦可以提供一下FRAM读取操作的正确代码吗
void FRAMRead_str (char index) { char *Fram_ptr = ((char *)FRAM_TEST_START) + index; return *Fram_ptr; }
您是否有参考例程?
https://dev.ti.com/tirex/explore/node?node=ADEFKoeyVMLgIZuOHPzCvQ__IOGqZri__LATEST
/* --COPYRIGHT--,BSD_EX * Copyright (c) 2014, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP430FR243x Demo - Long word writes to FRAM // // Description: Use long word write to write to 512 byte blocks of FRAM. // Toggle LED after every 100 writes. // ACLK = REFO, MCLK = SMCLK = default DCODIV = ~1MHz // // It is recommended to disable interrupt while code is writing to main FRAM, // because it is dangerous for running the interrupt services routine with // PFWP disabled. // This code examples is using DFWP which wouldn't have dangerous. But it is // recommended to disable interrupt if user is using PFWP. // // MSP430FR2433 // --------------- // /|\| | // | | | // --|RST | // | | // | P1.0 |---> LED // // Ling Zhu // Texas Instruments Inc. // Feb 2015 // Built with IAR Embedded Workbench v6.20 & Code Composer Studio v6.0.1 //****************************************************************************** #include <msp430.h> void FRAMWrite(void); unsigned char count = 0; unsigned long *FRAM_write_ptr; unsigned long data; #define FRAM_TEST_START 0x1800 int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer P1OUT &= ~BIT0; // Clear P1.0 output latch for a defined power-on state P1DIR |= BIT0; // Set P1.0 to output directionOUT PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode // to activate previously configured port settings data = 0x11111111; // Initialize dummy data while(1) { data += 0x00010001; FRAM_write_ptr = (unsigned long *)FRAM_TEST_START; FRAMWrite(); count++; if (count > 100) { P1OUT ^= 0x01; // Toggle LED to show 512 bytes count = 0; // have been written data = 0x11111111; } } } void FRAMWrite (void) { unsigned int i=0; SYSCFG0 = FRWPPW | PFWP; for (i = 0; i < 128; i++) { *FRAM_write_ptr++ = data; } SYSCFG0 = FRWPPW | PFWP | DFWP; }