Part Number: MSP430G2553
Other Parts Discussed in Thread: MSP430F5438A,
使用官方例程 msp430g2xx3_usci_i2c_standard_slave.c 代码 板子为官方 msp-exp430g2 时 无响应,连I2C起始 中断都不进入,测量P1.6 P1.7电压波形一切正常!有人用过MSP430 硬件I2C从机模式吗?之前试过MSP430F5438A,使用官方例程也没成功.附上官方例程代码
//******************************************************************************
// MSP430G2xx3 Demo - USCI_B0, I2C Slave multiple byte TX/RX
//
// Description: I2C master communicates to I2C slave sending and receiving
// 3 different messages of different length. (This is the slave code). The
// slave will be in LPM0 mode, waiting for the master to initiate the
// communication. The slave will send/receive bytes based on the master's
// request. The slave will handle I2C bytes sent/received using the
// I2C interrupt.
// ACLK = NA, MCLK = SMCLK = DCO 16MHz.
//
//
// MSP430G2553 3.3V
// ----------------- /|\ /|\
// /|\ | | | 4.7k
// | | | 4.7k |
// ---|RST | | |
// | | | |
// | P1.6|---|---+- I2C Clock (UCB0SCL)
// | | |
// | P1.7|---+----- I2C Data (UCB0SDA)
// | |
// | |
//
// Nima Eskandari
// Texas Instruments Inc.
// April 2017
// Built with CCS V7.0
//******************************************************************************
#include <msp430.h>
#include <stdint.h>
//******************************************************************************
// Example Commands ************************************************************
//******************************************************************************
#define SLAVE_ADDR 0x48
/* CMD_TYPE_X_SLAVE are example commands the master sends to the slave.
* The slave will send example SlaveTypeX buffers in response.
*
* CMD_TYPE_X_MASTER are example commands the master sends to the slave.
* The slave will initialize itself to receive MasterTypeX example buffers.
* */
#define CMD_TYPE_0_SLAVE 0
#define CMD_TYPE_1_SLAVE 1
#define CMD_TYPE_2_SLAVE 2
#define CMD_TYPE_0_MASTER 3
#define CMD_TYPE_1_MASTER 4
#define CMD_TYPE_2_MASTER 5
#define TYPE_0_LENGTH 1
#define TYPE_1_LENGTH 2
#define TYPE_2_LENGTH 6
#define MAX_BUFFER_SIZE 20
/* MasterTypeX are example buffers initialized in the master, they will be
* sent by the master to the slave.
* SlaveTypeX are example buffers initialized in the slave, they will be
* sent by the slave to the master.
* */
uint8_t MasterType2 [TYPE_2_LENGTH] = {0};
uint8_t MasterType1 [TYPE_1_LENGTH] = { 0, 0};
uint8_t MasterType0 [TYPE_0_LENGTH] = { 0};
uint8_t SlaveType2 [TYPE_2_LENGTH] = {'A', 'B', 'C', 'D', '1', '2'};
uint8_t SlaveType1 [TYPE_1_LENGTH] = {15, 16};
uint8_t SlaveType0 [TYPE_0_LENGTH] = {12};
//******************************************************************************
// General I2C State Machine ***************************************************
//******************************************************************************
typedef enum I2C_ModeEnum{
IDLE_MODE,
NACK_MODE,
TX_REG_ADDRESS_MODE,
RX_REG_ADDRESS_MODE,
TX_DATA_MODE,
RX_DATA_MODE,
SWITCH_TO_RX_MODE,
SWITHC_TO_TX_MODE,
TIMEOUT_MODE
} I2C_Mode;
/* Used to track the state of the software state machine*/
I2C_Mode SlaveMode = RX_REG_ADDRESS_MODE;
/* The Register Address/Command to use*/
uint8_t ReceiveRegAddr = 0;
/* ReceiveBuffer: Buffer used to receive data in the ISR
* RXByteCtr: Number of bytes left to receive
* ReceiveIndex: The index of the next byte to be received in ReceiveBuffer
* TransmitBuffer: Buffer used to transmit data in the ISR
* TXByteCtr: Number of bytes left to transfer
* TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer
* */
uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t RXByteCtr = 0;
uint8_t ReceiveIndex = 0;
uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t TXByteCtr = 0;
uint8_t TransmitIndex = 0;
/* Initialized the software state machine according to the received cmd
*
* cmd: The command/register address received
* */
void I2C_Slave_ProcessCMD(uint8_t cmd);
/* The transaction between the slave and master is completed. Uses cmd
* to do post transaction operations. (Place data from ReceiveBuffer
* to the corresponding buffer based in the last received cmd)
*
* cmd: The command/register address corresponding to the completed
* transaction
*/
void I2C_Slave_TransactionDone(uint8_t cmd);
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count);
void I2C_Slave_ProcessCMD(uint8_t cmd)
{
ReceiveIndex = 0;
TransmitIndex = 0;
RXByteCtr = 0;
TXByteCtr = 0;
switch (cmd)
{
case (CMD_TYPE_0_SLAVE): //Send slave device id (This device's id)
SlaveMode = TX_DATA_MODE;
TXByteCtr = TYPE_0_LENGTH;
//Fill out the TransmitBuffer
CopyArray(SlaveType0, TransmitBuffer, TYPE_0_LENGTH);
IE2 &= ~UCB0RXIE; // Disable RX interrupt
IE2 |= UCB0TXIE; // Enable TX interrupt
break;
case (CMD_TYPE_1_SLAVE): //Send slave device time (This device's time)
SlaveMode = TX_DATA_MODE;
TXByteCtr = TYPE_1_LENGTH;
//Fill out the TransmitBuffer
CopyArray(SlaveType1, TransmitBuffer, TYPE_1_LENGTH);
IE2 &= ~UCB0RXIE; // Disable RX interrupt
IE2 |= UCB0TXIE; // Enable TX interrupt
break;
case (CMD_TYPE_2_SLAVE): //Send slave device location (This device's location)
SlaveMode = TX_DATA_MODE;
TXByteCtr = TYPE_2_LENGTH;
//Fill out the TransmitBuffer
CopyArray(SlaveType2, TransmitBuffer, TYPE_2_LENGTH);
IE2 &= ~UCB0RXIE; // Disable RX interrupt
IE2 |= UCB0TXIE; // Enable TX interrupt
break;
case (CMD_TYPE_0_MASTER):
SlaveMode = RX_DATA_MODE;
RXByteCtr = TYPE_0_LENGTH;
IE2 &= ~UCB0TXIE; // Disable RX interrupt
IE2 |= UCB0RXIE; // Enable TX interrupt
break;
case (CMD_TYPE_1_MASTER):
SlaveMode = RX_DATA_MODE;
RXByteCtr = TYPE_1_LENGTH;
IE2 &= ~UCB0TXIE; // Disable RX interrupt
IE2 |= UCB0RXIE; // Enable TX interrupt
break;
case (CMD_TYPE_2_MASTER):
SlaveMode = RX_DATA_MODE;
RXByteCtr = TYPE_2_LENGTH;
IE2 &= ~UCB0TXIE; // Disable RX interrupt
IE2 |= UCB0RXIE; // Enable TX interrupt
break;
default:
__no_operation();
break;
}
}
void I2C_Slave_TransactionDone(uint8_t cmd)
{
switch (cmd)
{
case (CMD_TYPE_0_SLAVE): //Slave device id was sent(This device's id)
break;
case (CMD_TYPE_1_SLAVE): //Slave device time was sent(This device's time)
break;
case (CMD_TYPE_2_SLAVE): //Send slave device location (This device's location)
break;
case (CMD_TYPE_0_MASTER):
CopyArray(ReceiveBuffer, MasterType0, TYPE_0_LENGTH);
break;
case (CMD_TYPE_1_MASTER):
CopyArray(ReceiveBuffer, MasterType1, TYPE_1_LENGTH);
break;
case (CMD_TYPE_2_MASTER):
CopyArray(ReceiveBuffer, MasterType2, TYPE_2_LENGTH);
break;
default:
__no_operation();
break;
}
}
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
uint8_t copyIndex = 0;
for (copyIndex = 0; copyIndex < count; copyIndex++)
{
dest[copyIndex] = source[copyIndex];
}
}
//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************
void initClockTo16MHz()
{
if (CALBC1_16MHZ==0xFF) // If calibration constant erased
{
while(1); // do not load, trap CPU!!
}
DCOCTL = 0; // Select lowest DCOx and MODx settings
BCSCTL1 = CALBC1_16MHZ; // Set DCO
DCOCTL = CALDCO_16MHZ;
}
void initGPIO()
{
P1SEL |= BIT6 + BIT7; // Assign I2C pins to USCI_B0
P1SEL2|= BIT6 + BIT7; // Assign I2C pins to USCI_B0
}
void initI2C()
{
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMODE_3 + UCSYNC; // I2C Slave, synchronous mode
UCB0I2COA = SLAVE_ADDR; // Own Address
UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
UCB0I2CIE |= UCSTPIE + UCSTTIE; // Enable STT and STP interrupt
IE2 |= UCB0RXIE; // Enable RX interrupt
}
//******************************************************************************
// Main ************************************************************************
// Enters LPM0 and waits for I2C interrupts. The data sent from the master is *
// then interpreted and the device will respond accordingly *
//******************************************************************************
int main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
initClockTo16MHz();
initGPIO();
initI2C();
__bis_SR_register(LPM0_bits + GIE);
return 0;
}
//******************************************************************************
// I2C Interrupt For Received and Transmitted Data******************************
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCIAB0TX_VECTOR
__interrupt void USCIAB0TX_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCIAB0TX_VECTOR))) USCIAB0TX_ISR (void)
#else
#error Compiler not supported!
#endif
{
if (IFG2 & UCB0RXIFG) // Receive Data Interrupt
{
//Must read from UCB0RXBUF
uint8_t rx_val = UCB0RXBUF;
switch (SlaveMode)
{
case (RX_REG_ADDRESS_MODE):
ReceiveRegAddr = rx_val;
I2C_Slave_ProcessCMD(ReceiveRegAddr);
break;
case (RX_DATA_MODE):
ReceiveBuffer[ReceiveIndex++] = rx_val;
RXByteCtr--;
if (RXByteCtr == 0)
{
//Done Receiving MSG
SlaveMode = RX_REG_ADDRESS_MODE;
IE2 &= ~(UCB0TXIE);
IE2 |= UCB0RXIE; // Enable RX interrupt
I2C_Slave_TransactionDone(ReceiveRegAddr);
}
break;
default:
__no_operation();
break;
}
}
else if (IFG2 & UCB0TXIFG) // Transmit Data Interrupt
{
//Must write to UCB0TXBUF
switch (SlaveMode)
{
case (TX_DATA_MODE):
UCB0TXBUF = TransmitBuffer[TransmitIndex++];
TXByteCtr--;
if (TXByteCtr == 0)
{
//Done Transmitting MSG
SlaveMode = RX_REG_ADDRESS_MODE;
IE2 &= ~(UCB0TXIE);
IE2 |= UCB0RXIE; // Enable RX interrupt
I2C_Slave_TransactionDone(ReceiveRegAddr);
}
break;
default:
__no_operation();
break;
}
}
}
//******************************************************************************
// I2C Interrupt For Start, Restart, Nack, Stop ********************************
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCIAB0RX_VECTOR
__interrupt void USCIAB0RX_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCIAB0RX_VECTOR))) USCIAB0RX_ISR (void)
#else
#error Compiler not supported!
#endif
{
//仿真挂断点连这里都跳不进来
if (UCB0STAT & UCSTPIFG) //Stop or NACK Interrupt
{
UCB0STAT &=
~(UCSTTIFG + UCSTPIFG + UCNACKIFG); //Clear START/STOP/NACK Flags
}
if (UCB0STAT & UCSTTIFG)
{
UCB0STAT &= ~(UCSTTIFG); //Clear START Flags
}
}