This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2433: 捕获引脚确认

Part Number: MSP430FR2433


你好,

     我们想确认一下,在MSP430FR2433芯片上调试定时器捕获功能,我们将P2.3作为捕获引脚,请帮助确认一下该引脚是否可以作为捕获引脚使用?

     因为我们在文档内查看到下述信息,是否只有P1.1/P1.2/P1.4/P1.5可以用作捕获引脚功能?

  • 是否只有P1.1/P1.2/P1.4/P1.5可以用作捕获引脚功能?

    是的,您的理解是正确的

  • msp430fr243x_ta0_capture.c (ti.com)

    你好,如果我想将改示例代码内的P1.2捕获引脚改为P1.5捕获引脚,具体代码如下:

    我尝试将TA0.CCI2A(P1.2)修改为TA1.CCI1A(P1.5),但是现在回调功能不触发,可以帮助分析一下吗?

    #include <msp430.h>
    
    #define NUMBER_TIMER_CAPTURES        20
    
    volatile unsigned int timerAcaptureValues[NUMBER_TIMER_CAPTURES];
    unsigned int timerAcapturePointer = 0;
    
    int main(void)
    {
        WDTCTL = WDTPW | WDTHOLD;                       // Stop watchdog timer
    
        // Configure GPIO
        P1DIR |= BIT0;                                  // Set P1.0 as output
        P1OUT |= BIT0;                                  // P1.0 high
        P1SEL1 |= BIT5;                                 // TA0.CCI2A input capture pin, second function
        P1REN |= BIT5;                                  // enable internal pull-down resistor
        P1OUT &= ~BIT5;
        
        P2SEL1 |= BIT2;                                 // Set as ACLK pin, second function
        P2DIR |= BIT2;
    
        // Disable the GPIO power-on default high-impedance mode to activate
        // previously configured port settings
        PM5CTL0 &= ~LOCKLPM5;
    
        // Configure clock
        __bis_SR_register(SCG0);                        // disable FLL
        CSCTL3 |= SELREF__REFOCLK;                      // Set REFO as FLL reference source
        CSCTL0 = 0;                                     // clear DCO and MOD registers
        CSCTL1 &= ~(DCORSEL_7);                         // Clear DCO frequency select bits first
        CSCTL1 |= DCORSEL_2;                            // Set DCO = 4MHz
        CSCTL2 = FLLD_1 + 60;                           // DCODIV = 2MHz
        __delay_cycles(3);  
        __bic_SR_register(SCG0);                        // enable FLL
        while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));      // Poll until FLL is locked
    
        CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK;      // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
                                                        // default DCODIV as MCLK and SMCLK source
        CSCTL5 |= DIVM__1 | DIVS__2;                    // SMCLK = 1MHz, MCLK = 2MHz
    
        // Timer0_A3 Setup
        TA1CCTL1 |= CM_1 | CCIS_0 | CCIE | CAP | SCS;
                                                        // Capture rising edge,
                                                        // Use CCI2A=ACLK,
                                                        // Synchronous capture,
                                                        // Enable capture mode,
                                                        // Enable capture interrupt
    
        TA1CTL |= TASSEL_2 | MC_2 | TACLR;              // Use SMCLK as clock source, clear TA0R
                                                        // Start timer in continuous mode
    
        __bis_SR_register(LPM0_bits | GIE);
        __no_operation();
    }
    
    // Timer0_A3 CC1-2, TA Interrupt Handler
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector = TIMER1_A1_VECTOR
    __interrupt void TIMER1_A1_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(TIMER0_A1_VECTOR))) TIMER0_A1_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
        switch(__even_in_range(TA1IV,TA1IV_TAIFG))
        {
            case TA1IV_NONE:
                break;                                  // No interrupt
            case TA1IV_TACCR1:
                timerAcaptureValues[timerAcapturePointer++] = TA1CCR1;
                if (timerAcapturePointer >= 20)
                {
                    while (1) 
                    {
                        P1OUT ^= 0x01;                  // Toggle P1.0 (LED)
                        __delay_cycles(100000);
                    }
                }
                break;                                  // CCR1 not used
            case TA1IV_TACCR2:
                break;                                  // CCR2 not used
            case TA1IV_TAIFG:
                break;                                  // overflow 
            default: 
                break;
        }
    }

  • 下面是我之前成功测试1.4的,您可以看一下,我也来测试一下1.5

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2014, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     *
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //***************************************************************************************
    //  MSP430FR24xx Demo - Timer0_A3 Capture of ACLK
    //
    //  Description: Capture a number of periods of the ACLK clock and store them in an array.
    //  When the set number of periods is captured the program is trapped and the LED on
    //  P1.0 is toggled. At this point halt the program execution read out the values using
    //  the debugger.
    //  ACLK = REFOCLK = 32kHz, MCLK = SMCLK = default DCODIV = 1MHz.
    //
    //                MSP430FR2433
    //             -----------------
    //         /|\|                 |
    //          | |             P1.2|<-- TA0.CCI2A
    //          --|RST              |  |
    //            |             P2.2|--> ACLK
    //            |                 |
    //            |             P1.0|-->LED
    //
    //
    //  Wei Zhao
    //  Texas Instruments Inc.
    //  Jan 2014
    //  Built with IAR Embedded Workbench v6.20 & Code Composer Studio v6.0.1
    //***************************************************************************************
    #include <msp430.h>
    
    #define NUMBER_TIMER_CAPTURES        20
    
    volatile unsigned int timerAcaptureValues[NUMBER_TIMER_CAPTURES];
    unsigned int timerAcapturePointer = 0;
    
    int main(void)
    {
        WDTCTL = WDTPW | WDTHOLD;                       // Stop watchdog timer
    
        // Configure GPIO
        P1DIR |= BIT0;                                  // Set P1.0 as output
        P1OUT |= BIT0;                                  // P1.0 high
        P1SEL1 |= BIT4;                                 // TA0.CCI2A input capture pin, second function
        P1REN |= BIT4;                                  // enable internal pull-down resistor
        P1OUT &= ~BIT4;
    
        P2SEL1 |= BIT2;                                 // Set as ACLK pin, second function
        P2DIR |= BIT2;
    
        // Disable the GPIO power-on default high-impedance mode to activate
        // previously configured port settings
        PM5CTL0 &= ~LOCKLPM5;
    
        // Configure clock
        __bis_SR_register(SCG0);                        // disable FLL
        CSCTL3 |= SELREF__REFOCLK;                      // Set REFO as FLL reference source
        CSCTL0 = 0;                                     // clear DCO and MOD registers
        CSCTL1 &= ~(DCORSEL_7);                         // Clear DCO frequency select bits first
        CSCTL1 |= DCORSEL_2;                            // Set DCO = 4MHz
        CSCTL2 = FLLD_1 + 60;                           // DCODIV = 2MHz
        __delay_cycles(3);
        __bic_SR_register(SCG0);                        // enable FLL
        while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));      // Poll until FLL is locked
    
        CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK;      // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
                                                        // default DCODIV as MCLK and SMCLK source
        CSCTL5 |= DIVM__1 | DIVS__2;                    // SMCLK = 1MHz, MCLK = 2MHz
    
        // Timer0_A3 Setup
        TA1CCTL2 |= CM_1 | CCIS_0 | CCIE | CAP | SCS;
                                                        // Capture rising edge,
                                                        // Use CCI2A=ACLK,
                                                        // Synchronous capture,
                                                        // Enable capture mode,
                                                        // Enable capture interrupt
    
        TA1CTL |= TASSEL_2 | MC_2 | TACLR;              // Use SMCLK as clock source, clear TA0R
                                                        // Start timer in continuous mode
    
        __bis_SR_register(LPM0_bits | GIE);
        __no_operation();
    }
    
    // Timer0_A3 CC1-2, TA Interrupt Handler
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector = TIMER1_A1_VECTOR
    __interrupt void TIMER1_A1_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(TIMER1_A1_VECTOR))) TIMER1_A1_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
        switch(__even_in_range(TA1IV,TA1IV_TAIFG))
        {
            case TA1IV_NONE:
                break;                                  // No interrupt
            case TA1IV_TACCR1:
                break;                                  // CCR1 not used
            case TA1IV_TACCR2:
                timerAcaptureValues[timerAcapturePointer++] = TA0CCR2;
                if (timerAcapturePointer >= 20)
                {
                    while (1)
                    {
                        P1OUT ^= 0x01;                  // Toggle P1.0 (LED)
                        __delay_cycles(100000);
                    }
                }
                break;                                  // CCR2 not used
            case TA1IV_TAIFG:
                break;                                  // overflow
            default:
                break;
        }
    }
    

  • Hi Susan Yang

        请问P1.5可以吗?我想知道CCI2A 改为CCI1A还需要改哪些配置?我尝试修改引脚为P1.5,但是中断不会触发,请帮助确认

  • 抱歉,今天在家办公,板子没在身边

    之前我给出的P1.4您是可以成功进入中断的吗?

    我想知道CCI2A 改为CCI1A还需要改哪些配置?

    理论上没有其他需要修改的了

  • 你好,我刚尝试了一下,将您提供的P1.4下述代码进行修改:

        // Timer0_A3 Setup
        TA1CCTL2 |= CM_1 | CCIS_0 | CCIE | CAP | SCS;

    修改为

        // Timer0_A3 Setup
        TA1CCTL1 |= CM_1 | CCIS_0 | CCIE | CAP | SCS;

    此时P1.5下拉可以触发中断,此时触发的是中断 TA1IV_TACCR1

    但是TA0CCR2参数想确认一下,0和2是依据什么修改的?因为此时从TA0CCR2获取的参数是0,所以可能需要尝试其他参数

  • 但是TA0CCR2参数想确认一下,0和2是依据什么修改的?

    SFR_16BIT(TA0CCR0); /* Timer0_A3 Capture/Compare 0 */
    SFR_16BIT(TA0CCR1); /* Timer0_A3 Capture/Compare 1 */
    SFR_16BIT(TA0CCR2); /* Timer0_A3 Capture/Compare 2 */‘

    上面是"msp430fr2433.h"内的描述

    此时P1.5下拉可以触发中断,此时触发的是中断 TA1IV_TACCR1

    SFR_16BIT(TA1CCTL1); /* Timer1_A3 Capture/Compare Control 1 */
    SFR_16BIT(TA1CCTL2); /* Timer1_A3 Capture/Compare Control 2 */