This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: MSP430F5244: 25M时钟



__bis_SR_register(SCG0) ; // 关闭FLL控制回路
UCSCTL0 = 0x0000 ; // 设置DCOx, MODx
UCSCTL1 = DCORSEL_6 ; // 设置DCO振荡范围
UCSCTL2 = FLLD__1 + 799; // Fdco = ( FLL_FACTOR + 1)×FLLRef = (649 + 1) * 32768 = 21.2992MHz
__bic_SR_register(SCG0) ; // 打开FLL控制回路
__delay_cycles(1024000) ;
do
{
UCSCTL7 &=~(XT2OFFG+XT1LFOFFG+DCOFFG) ; // 清除 XT2,XT1,DCO 错误标志
SFRIFG1 &=~OFIFG ;
}while(SFRIFG1&OFIFG) ; // 检测振荡器错误标志

还有个问题,配置时钟25MHz时

设置UCSCTL2 = FLLD__1 + 799 ,一直停在while这里,这个有例程吗