Part Number: MSP430FR5994
使用了MSP430FR5994单片机,使用8MHz的晶体,连接至XT2OUT和XT2IN,作为高速时钟使用。通过配置PJSEL1.6=0,PJSEL0.6=1,并关闭HFXTOFF。在晶振错误标识为0,时,切换至HF,但是输出是4.MHz。通过CTL2可以正确设置MCLK和SMCLK为DCO、MODCLK、ACLk,但是就是无法使用HF。选择了HF后得到的依然是MODCLK时钟,也就是4.8MHz。不知何故?请指教!谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR5994
使用了MSP430FR5994单片机,使用8MHz的晶体,连接至XT2OUT和XT2IN,作为高速时钟使用。通过配置PJSEL1.6=0,PJSEL0.6=1,并关闭HFXTOFF。在晶振错误标识为0,时,切换至HF,但是输出是4.MHz。通过CTL2可以正确设置MCLK和SMCLK为DCO、MODCLK、ACLk,但是就是无法使用HF。选择了HF后得到的依然是MODCLK时钟,也就是4.8MHz。不知何故?请指教!谢谢!
请问您是否有测试下面的例程?在此例程中使用的是8Mhz的晶振
// Description: Configure ACLK = LFXT, SMCLK = HFXT and MCLK = DCO
// NOTE1: 32768Hz and 8MHz crystals required!
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2015, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430FR5x9x Demo - ACLK = XT1 = 32768Hz, SMCLK= XT2 = 8MHz, MCLK = DCO
//
// Description: Configure ACLK = LFXT, SMCLK = HFXT and MCLK = DCO
// NOTE1: 32768Hz and 8MHz crystals required!
//
// MSP430FR5994
// ---------------
// /|\| |
// | | |-LFXIN
// --|RST |-LFXOUT
// | |
// | |-HFXIN
// | |-HFXOUT
// | |
// | P1.0|---> LED
// | P2.0|---> ACLK = 32768Hz
// | P3.4|---> SMCLK = 8MHz
//
// William Goh
// Texas Instruments Inc.
// October 2015
// Built with IAR Embedded Workbench V6.30 & Code Composer Studio V6.1
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW | WDTHOLD;
// Configure GPIO
P1OUT = 0;
P1DIR = BIT0; // For LED
P2DIR |= BIT0;
P2SEL0 |= BIT0; // Output ACLK
P2SEL1 |= BIT0;
P3DIR |= BIT4;
P3SEL1 |= BIT4; // Output SMCLK
P3SEL0 |= BIT4;
PJSEL0 |= BIT4 | BIT5 | BIT6 | BIT7; // For XT1 and XT2
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
CSCTL0_H = CSKEY_H; // Unlock CS registers
CSCTL1 = DCOFSEL_6; // Set DCO to 8MHz
CSCTL2 = SELA__LFXTCLK | SELS__HFXTCLK | SELM__DCOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers to 1
CSCTL4 |= LFXTDRIVE_3 | HFXTDRIVE_3;
CSCTL4 &= ~(LFXTOFF | HFXTOFF);
do
{
CSCTL5 &= ~(LFXTOFFG | HFXTOFFG); // Clear XT1 and XT2 fault flag
SFRIFG1 &= ~OFIFG;
} while (SFRIFG1 & OFIFG); // Test oscillator fault flag
CSCTL0_H = 0; // Lock CS registers
while (1)
{
P1OUT ^= 0x01; // Toggle LED
__delay_cycles(8000000); // Wait 8,000,000 CPU Cycles
}
}