Part Number: MSP430FR6972
软件清LFXTOFFG时,会导致单片机重启,我在用户手册上没有找到相关解释,是正常现象吗?如果是正常现象,能否避免软件清LFXTOFFG时,单片机重启呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR6972
软件清LFXTOFFG时,会导致单片机重启,我在用户手册上没有找到相关解释,是正常现象吗?如果是正常现象,能否避免软件清LFXTOFFG时,单片机重启呢?
CSCTL5 &= ~(LFXTOFFG);
外部32768晶振遇到在设备组装时可能会受到轻微挤压导致,32768晶振瞬间故障,但是挤压过后又会恢复震荡,因为我的ACLK用的是外部的32768,单片机用户手册说,当外部晶振故障时会自动置位LFXTOFFG,并且自动切换到MODCLK代替32768供给ACLK,LFXTOFFG需要软件清除才会从MODCLK切回到32768。但是一执行CSCTL5 &= ~(LFXTOFFG);语句后单片机就自动重启一次。后来实验发现就算LFXTOFFG没置位,执行CSCTL5 &= ~(LFXTOFFG);也会重启一次。
时钟系统似乎工作不正常。您能否将 MCLK 和 SMCLK 输出到 GPIO 并确定频率范围?
CSCTL0_H = CSKEY >> 8;
CSCTL1 = DCOFSEL_1;
CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1;
CSCTL4 = 0;
CSCTL4 |= VLOOFF + SMCLKOFF + HFXTOFF;
do
{
CSCTL5 &= ~(LFXTOFFG+ HFXTOFFG);//
SFRIFG1 &= ~OFIFG;
}while (SFRIFG1&OFIFG);
CSCTL5 &= ~(ENSTFCNT1 + ENSTFCNT2);
CSCTL6 &=~( ACLKREQEN|MCLKREQEN|SMCLKREQEN);
CSCTL0_H = 0;
这是我的时钟配置,MCLK是用的DCOCLK,您要我在什么情况下,是把LFXTCLK输出吗?
是把LFXTCLK输出吗?
是的,您的理解是正确的。
正常运行时32.75K--32.81K
晶振受挤压后自动跳到modclk时是36.98K--37.0K
谢谢您的反馈。
请您试一下下面的代码能否正常运行,而不会复位
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2014, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430FR6x7x Demo - Output 32768Hz crystal on XT1 and observe failsafe
//
// Description: Configure ACLK = LFXT1 and enter LPM3.
// To observe failsafe behavior short the crystal briefly on the target board.
// This will cause an NMI to occur. P1.0 is toggled inside the NMI ISR.
// Once the fault flag is cleared XT1 operation continues from 32768Hz crystal
// Otherwise ACLK defaults to LFMODCLK (~37.5KHz).
// ACLK = LFXT1 = 32kHz, MCLK = SMCLK = 1MHz
//
// MSP430FR6972
// ---------------
// /|\| XIN|-
// | | | 32KHz Crystal
// --|RST XOUT|-
// | |
// | PJ.2|---> ACLK = 32.768kHz (or 37.5kHz during LFXTOFFG)
// | P7.4|---> SMCLK = MCLK = 1MHz
// | P1.0|---> LED
//
// Andreas Dannenberg
// Texas Instruments Inc.
// September 2014
// Built with IAR Embedded Workbench V5.60 & Code Composer Studio V6.0
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW | WDTHOLD;
// GPIO Setup
P1OUT = 0;
P1DIR = BIT0; // For LED
PJDIR |= BIT2;
PJSEL0 |= BIT2; // Output ACLK
PJSEL1 &= ~BIT2;
P7DIR |= BIT4;
P7SEL0 |= BIT4;
P7SEL1 |= BIT4; // Output SMCLK
PJSEL0 |= BIT4 | BIT5; // For XT1
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Clock System Setup
CSCTL0_H = CSKEY >> 8; // Unlock CS registers
CSCTL1 = DCOFSEL_0; // Set DCO to 1MHz
CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers
CSCTL4 &= ~LFXTOFF;
do
{
CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
// Now that osc is running enable fault interrupt
SFRIE1 |= OFIE;
__bis_SR_register(LPM0_bits); // Wait in LPM0 for fault flag
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=UNMI_VECTOR
__interrupt void UNMI_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(UNMI_VECTOR))) UNMI_ISR (void)
#else
#error Compiler not supported!
#endif
{
do
{
// set a breakpoint on the line below to observe XT1 operating from VLO
// when the breakpoint is hit during a crystal fault
CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
P1OUT |= BIT0;
__delay_cycles(25000); // time for flag to get set again
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
P1OUT &= ~BIT0;
}
上午又做实验应该是找到原因了
我的时钟初始化代码中

第一条语句解锁,然后最后一条又相当于锁了时钟的寄存器,手册里边说的是,
| CSKEY password. Must always be written with A5h; a PUC is generated if any other value is written. Always reads as 96h. After the correct password is written, all CS registers are available for writing. |
相当于我再后边的程序没有解锁,直接这样写CSCTL5 &= ~(LFXTOFFG);,导致了一个PUC,所以只要执行这个就复位。
后来改了一下清LFXTOFFG的后边程序的代码
CSCTL0_H = CSKEY >> 8;
do
{
CSCTL5 &= ~(LFXTOFFG+ HFXTOFFG);//
SFRIFG1 &= ~OFIFG;
}while (SFRIFG1&OFIFG);
CSCTL0_H = 0;
这样就OK了,不重启
再次感谢您抽时间给我解答问题,没有您的帮助我还不知道啥时候能找出问题所在,谢谢!!!!!