请问在定时器A中有TASSEL_0和TASSEL_1和TASSEL1 和TASSEL0 有什么区别
再就是MC0和MC_0的区别
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
我翻了一下宏定义
#define TASSEL1 (0x0200) /* Timer A clock source select 1 */
#define TASSEL0 (0x0100) /* Timer A clock source select 0 */
#define ID1 (0x0080) /* Timer A clock input divider 1 */
#define ID0 (0x0040) /* Timer A clock input divider 0 */
#define MC1 (0x0020) /* Timer A mode control 1 */
#define MC0 (0x0010) /* Timer A mode control 0 */
#define TACLR (0x0004) /* Timer A counter clear */
#define TAIE (0x0002) /* Timer A counter interrupt enable */
#define TAIFG (0x0001) /* Timer A counter interrupt flag */
#define MC_0 (0*0x10u) /* Timer A mode control: 0 - Stop */
#define MC_1 (1*0x10u) /* Timer A mode control: 1 - Up to CCR0 */
#define MC_2 (2*0x10u) /* Timer A mode control: 2 - Continous up */
#define MC_3 (3*0x10u) /* Timer A mode control: 3 - Up/Down */
#define ID_0 (0*0x40u) /* Timer A input divider: 0 - /1 */
#define ID_1 (1*0x40u) /* Timer A input divider: 1 - /2 */
#define ID_2 (2*0x40u) /* Timer A input divider: 2 - /4 */
#define ID_3 (3*0x40u) /* Timer A input divider: 3 - /8 */
#define TASSEL_0 (0*0x100u) /* Timer A clock source select: 0 - TACLK */
#define TASSEL_1 (1*0x100u) /* Timer A clock source select: 1 - ACLK */
#define TASSEL_2 (2*0x100u) /* Timer A clock source select: 2 - SMCLK */
#define TASSEL_3 (3*0x100u) /* Timer A clock source select: 3 - INCLK */
有_的是直接为你提供的快捷宏定义,没有_的猜想是寄存器中的两个控制位
本人同样新手,答错请勿怪
Peter_Zheng你怎么回事呀?怎么说没区别?楼主是起的英文名字,应该不是一般的小混混吧?很可能是外企公司的?
例如,MC0对应两个控制位中的第0位,MC1对应第1位。而MC_0~MC_3对应两个控制位组成的二位二进制值,但是实际值还要看这两个控制位在整个控制寄存器中的位置,这可以从二楼贴出的看出来。注意有的是乘零
所以,使用MC0和使用MC_1是一样,使用MC1和使用MC_2是一样。
Jack John, TI为了方便用户编程而在头文件中定义了不同的宏,
以MC0和MC_0为例,
#define MC1 (0x0020) /* Timer A mode control 1 */
#define MC0 (0x0010) /* Timer A mode control 0 */
#define MC_0 (0*0x10u) /* Timer A mode control: 0 - Stop */
#define MC_1 (1*0x10u) /* Timer A mode control: 1 - Up to CCR0 */
#define MC_2 (2*0x10u) /* Timer A mode control: 2 - Continous up */
#define MC_3 (3*0x10u) /* Timer A mode control: 3 - Up/Down */
MC0是用于直接指示MCx的低位在TACTL register的 bit4, MC0则指示MCx的第二位在TACTL register的 bit5.
而增加下划线后的MC_0,MC_1,MC_2,MC_3则是直接说明MCx Mode control几种不同的选择时,MCx对应在TACTL register该设置的值。
用法举例:例如你想设置 MCx Mode control为Up/down mode,
1.如果用MC0,MC1来控制,则为 TACTL |= MC0+MC1; ---此种用法,是直接置MCx对应位,当然也方便客户直接清对应位。但是不方便别人看程序。
2.如果用MC_x来控制,则为 TACTL |= MC_3; -----此种用法,更方便读者看程序。
关于 TASSEL_0和TASSEL_1和TASSEL1 和TASSEL0的区别,以此类推。