This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
芯片:MSP430F5418A
编程软件:IAR5.4
仿真器:ZT-FET430UIF
问题:在下载程序时,IAR软件报错,Couldn't find device...,软件中器件类型、Debugger->Driver选择为FET Debugger,Connection为TI USB-IF,开发板为自己画的PCB板,焊了4块(只焊了晶振、去耦电容和SBW接口,便于进行测试),在下载时都是这个问题。问题补充:购买的第一批5418A芯片没有出现这个问题,第二批的芯片都不能下载成功,同一家供应商买的,质量估计没有问题。仿真器也换了一个,也是同样的问题。
Lei Bao3,
既然之前曾经连接并下载成功过,那说明电路设计是没有问题的,可能是芯片本身或者焊接过程中导致芯片损坏。你找个曾经成功下载的板子,换个这一批的芯片上去,看看还可不可以成功下载。
焊接过程中可能导致芯片损坏的原因有很多,譬如存放芯片过程中可能遭遇静电,焊接温度过高且时间过长等。但是200~300oC应该是没有问题的。而且一般而言,MCU的芯片也不会这么脆弱。你先测测看吧,看看究竟是不是芯片本身的问题。另外你有没有对应的socket 板,如果有的话,可以直接把芯片放到socket板上,试着用debugger连一下。看看芯片是不是好的。