This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、MSP430FR6007中关于调用LEA对ADC采集的数据进行FFT变换的时候,由于ADC采集的是int16_t型数据,但是官方给出的API函数都是_q15/-q31类型的,请问LEA怎样直接使用int6_t类型进行福利也变化?(如果不能直接使用int6_t类型,改怎么处理?我测试了一下,如果将每个int16_t类型在一个个转换为_q15类型,这个浪费时间太长?)
需要将 ADC 结果转换为Q15 和 iQ31 格式,有两个疑问:
1、有什么高效率的转化方法吗?转化过程中的大量乘除运算花费的时间也不少的啊
2、运用LEA处理ADC采集的数据,对于该芯片应该是很普通的应用。然而ADC采集的整型数据,但是LEA处理的是Q15 和 iQ31 ,这两者就会出现严重的不匹配,如果通过软件去转化整型数据为Q15 和 iQ31 格式,这不是有把LEA节省的时间,有给变相的浪费掉了吗?
请参阅MSPDSPLib 文档,该文档定义了宏以便在数据类型之间进行高效转换。
请参阅以下链接以帮助量化 LEA 的性能:
https://www.ti.com/tool/MSP430-LEA-GUI
Benchmarking the Signal Processing Capabilities of the Low-Energy Accelerator (Rev. B)