在下载IAR5.51时无论30天的限制版本还是4k的限制版本都说与正式版本的区别是不含有“Source code for runtime libraries ”,这个是什么?在使用时有没有这个有什么区别吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在下载IAR5.51时无论30天的限制版本还是4k的限制版本都说与正式版本的区别是不含有“Source code for runtime libraries ”,这个是什么?在使用时有没有这个有什么区别吗?
tianm 21ic,
关于MSP430的runtime libraries, 在 MSP430 Optimizing C/C++ Compiler v 4.1 User's Guide中的第七章7 Using Run-Time-Support Functions and Building Libraries有,下载链接为:
http://www.ti.com/lit/ug/slau132g/slau132g.pdf
主要包括:
The run-time-support library contains the following:
• ANSI/ISO C/C++ standard library
• C I/O library
• Low-level support functions that provide I/O to the host operating system
• Fundamental arithmetic routines
• System startup routine, _c_int00
• Functions and macros that allow C/C++ to access specific instructions