Part Number: EVM430-FR6043
您好,我在使用EVM430-FR6043平台评价气体超声流量模块,实际应用中,我们需要150hz的Delta_TOF采样频率,目前通过USSSWLIB软件调试最高只可以设置到20hz(依据UPS0到UPS1的最小时间可以设置为50ms推算),所以想在我想知道为何最小限制为50ms,初步推断可能是软运行时间占比较大,目前我不知道算法(hibert wide)实际运行时间多少?是否可以优化?我需要详细的分析此平台可以做到的最高的Delta_TOFd的获取频率。