Part Number: MSP-EXP430G2
手头有一块MSP-EXP430G2,发现它有一个SBW的对外接口,
不知道这个SBW的接口可不可以仿真另一个目标板。就是将跳线J3全部断开,使用J4的2.3.4.5四个脚,对应
VCC,SBWTCK ,SBWTDIO,GND.
如果看可以的话,能仿真全系列的MSP430吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、可以仿真其他板子,这可以看成就是一个JTAG接口。
2、这个你可以看一下user's guide中的说明:On some Spy-Bi-Wire capable MSP430 devices, TEST/SBWTCK is very sensitive to rising signal edges that can cause the test logic to enter a state where an entry sequence (either 2‑wire or 4-wire) is not recognized correctly and JTAG access stays disabled. Unintentional edges on SBWTCK can occur when the JTAG connector is connected to the target device.