我最近设计一款低功耗的万用表,按键我想采用MSP430F5529开发板自带的触摸按键,当没有测量的时候,我准备叫他进入低功耗的待机模式(如:LPM0模式),问题是触摸按键可以唤醒MCU吗,我知道普通的轻触按键可以唤醒的;再就是好像ADC12(关于ADC12中断唤醒MCU不是很明白)中断也可以唤醒的,问题是当ADC12进入低功耗模式后,还是执行ADC12吗?如何唤醒??或者是ADC12采样的值发生变化的时候唤醒MCU??、
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我最近设计一款低功耗的万用表,按键我想采用MSP430F5529开发板自带的触摸按键,当没有测量的时候,我准备叫他进入低功耗的待机模式(如:LPM0模式),问题是触摸按键可以唤醒MCU吗,我知道普通的轻触按键可以唤醒的;再就是好像ADC12(关于ADC12中断唤醒MCU不是很明白)中断也可以唤醒的,问题是当ADC12进入低功耗模式后,还是执行ADC12吗?如何唤醒??或者是ADC12采样的值发生变化的时候唤醒MCU??、
触摸按键本身不能唤醒mcu,因为触摸按键是需要mcu进行相关运算。可以考虑在固定时间里去多次监测触摸按键,其他时间在低功耗下待机,以达到低功耗的目的。
您好,我只是举个例子,具体的功耗模式还没有测量,只是在设计的时候考虑到触摸按键比较创新,但是我还是想降低功耗,感觉触摸按键就是不能唤醒,这是不死心再问问!
既然触摸按键不能唤醒,那么ADC12的中断可以唤醒MCU吗?
楼主,你给的那个链接不存在了,在官网也打不开了!!
谢谢!!