This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我创建一个程式码试着用Energia跑2355,但这串错误指令我无法找到所需要的文件。
Energia: 1.8.11E23 (Windows 10), 開發板:"MSP-EXP430FR2355LP"
In file included from C:\Users\20753004\AppData\Local\Energia15\packages\energia\hardware\msp430\1.0.7\cores\msp430/Energia.h:4:0,
from C:\Users\20753004\AppData\Local\Energia15\packages\energia\hardware\msp430\1.0.7\cores\msp430/Arduino.h:3,
from sketch\sketch_feb14a.ino.cpp:1:
c:\users\20753004\appdata\local\energia15\packages\energia\tools\msp430-gcc\4.6.6\bin\../lib/gcc/msp430/4.6.3/../../../../msp430/include/msp430.h:1793:2: error: #error "Failed to match a default include file"
exit status 1
開發板 MSP-EXP430FR2355LP 編譯錯誤。
This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.
upload出现的错误
DSLite version 8.2.0.1400
Configuring Debugger (may take a few minutes on first launch)...
上傳草稿碼時發生錯誤
Failed: Cannot read System Setup data from XML file C:\Users\20753004\AppData\Local\Energia15\packages\energia\tools\dslite\8.2.0.1400/MSP-EXP430FR2355LP.ccxml
Error parsing file:
Fatal Error at (0, 0): An exception occurred! Type:RuntimeException, Message:The primary document entity could not be opened. Id=C:\Users\20753004\AppData\Local\Energia15\packages\energia\tools\dslite\8.2.0.1400/MSP-EXP430FR2355LP.ccxml