This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用DCO TimerA设计秒计时器



1.有几个难题,不能自动重装,也不是PWM方式,如何保证1s中断一次.(假设DCO无误差)

2.每次进入中断后进行DCO校准.误差可以更好地控制吗?

3.纽扣电池2.8V供电,能保证MCLK = 1MHz,SMCLK = 125kHz吗?

4.计时上限9999秒,不用考虑长期走时.这样做可靠吗?

  • 1.,不能重装载是配置不正确,自己再检查。关于一秒的中断,可以达到,但是你的外部时钟可能很低,当然,大家一般不是这么去定时一秒的,一般是先固定一个单位,比如50ms,每50ms中断一次,那20次中断不就是1s了吗,没中断意思计数,够20次了在动做,

    2、不建议dco校准,很费劲的,直接用外部的相对稳定

    3、这个的看数据手册里面的时钟电源关系图了。印象中可以的

    4、单片机计时绝对可靠,除非你的程序错了

  • 楼上正解,单片机一般使用小单位定时,这样这个定时器还可以用于其它终端的刷新。