This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F169的ADC12采样率问题



求点拨!!
想要使用单通道重复采样,工作在最高采样率。但是用TI的例程实测,采样率都低太多,跟手册上说的200ksps都不在一个数量级。

时钟用ADC内部振荡器,约5MHz,2个采样周期+13个转换周期,计算下来应该4us左右采一个点。

但是,计数1s进入ADC中断的次数,才不到6000多次。

IAR编译,自己画的开发板,代码如下:

#include  <msp430.h>
#include  "..\com\delay.h"

#define   Num_of_Results   30

static unsigned int results[Num_of_Results];  // Needs to be global in this
                                              // example. Otherwise, the
                                              // compiler removes it because it
                                              // is not used for anything.
static unsigned int index = 0;
unsigned char ir;

void main(void)
{
  WDTCTL = WDTPW+WDTHOLD;                   // Stop watchdog timer
  /* for test */
  P1DIR |= BIT0;                            // 上电指示
  P1OUT |= BIT0;
  
  P2DIR |= BIT6;                            // ADC12CLK
  P2SEL |= BIT6;
  // Vref+ 在pin7测试
  
  P5DIR |= 0x70;                            // P5.6,5,4 outputs
  P5SEL |= 0x70;                            // P5.6,5,4 options, ACLK, SMCLK, MCLK
  /**/
  
  P6SEL |= 0x01;                            // Enable A/D channel A0
  ADC12CTL0 = ADC12ON + SHT0_2 + REFON + MSC;           // Turn on ADC12, set sampling time
  ADC12CTL1 = SHP + CONSEQ_2;               // Use sampling timer, single-repeat mode, default:  ADC12CLK = ADC12OSC(about 5MHz)
  ADC12MCTL0 = SREF_1;                      // Vr+=Vref+
  ADC12IE = 0x01;                           // Enable ADC12IFG.0
  delay_ms(20);
  ADC12CTL0 |= ENC;                         // Enable conversions
  ADC12CTL0 |= ADC12SC;                     // Start conversion
  
  _BIS_SR(LPM0_bits + GIE);                 // Enter LPM0,Enable interrupts
}


#pragma vector=ADC12_VECTOR
__interrupt void ADC12ISR (void)
{
  results[index] = ADC12MEM0;               // Move results
  index = (index+1)%Num_of_Results;         // Increment results index, modulo
}