我想选择VCC作为电压参考源,因为目前引脚不够用,但是没找到,或者哪里可以输出1.2V参考电压?我用的是F2O13
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想选择VCC作为电压参考源,因为目前引脚不够用,但是没找到,或者哪里可以输出1.2V参考电压?我用的是F2O13
你好,参照例程具体的设置如下
SD16CTL = SD16REFON + SD16SSEL_1; // 参考电压选择1.2V ref,ADC的时钟源选择 SMCLK
SD16INCTL0 = SD16INCH_1; // A1+/-
SD16CCTL0 = SD16UNI + SD16IE; // 256OSR, unipolar, interrupt enable
SD16AE = SD16AE2; // P1.1 A1+, A1- = VSS
SD16CCTL0 |= SD16SC; // Set bit to start conversion
XinXin Li,
对于SD16而言,其电压参考源可以直接使用内部参考源1.2V,只要将SD16REFON设为1即可, 不需要输出的。另外使用它时,建议在VREF和AVSS间加一个100nf的电容。当然,如果想要将其输出,需要设置SD16VMIDON = 1。此时建议在VREF和AVSS间加一个470nf的电容。也是可以的在User guide上有详细的描述,如下所示:
26.2.3 Voltage Reference Generator
The SD16_A module has a built-in 1.2-V reference. It is enabled by the SD16REFON bit. When using the
internal reference an external 100-nF capacitor connected from VREF to AVSS is recommended to reduce
noise. The internal reference voltage can be used off-chip when SD16VMIDON = 1. The buffered output
can provide up to 1 mA of drive. When using the internal reference off-chip, a 470-nF capacitor connected
from VREF to AVSS is required. See the device-specific data sheet for parameters.
An external voltage reference can be applied to the VREF input when SD16REFON and SD16VMIDON are
both reset.