This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f169 UART编程

能帮帮忙看看这个程序吗?这是我自己买的开发板自带的例程,为什么在开发板上就不能都实现它的功能呢?

板子应该是没问题的应为我跑过一个把接收到的在发出去的例程

/*****************************************************
程序功能:MCU不停向PC机发送数据,在屏幕上显示0~127对应
          的ASCII字符
------------------------------------------------------
通信格式:N.8.1, 2400
------------------------------------------------------
测试说明:打开串口调试助手,正确设置通信格式,观察屏幕
******************************************************/

#include  <msp430x16x.h>
#include  "BoardConfig.h"

void Delays(void);
void PutString(uchar *ptr);

/********************主函数**********************/
void main(void)
{
    uchar *tishi = " MCU sends 0~127 to PC and the\
                    \n screen will display their corresponding\
                    \n ASCII code as follows:";
    uchar value = 0;
 
    WDTCTL = WDTPW + WDTHOLD;                 // 关狗
    BoardConfig(0xb8);                        // 关流水灯、蜂鸣器和数码管
    P3SEL |= 0x30;                            // P3.4,5选择为UART收发端口
    ME1 |= UTXE0 + URXE0;                     // 使能USART0收发
    UCTL0 |= CHAR;                            // 8-bit character
    UTCTL0 |= SSEL0;                          // UCLK = ACLK
    UBR00 = 0x0D;                             // 32k/2400 - 13.65
    UBR10 = 0x00;                             //
    UMCTL0 = 0x6B;                            // Modulation
    UCTL0 &= ~SWRST;                          // 初始化UART0状态机
    IE1 |= URXIE0;                            // 使能接收中断
    _EINT();
    PutString(tishi);
    while(1)
    {    
        while (!(IFG1 & UTXIFG0));
        TXBUF0 = value++;
        value &= 0x7f;                        // 保证value的数值小于128
      PutString(tishi);
        while (!(IFG1 & UTXIFG0));
        TXBUF0 = '\n';
       Delays();
    }
}
/*******************************************
函数名称:PutSting
功    能:向PC机发送字符串
参    数:无
返回值  :无
********************************************/
void PutString(uchar *ptr)
{
      while(*ptr != '\0')
      {
            while (!(IFG1 & UTXIFG0));                // TX缓存空闲?
            TXBUF0 = *ptr++;                       // 发送数据
            Delays();
      }
      while (!(IFG1 & UTXIFG0));
      TXBUF0 = '\n';
}
/*******************************************
函数名称:Delays
功    能:延时一会
参    数:无
返回值  :无
********************************************/
void Delays(void)
{
    uchar i=20;
    uint j;

    while(i--)
    {
            j=2000;
            while(j--);
    }
}